![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The host_demo.c file implements the ISSDK HOST I/O Demo. More...
#include "board.h"#include "pin_mux.h"#include "clock_config.h"#include "Driver_USART.h"#include "issdk_hal.h"#include "gpio_driver.h"#include "host_io_uart.h"#include "systick_utils.h"#include "auto_detection_service.h"
Go to the source code of this file.
Macros | |
| #define | APPLICATION_NAME "HOST_DEMO" |
| Unique Name for this application which should match the target GUI pkg name. More... | |
| #define | APPLICATION_VERSION "1.0" |
| Version to distinguish between instances the same application based on target Shield and updates. More... | |
Functions | |
| bool | process_host_command (uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse, size_t *hostMsgSize, size_t respBufferSize) |
| int | main (void) |
| Main function. More... | |
Variables | |
| char | boardString [ADS_MAX_STRING_LENGTH] = {0} |
| char | shieldString [ADS_MAX_STRING_LENGTH] = {0} |
| char | embAppName [ADS_MAX_STRING_LENGTH] = {0} |
The host_demo.c file implements the ISSDK HOST I/O Demo.
Definition in file host_demo.c.
| #define APPLICATION_NAME "HOST_DEMO" |
Unique Name for this application which should match the target GUI pkg name.
Definition at line 59 of file host_demo.c.
Referenced by main().
| #define APPLICATION_VERSION "1.0" |
Version to distinguish between instances the same application based on target Shield and updates.
Definition at line 61 of file host_demo.c.
Referenced by main().
| int main | ( | void | ) |
Main function.
Initialize the MCU hardware.
Initialize GREEN LED pin used by FRDM board
Initialize the UART driver.
Set the UART Power mode.
Set UART Baud Rate.
Initialize Host I/O.
Definition at line 125 of file host_demo.c.
References ADS_MAX_STRING_LENGTH, APPLICATION_NAME, APPLICATION_VERSION, BOARD_BootClockRUN, BOARD_DEBUG_UART_BAUDRATE, BOARD_RunADS(), BOARD_SystickEnable(), boardString, Driver_GPIO_KSDK, embAppName, GPIO_DIRECTION_OUT, GREEN_LED, HOST_FORMAT_HDLC, HOST_FORMAT_PLAIN, Host_IO_Init(), Host_IO_Receive(), Host_IO_Send(), HOST_S_DRIVER, HOST_S_SIGNAL_EVENT, int32_t(), pGpioDriver, GENERIC_DRIVER_GPIO::pin_init, process_host_command(), SHIELD_NAME, shieldString, SMC, SMC_SetPowerModeWait(), status, and GENERIC_DRIVER_GPIO::toggle_pin.

| bool process_host_command | ( | uint8_t | tag, |
| uint8_t * | hostCommand, | ||
| uint8_t * | hostResponse, | ||
| size_t * | hostMsgSize, | ||
| size_t | respBufferSize | ||
| ) |
Definition at line 73 of file host_demo.c.
References boardString, embAppName, HOST_PRO_INT_DEV_TAG, and shieldString.
Referenced by main().

| char boardString[ADS_MAX_STRING_LENGTH] = {0} |
Definition at line 66 of file host_demo.c.
Referenced by main(), and process_host_command().
| char embAppName[ADS_MAX_STRING_LENGTH] = {0} |
Definition at line 67 of file host_demo.c.
Referenced by main(), and process_host_command().
| char shieldString[ADS_MAX_STRING_LENGTH] = {0} |
Definition at line 66 of file host_demo.c.
Referenced by main(), and process_host_command().