![]()  | 
  
    ISSDK
    1.7
    
   IoT Sensing Software Development Kit 
   | 
 

Files | |
| file | data_logger_demo.c [code] | 
| The data_logger_demo.c file implements the ISSDK Data Logger for RD-KL25-AGMP01 example demonstration with one sensor in Interrupt mode and other two in polling mode. MPL3115 is in One-Shot Poll Mode. FXOS8700 is @200Hz Hybrid Poll Mode. FXAS21002 is @200Hz Interrupt Mode. Data from MPL3115, FXOS8700 and FXAS21002 is only read when INT from FXAS21002 is received. The FXAS21002 ODR serves as the application ODR time keeper.  | |
| file | demo_11_axis_mult2b.c [code] | 
| The demo_11_axis_mult2b.c file implements the ISSDK MMA8652, MAG3110, FXAS21002 and MPL3115 sensors 11-Axis demo example demonstration using Bluetooth.  | |
| file | diff_p_demo.c [code] | 
| The diff_p_demo.c file implements the ISSDK DIFF_P sensor driver example demonstration with Interrupt mode.  | |
| file | dp5004_demo.c [code] | 
| The dp5004_demo.c file implements the ISSDK MPXVDP5004 analog sensor driver demo demonstration in interrupt mode with FRDM-KE15Z.  | |
| file | fxas21002_demo.c [code] | 
| The fxas21002_demo.c file implements the ISSDK FXAS21002 sensor demo example demonstration with interrupt mode.  | |
| file | fxas21002_poll_demo.c [code] | 
| The fxas21002_poll_demo.c file implements the ISSDK FXAS21002 sensor demo example demonstration with Poll mode.  | |
| file | fxlc95000_flash_demo.c [code] | 
| The fxlc95000_flash_demo.c file implements the ISSDK FXLC95000L sensor driver example demonstration for FLASH programming and Streaming for I2C Mode using Host I/O.  | |
| file | fxls8471_demo.c [code] | 
| The fxls8471_demo.c file implements the ISSDK FXLS8471 sensor demo example demonstration with interrupt mode.  | |
| file | fxls8962_demo.c [code] | 
| The fxls8962_demo.c file implements the ISSDK FXLS8962 sensor demo example demonstration with interrupt mode.  | |
| file | fxos8700_demo.c [code] | 
| The fxos8700_demo.c file implements the ISSDK FXOS8700 sensor driver example demonstration with interrupt mode.  | |
| file | fxos8700_poll_demo.c [code] | 
| file | fxpq3115_demo.c [code] | 
| The fxpq3115_demo.c file implements the ISSDK FXPQ3115 sensor demo example demonstration with One-Shot mode.  | |
| file | host_demo.c [code] | 
| The host_demo.c file implements the ISSDK HOST I/O Demo.  | |
| file | mag3110_demo.c [code] | 
| The mag3110_demo.c file implements the ISSDK MAG3110 sensor demo example demonstration with interrupt mode.  | |
| file | mag3110_poll_demo.c [code] | 
| The mag3110_poll_demo.c file implements the ISSDK MAG3110 sensor demo example demonstration with poll mode.  | |
| file | mma845x_demo.c [code] | 
| The mma845x_demo.c file implements the ISSDK MMA845x sensor demo example demonstration with interrupt mode.  | |
| file | mma8491q_demo.c [code] | 
| The mma8491q_demo.c file implements the ISSDK MMA8491Q sensor driver demo demonstration with polling mode.  | |
| file | mma865x_demo.c [code] | 
| The mma865x_demo.c file implements the ISSDK MMA865x sensor demo example demonstration with interrupt mode.  | |
| file | mma9553_demo.c [code] | 
| The mma9553_demo.c file implements the ISSDK MMA9553L sensor driver example demonstration as a Accelerometer in I2C Mode.  | |
| file | mpl3115_demo.c [code] | 
| The mpl3115_demo.c file implements the ISSDK MPL3115 sensor demo example demonstration with One-Shot mode.  | |
| file | mpl3115_oneShot_demo.c [code] | 
| The mpl3115_oneShot_demo.c file implements the ISSDK MPL3115 sensor demo example demonstration with One-Shot mode.  | |
| file | mpl3115_poll_demo.c [code] | 
| The mpl3115_poll_demo.c file implements the ISSDK MPL3115 sensor demo example demonstration with One-Shot Poll mode.  | |
| file | orientaion_application_baremetal_agm01.c [code] | 
| The orientaion_application_baremetal_agm01.c file implements the ISSDK baremetal orientation application for FRDM-STBC-AGM01 using sensor fusion core functional interfaces and host i/o interface.  | |
| file | orientaion_application_baremetal_agm04.c [code] | 
| The orientaion_application_baremetal_agm04.c file implements the ISSDK baremetal orientation application for FRDM-STBC-AGM04 using sensor fusion core functional interfaces and host i/o interface.  | |
| file | orientaion_application_baremetal_agmp03.c [code] | 
| The orientaion_application_baremetal_agmp03.c file implements the ISSDK baremetal orientation application for FRDM-STBC-AGMP03 using sensor fusion core functional interfaces and host i/o interface.  | |