46 #include "clock_config.h"    47 #include "fsl_debug_console.h"    52 #include "Driver_I2C.h"    57 #include "issdk_hal.h"    58 #include "gpio_driver.h"    68 #define FF_MT_WT_DBCNT 0x28      69 #define FF_MT_THS_VALUE 0x03    132     PRINTF(
"\r\n ISSDK MMA865x sensor driver example for Freefall Detection. \r\n");
   139     if (ARM_DRIVER_OK != status)
   141         PRINTF(
"\r\n I2C Initialization Failed\r\n");
   146     status = I2Cdrv->PowerControl(ARM_POWER_FULL);
   147     if (ARM_DRIVER_OK != status)
   149         PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
   154     status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   155     if (ARM_DRIVER_OK != status)
   157         PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
   166         PRINTF(
"\r\n Sensor Initialization Failed\r\n");
   169     PRINTF(
"\r\n Successfully Initiliazed Sensor\r\n");
   182         PRINTF(
"\r\n MMA865x Sensor Configuration Failed, Err = %d \r\n", status);
   185     PRINTF(
"\r\n MMA865x now active and detecting freefall... \r\n");
   204             PRINTF(
"\r\n Read Failed\r\n");
   214         PRINTF(
"\r\n Freefall detected !!!\r\n");
 #define MMA865x_CTRL_REG3_IPOL_MASK
 
#define MMA865x_XYZ_DATA_CFG_FS_MASK
 
#define __END_WRITE_DATA__
 
int32_t MMA865x_I2C_Initialize(mma865x_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
 
#define BOARD_BootClockRUN
 
int main(void)
Main function. 
 
#define MMA865x_CTRL_REG5_INT_CFG_FF_MT_MASK
 
#define MMA865x_CTRL_REG3_IPOL_ACTIVE_HIGH
 
const registerreadlist_t cMma865xFreeFallEvent[]
Address of Freefall Status Register. 
 
#define MMA865x_FF_MT_THS_THS_MASK
 
int32_t MMA865x_I2C_ReadData(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
#define MMA865x_FF_MT_CFG_ELE_EN
 
void BOARD_InitDebugConsole(void)
 
This defines the sensor specific information. 
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
#define MMA865x_CTRL_REG1_DR_MASK
 
#define __END_READ_DATA__
 
#define MMA865x_FF_MT_CFG_YEFE_MASK
 
GENERIC_DRIVER_GPIO * pGpioDriver
 
volatile bool gMma865xEventReady
 
#define MMA865x_CTRL_REG1_DR_100HZ
 
void MMA865x_I2C_SetIdleTask(mma865x_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
#define MMA8652_WHOAMI_VALUE
 
#define MMA865x_CTRL_REG4_INT_EN_FF_MT_EN
 
void mma865x_int_event_ready_callback(void *pUserData)
This is the Sensor Event Ready ISR implementation. 
 
#define MMA865x_FF_MT_CFG_OAE_FREEFALL
 
int32_t MMA865x_I2C_Configure(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
const registerwritelist_t cMma865xConfigFreeFall[]
Register settings for freefall detection. 
 
#define MMA865x_FF_MT_CFG_XEFE_EN
 
#define MMA865x_XYZ_DATA_CFG_FS_2G
 
#define MMA865x_CTRL_REG4_INT_EN_FF_MT_MASK
 
#define MMA865x_CTRL_REG2_MODS_MASK
 
#define MMA865x_FF_MT_CFG_ZEFE_EN
 
#define MMA865x_FF_MT_CFG_ZEFE_MASK
 
#define MMA865x_CTRL_REG5_INT_CFG_FF_MT_INT1
 
#define MMA865x_FF_MT_SRC_EA_NONE
 
#define I2C_S_DEVICE_INDEX
 
#define MMA865x_FF_MT_CFG_XEFE_MASK
 
The mma865x_drv.h file describes the MMA865x driver interface and structures. 
 
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
 
#define MMA865x_FF_MT_THS_DBCNTM_INC_CLR
 
#define MMA865x_FF_MT_CFG_ELE_MASK
 
Access structure of the GPIO Driver. 
 
#define MMA865x_FF_MT_SRC_EA_MASK
 
#define MMA865x_CTRL_REG2_MODS_HR
 
This structure defines the Write command List. 
 
This structure defines the Read command List. 
 
#define MMA865x_FF_MT_CFG_YEFE_EN
 
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
 
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features. 
 
#define I2C_S_SIGNAL_EVENT
 
#define MMA865x_FF_MT_THS_DBCNTM_MASK
 
#define MMA865x_FF_MT_CFG_OAE_MASK