ISSDK  1.8
IoT Sensing Software Development Kit
Functions | Variables
fxls8962_drv.c File Reference

The fxls8962_drv.c file implements the FXLS8962 sensor driver interfaces. More...

#include "gpio_driver.h"
#include "fxls8962_drv.h"
#include "systick_utils.h"
Include dependency graph for fxls8962_drv.c:

Go to the source code of this file.

Functions

void FXLS8962_SPI_ReadPreprocess (void *pCmdOut, uint32_t offset, uint32_t size)
 The SPI Read Pre-Process function to generate Sensor specific SPI Message Header. More...
 
void FXLS8962_SPI_WritePreprocess (void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
 The SPI Write Pre-Process function to generate Sensor specific SPI Message Header. More...
 
int32_t FXLS8962_SPI_Initialize (fxls8962_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSlaveSelect, uint8_t *whoami)
 The interface function to initialize the sensor. More...
 
void FXLS8962_SPI_SetIdleTask (fxls8962_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
 : The interface function to set the SPI Idle Task. More...
 
int32_t FXLS8962_SPI_Configure (fxls8962_spi_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
 The interface function to configure he sensor. More...
 
int32_t FXLS8962_SPI_ReadData (fxls8962_spi_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
 The interface function to read the sensor data. More...
 
int32_t FXLS8962_SPI_Deinit (fxls8962_spi_sensorhandle_t *pSensorHandle)
 The interface function to De Initialize sensor.. More...
 
int32_t FXLS8962_I2C_Initialize (fxls8962_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t *whoami)
 The interface function to initialize the sensor. More...
 
void FXLS8962_I2C_SetIdleTask (fxls8962_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
 : The interface function to set the I2C Idle Task. More...
 
int32_t FXLS8962_I2C_Configure (fxls8962_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
 The interface function to configure he sensor. More...
 
int32_t FXLS8962_I2C_ReadData (fxls8962_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
 The interface function to read the sensor data. More...
 
int32_t FXLS8962_I2C_DeInit (fxls8962_i2c_sensorhandle_t *pSensorHandle)
 The interface function to De Initialize sensor.. More...
 

Variables

uint8_t fxls8962_spiRead_CmdBuffer [FXLS8962_SPI_MAX_MSG_SIZE] = {0}
 
uint8_t fxls8962_spiRead_DataBuffer [FXLS8962_SPI_MAX_MSG_SIZE] = {0}
 
uint8_t fxls8962_spiWrite_CmdDataBuffer [FXLS8962_SPI_MAX_MSG_SIZE] = {0}
 

Detailed Description

The fxls8962_drv.c file implements the FXLS8962 sensor driver interfaces.

Definition in file fxls8962_drv.c.

Function Documentation

◆ FXLS8962_I2C_Configure()

int32_t FXLS8962_I2C_Configure ( fxls8962_i2c_sensorhandle_t *  pSensorHandle,
const registerwritelist_t *  pRegWriteList 
)

The interface function to configure he sensor.

This function configure the sensor with requested ODR, Range and registers in the regsiter pair array.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pRegWriteListpointer to the register list.
Constraints:
This can be called any number of times only after FXLS8962_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLS8962_I2C_Configure() returns the status .

Validate for the correct handle and register write list.

Check whether sensor handle is initialized before applying configuration.

Put the device into standby mode so that configuration can be applied.

Apply the Sensor Configuration based on the Register Write List

Put the device into active mode and ready for reading data.

Definition at line 286 of file fxls8962_drv.c.

References fxls8962_i2c_sensorhandle_t::deviceInfo, FXLS8962_SENS_CONFIG1, FXLS8962_SENS_CONFIG1_ACTIVE_ACTIVE, FXLS8962_SENS_CONFIG1_ACTIVE_MASK, FXLS8962_SENS_CONFIG1_ACTIVE_STANDBY, int32_t(), fxls8962_i2c_sensorhandle_t::isInitialized, fxls8962_i2c_sensorhandle_t::pCommDrv, Register_I2C_Write(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, Sensor_I2C_Write(), fxls8962_i2c_sensorhandle_t::slaveAddress, and status.

Referenced by apply_register_write(), main(), perform_selftest(), and process_host_command().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLS8962_I2C_DeInit()

int32_t FXLS8962_I2C_DeInit ( fxls8962_i2c_sensorhandle_t *  pSensorHandle)

The interface function to De Initialize sensor..

This function made sensor in a power safe state and de initialize its handle.

Parameters
[in]pSensorHandlehandle to the sensor.
Constraints:
This can be called only after FXLS8962_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLS8962_I2C_DeInit() returns the status .

Check whether sensor handle is initialized before triggering sensor reset.

Trigger sensor device reset.

De-initialize sensor handle.

Definition at line 360 of file fxls8962_drv.c.

References BOARD_DELAY_ms(), fxls8962_i2c_sensorhandle_t::deviceInfo, FXLS8962_SENS_CONFIG1, FXLS8962_SENS_CONFIG1_RST_MASK, FXLS8962_SENS_CONFIG1_RST_RST, FXLS8962_TBOOT_MAX, int32_t(), fxls8962_i2c_sensorhandle_t::isInitialized, fxls8962_i2c_sensorhandle_t::pCommDrv, Register_I2C_Write(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, fxls8962_i2c_sensorhandle_t::slaveAddress, and status.

Referenced by process_host_command().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLS8962_I2C_Initialize()

int32_t FXLS8962_I2C_Initialize ( fxls8962_i2c_sensorhandle_t *  pSensorHandle,
ARM_DRIVER_I2C *  pBus,
uint8_t  index,
uint16_t  sAddress,
uint8_t *  whoAmi 
)

The interface function to initialize the sensor.

This function initialize the sensor and sensor handle.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pBuspointer to the CMSIS API compatible I2C bus object.
[in]indexthe I2C device number.
[in]sAddressslave address of the device on the bus.
[in]whoamiWHO_AM_I value of the device.
Constraints:
This should be the first API to be called. Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLS8962_I2C_Initialize() returns the status .

Check the input parameters.

Read and store the device's WHO_AM_I.

Initialize the sensor handle.

Definition at line 240 of file fxls8962_drv.c.

References fxls8962_i2c_sensorhandle_t::deviceInfo, registerDeviceInfo_t::deviceInstance, registerDeviceInfo_t::functionParam, FXLS8962_WHO_AM_I, FXLS8962_WHOAMI_VALUE, FXLS8964_WHOAMI_VALUE, FXLS8967_WHOAMI_VALUE, FXLS8974_WHOAMI_VALUE, registerDeviceInfo_t::idleFunction, int32_t(), fxls8962_i2c_sensorhandle_t::isInitialized, fxls8962_i2c_sensorhandle_t::pCommDrv, Register_I2C_Read(), SENSOR_ERROR_BAD_ADDRESS, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, fxls8962_i2c_sensorhandle_t::slaveAddress, and status.

Referenced by main(), and process_host_command().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLS8962_I2C_ReadData()

int32_t FXLS8962_I2C_ReadData ( fxls8962_i2c_sensorhandle_t *  pSensorHandle,
const registerreadlist_t *  pReadList,
uint8_t *  pBuffer 
)

The interface function to read the sensor data.

This function read the sensor data out from the device and returns raw data in a byte stream.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pReadListpointer to the list of device registers and values to read.
[out]pBufferbuffer which holds raw sensor data.This buffer may be back to back databuffer based command read in the list.
Constraints:
This can be called any number of times only after FXLS8962_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLS8962_I2C_ReadData() returns the status .

Validate for the correct handle and register read list.

Check whether sensor handle is initialized before reading sensor data.

Parse through the read list and read the data one by one.

Definition at line 331 of file fxls8962_drv.c.

References fxls8962_i2c_sensorhandle_t::deviceInfo, int32_t(), fxls8962_i2c_sensorhandle_t::isInitialized, fxls8962_i2c_sensorhandle_t::pCommDrv, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_READ, Sensor_I2C_Read(), fxls8962_i2c_sensorhandle_t::slaveAddress, and status.

Referenced by apply_register_read(), apply_register_readall(), main(), and perform_selftest().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLS8962_I2C_SetIdleTask()

void FXLS8962_I2C_SetIdleTask ( fxls8962_i2c_sensorhandle_t *  pSensorHandle,
registeridlefunction_t  idleTask,
void *  userParam 
)

: The interface function to set the I2C Idle Task.

Parameters
[in]fxls8962_i2c_sensorhandle_t *pSensorHandle, handle to the sensor handle.
[in]registeridlefunction_t idleTask, function pointer to the function to execute on I2C Idle Time.
[in]void *userParam, the pointer to the user idle ftask parameters.
Returns
void.
Constraints:
This can be called any number of times only after FXLS8962_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No

Definition at line 278 of file fxls8962_drv.c.

References fxls8962_i2c_sensorhandle_t::deviceInfo, registerDeviceInfo_t::functionParam, and registerDeviceInfo_t::idleFunction.

Referenced by main().

Here is the caller graph for this function:

◆ FXLS8962_SPI_Configure()

int32_t FXLS8962_SPI_Configure ( fxls8962_spi_sensorhandle_t *  pSensorHandle,
const registerwritelist_t *  pRegWriteList 
)

The interface function to configure he sensor.

This function configure the sensor with requested ODR, Range and registers in the regsiter pair array.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pRegWriteListpointer to the register list.
Constraints:
This can be called any number of times only after FXLS8962_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLS8962_SPI_Configure() returns the status .

Validate for the correct handle and register write list.

Check whether sensor handle is initialized before applying configuration.

Put the device into standby mode so that configuration can be applied.

Apply the Sensor Configuration based on the Register Write List

Put the device into active mode and ready for reading data.

Definition at line 131 of file fxls8962_drv.c.

References fxls8962_spi_sensorhandle_t::deviceInfo, FXLS8962_SENS_CONFIG1, FXLS8962_SENS_CONFIG1_ACTIVE_ACTIVE, FXLS8962_SENS_CONFIG1_ACTIVE_MASK, FXLS8962_SENS_CONFIG1_ACTIVE_STANDBY, int32_t(), fxls8962_spi_sensorhandle_t::isInitialized, fxls8962_spi_sensorhandle_t::pCommDrv, Register_SPI_Write(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, Sensor_SPI_Write(), fxls8962_spi_sensorhandle_t::slaveParams, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLS8962_SPI_Deinit()

int32_t FXLS8962_SPI_Deinit ( fxls8962_spi_sensorhandle_t *  pSensorHandle)

The interface function to De Initialize sensor..

This function made sensor in a power safe state and de initialize its handle.

Parameters
[in]pSensorHandlehandle to the sensor.
Constraints:
This can be called only after after FXLS8962_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLS8962_SPI_Deinit() returns the status .

Check whether sensor handle is initialized before triggering sensor reset.

Trigger sensor device reset.

De-initialize sensor handle.

Definition at line 205 of file fxls8962_drv.c.

References BOARD_DELAY_ms(), fxls8962_spi_sensorhandle_t::deviceInfo, FXLS8962_SENS_CONFIG1, FXLS8962_SENS_CONFIG1_RST_MASK, FXLS8962_SENS_CONFIG1_RST_RST, FXLS8962_TBOOT_MAX, int32_t(), fxls8962_spi_sensorhandle_t::isInitialized, fxls8962_spi_sensorhandle_t::pCommDrv, Register_SPI_Write(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, fxls8962_spi_sensorhandle_t::slaveParams, and status.

Here is the call graph for this function:

◆ FXLS8962_SPI_Initialize()

int32_t FXLS8962_SPI_Initialize ( fxls8962_spi_sensorhandle_t *  pSensorHandle,
ARM_DRIVER_SPI *  pBus,
uint8_t  index,
void *  pSlaveSelect,
uint8_t *  whoAmi 
)

The interface function to initialize the sensor.

This function initializes the sensor and sensor handle.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pBuspointer to the CMSIS API compatible SPI bus object.
[in]indexthe I2C device number.
[in]pSlaveSelectslave select hndle of the device on the bus.
[in]whoamiWHO_AM_I value of the device.
Constraints:
This should be the first API to be called. Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLS8962_SPI_Initialize() returns the status .

Check the input parameters.

Initialize the sensor handle.

Read and store the device's WHO_AM_I.

Definition at line 68 of file fxls8962_drv.c.

References GENERIC_DRIVER_GPIO::clr_pin, fxls8962_spi_sensorhandle_t::deviceInfo, registerDeviceInfo_t::deviceInstance, Driver_GPIO_KSDK, registerDeviceInfo_t::functionParam, FXLS8962_SPI_CMD_LEN, FXLS8962_SPI_ReadPreprocess(), FXLS8962_SPI_WritePreprocess(), FXLS8962_SS_ACTIVE_VALUE, FXLS8962_WHO_AM_I, FXLS8962_WHOAMI_VALUE, FXLS8964_WHOAMI_VALUE, FXLS8967_WHOAMI_VALUE, FXLS8974_WHOAMI_VALUE, GPIO_DIRECTION_OUT, registerDeviceInfo_t::idleFunction, int32_t(), fxls8962_spi_sensorhandle_t::isInitialized, fxls8962_spi_sensorhandle_t::pCommDrv, pGPIODriver, GENERIC_DRIVER_GPIO::pin_init, spiSlaveSpecificParams_t::pReadPreprocessFN, spiSlaveSpecificParams_t::pTargetSlavePinID, spiSlaveSpecificParams_t::pWritePreprocessFN, Register_SPI_Read(), SENSOR_ERROR_BAD_ADDRESS, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, GENERIC_DRIVER_GPIO::set_pin, fxls8962_spi_sensorhandle_t::slaveParams, SPI_SS_ACTIVE_LOW, spiSlaveSpecificParams_t::spiCmdLen, spiSlaveSpecificParams_t::ssActiveValue, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLS8962_SPI_ReadData()

int32_t FXLS8962_SPI_ReadData ( fxls8962_spi_sensorhandle_t *  pSensorHandle,
const registerreadlist_t *  pReadList,
uint8_t *  pBuffer 
)

The interface function to read the sensor data.

This function read the sensor data out from the device and returns raw data in a byte stream.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pReadListpointer to the list of device registers and values to read.
[out]pBufferbuffer which holds raw sensor data.This buffer may be back to back databuffer based command read in the list.
Constraints:
This can be called any number of times only after FXLS8962_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
FXLS8962_SPI_ReadData() returns the status .

Validate for the correct handle and register read list.

Check whether sensor handle is initialized before reading sensor data.

Parse through the read list and read the data one by one.

Definition at line 176 of file fxls8962_drv.c.

References fxls8962_spi_sensorhandle_t::deviceInfo, int32_t(), fxls8962_spi_sensorhandle_t::isInitialized, fxls8962_spi_sensorhandle_t::pCommDrv, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_READ, Sensor_SPI_Read(), fxls8962_spi_sensorhandle_t::slaveParams, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ FXLS8962_SPI_ReadPreprocess()

void FXLS8962_SPI_ReadPreprocess ( void *  pCmdOut,
uint32_t  offset,
uint32_t  size 
)

The SPI Read Pre-Process function to generate Sensor specific SPI Message Header.

This function prepares the SPI Read Command Header with register address and R/W bit encoded as the Sensor.

Parameters
[out]pCmdOuthandle to the output buffer.
[in]offsetthe address of the register to start reading from.
[in]sizenumber of bytes to read.
Constraints:
None Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
:: None.

Definition at line 31 of file fxls8962_drv.c.

References FXLS8962_SPI_CMD_LEN, fxls8962_spiRead_CmdBuffer, fxls8962_spiRead_DataBuffer, spi_mater_SlaveCmd::pReadBuffer, spi_mater_SlaveCmd::pWriteBuffer, and spi_mater_SlaveCmd::size.

Referenced by FXLS8962_SPI_Initialize().

Here is the caller graph for this function:

◆ FXLS8962_SPI_SetIdleTask()

void FXLS8962_SPI_SetIdleTask ( fxls8962_spi_sensorhandle_t *  pSensorHandle,
registeridlefunction_t  idleTask,
void *  userParam 
)

: The interface function to set the SPI Idle Task.

Parameters
[in]fxls8962_spi_sensorhandle_t *pSensorHandle, handle to the sensor handle.
[in]registeridlefunction_t idleTask, function pointer to the function to execute on SPI Idle Time.
[in]void *userParam, the pointer to the user idle ftask parameters.
Returns
void.
Constraints:
This can be called any number of times only after FXLS8962_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No

Definition at line 123 of file fxls8962_drv.c.

References fxls8962_spi_sensorhandle_t::deviceInfo, registerDeviceInfo_t::functionParam, and registerDeviceInfo_t::idleFunction.

Referenced by main().

Here is the caller graph for this function:

◆ FXLS8962_SPI_WritePreprocess()

void FXLS8962_SPI_WritePreprocess ( void *  pCmdOut,
uint32_t  offset,
uint32_t  size,
void *  pWritebuffer 
)

The SPI Write Pre-Process function to generate Sensor specific SPI Message Header.

This function prepares the SPI Write Command Header with register address and R/W bit encoded as the Sensor.

Parameters
[out]pCmdOuthandle to the output buffer.
[in]offsetthe address of the register to start writing from.
[in]sizenumber of bytes to write.
Constraints:
None Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
:: None.

Definition at line 48 of file fxls8962_drv.c.

References FXLS8962_SPI_CMD_LEN, fxls8962_spiWrite_CmdDataBuffer, spi_mater_SlaveCmd::pReadBuffer, spi_mater_SlaveCmd::pWriteBuffer, and spi_mater_SlaveCmd::size.

Referenced by FXLS8962_SPI_Initialize().

Here is the caller graph for this function:

Variable Documentation

◆ fxls8962_spiRead_CmdBuffer

uint8_t fxls8962_spiRead_CmdBuffer[FXLS8962_SPI_MAX_MSG_SIZE] = {0}

Definition at line 24 of file fxls8962_drv.c.

Referenced by FXLS8962_SPI_ReadPreprocess().

◆ fxls8962_spiRead_DataBuffer

uint8_t fxls8962_spiRead_DataBuffer[FXLS8962_SPI_MAX_MSG_SIZE] = {0}

Definition at line 25 of file fxls8962_drv.c.

Referenced by FXLS8962_SPI_ReadPreprocess().

◆ fxls8962_spiWrite_CmdDataBuffer

uint8_t fxls8962_spiWrite_CmdDataBuffer[FXLS8962_SPI_MAX_MSG_SIZE] = {0}

Definition at line 26 of file fxls8962_drv.c.

Referenced by FXLS8962_SPI_WritePreprocess().