19 #include "clock_config.h" 21 #include "fsl_debug_console.h" 26 #include "issdk_hal.h" 27 #include "gpio_driver.h" 33 #include "Driver_SPI.h" 89 PRINTF(
"\r\n ISSDK FXLS8471Q sensor driver example demonstration with fifo mode\r\n");
93 if (ARM_DRIVER_OK != status)
95 PRINTF(
"\r\n SPI Initialization Failed\r\n");
100 status = pSPIdriver->PowerControl(ARM_POWER_FULL);
101 if (ARM_DRIVER_OK != status)
103 PRINTF(
"\r\n SPI Power Mode setting Failed\r\n");
109 status = pSPIdriver->Control(ARM_SPI_MODE_MASTER | ARM_SPI_CPOL1_CPHA0,
SPI_S_BAUDRATE);
111 status = pSPIdriver->Control(ARM_SPI_MODE_MASTER | ARM_SPI_SS_MASTER_HW_OUTPUT,
SPI_S_BAUDRATE);
113 if (ARM_DRIVER_OK != status)
115 PRINTF(
"\r\n SPI Control Mode setting Failed\r\n");
124 PRINTF(
"\r\n FXLS8471Q Sensor Initialization Failed\r\n");
127 PRINTF(
"\r\n Successfully Initiliazed FXLS8471Q Sensor\r\n");
136 PRINTF(
"\r\n FXLS8471Q Sensor Configuration Failed, Err = %d\r\n", status);
139 PRINTF(
"\r\n Successfully Applied FXLS8471Q Sensor Configuration\r\n");
152 if (ARM_DRIVER_OK != status)
154 PRINTF(
"\r\nRead Failed.\r\n");
163 rawData.
accel[0] /= 4;
166 rawData.
accel[1] /= 4;
169 rawData.
accel[2] /= 4;
172 PRINTF(
"\r\n Accel X = %d Y = %d Z = %d \r\n", rawData.
accel[0], rawData.
accel[1], rawData.
accel[2]);
const registerwritelist_t cFxls8471q_Config_with_Fifo[]
This defines the sensor specific information for SPI.
#define FIFO_SIZE
The watermark value configured for FXLS8471Q FIFO Buffer.
#define FXLS8471Q_F_SETUP_F_WMRK_MASK
This structure defines the Write command List.
#define ASK_USER_TO_RESUME(x)
int32_t FXLS8471Q_SPI_Initialize(fxls8471q_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSlaveSelect, uint8_t whoAmi)
The interface function to initialize the sensor for I2C.
int32_t FXLS8471Q_SPI_ReadData(fxls8471q_spi_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
#define FXLS8471Q_F_STATUS_F_WMRK_FLAG_MASK
#define FXLS8471Q_ACCEL_DATA_SIZE
The size of the FXLS8471Q accel data.
The fxls8471q_drv.h file describes the fxls8471q driver interface and structures. ...
void FXLS8471Q_SPI_SetIdleTask(fxls8471q_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the SPI Idle Task.
#define __END_WRITE_DATA__
#define FXLS8471Q_WHO_AM_I_WHOAMI_VALUE
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
#define SPI_S_BAUDRATE
Transfer baudrate - 500k.
#define SPI_S_DEVICE_INDEX
const registerreadlist_t cFxls8471q_Fifo_Event[]
#define FXLS8471Q_F_SETUP_F_MODE_FIFOSTOP
#define BOARD_BootClockRUN
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
This structure defines the fxls8471q raw data buffer.
int main(void)
This is the The main function implementation.
uint8_t data[FXLS8962_DATA_SIZE]
#define FXLS8471Q_CTRL_REG1_DR_12DOT5HZ
#define __END_READ_DATA__
#define FXLS8471Q_F_SETUP_F_WMRK_SHIFT
fxos8700_accelmagdata_t rawData
#define FXLS8471Q_CTRL_REG1_DR_MASK
This structure defines the Read command List.
const registerreadlist_t cFxls8471q_Output_Values[]
#define SPI_S_SIGNAL_EVENT
#define FXLS8471Q_F_SETUP_F_MODE_MASK
void BOARD_InitDebugConsole(void)
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
int32_t FXLS8471Q_SPI_Configure(fxls8471q_spi_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.