20 #include "clock_config.h"    21 #include "fsl_debug_console.h"    26 #include "issdk_hal.h"    27 #include "gpio_driver.h"    33 #include "Driver_SPI.h"    38 #define RAW_ACCELMAG_DATA_SIZE (12)    82     PRINTF(
"\r\n ISSDK FXOS8700 sensor driver example demonstration for SPI with Poll Mode.\r\n");
    86     if (ARM_DRIVER_OK != status)
    88         PRINTF(
"\r\n SPI Initialization Failed\r\n");
    93     status = pSPIdriver->PowerControl(ARM_POWER_FULL);
    94     if (ARM_DRIVER_OK != status)
    96         PRINTF(
"\r\n SPI Power Mode setting Failed\r\n");
   101     status = pSPIdriver->Control(ARM_SPI_MODE_MASTER | ARM_SPI_CPOL0_CPHA0, 
SPI_S_BAUDRATE);
   102     if (ARM_DRIVER_OK != status)
   104         PRINTF(
"\r\n SPI Control Mode setting Failed\r\n");
   113         PRINTF(
"\r\n Sensor Initialization Failed\r\n");
   116     PRINTF(
"\r\n Successfully Initiliazed Sensor\r\n");
   125         PRINTF(
"\r\n FXOS8700 Sensor Configuration Failed, Err = %d\r\n", status);
   128     PRINTF(
"\r\n Successfully Applied FXOS8700 Sensor Configuration\r\n");
   141         if (ARM_DRIVER_OK != status)
   143             PRINTF(
"\r\n Read Failed. \r\n");
   148         rawData.
accel[0] = ((uint16_t)data[0] << 8) | data[1];
   149         rawData.
accel[0] /= 4;
   150         rawData.
accel[1] = ((uint16_t)data[2] << 8) | data[3];
   151         rawData.
accel[1] /= 4;
   152         rawData.
accel[2] = ((uint16_t)data[4] << 8) | data[5];
   153         rawData.
accel[2] /= 4;
   154         rawData.
mag[0] = ((uint16_t)data[6] << 8) | data[7];
   155         rawData.
mag[1] = ((uint16_t)data[8] << 8) | data[9];
   156         rawData.
mag[2] = ((uint16_t)data[10] << 8) | data[11];
   159         PRINTF(
"\r\n Accel X = %d  Y = %d  Z = %d \r\n", rawData.
accel[0], rawData.
accel[1], rawData.
accel[2]);
   160         PRINTF(
"\r\n Mag   X = %d  Y = %d  Z = %d \r\n", rawData.
mag[0], rawData.
mag[1], rawData.
mag[2]);
 This structure defines the fxos8700 raw data buffer. 
 
This structure defines the Write command List. 
 
#define FXOS8700_M_CTRL_REG2_M_AUTOINC_MASK
 
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
 
#define FXOS8700_M_CTRL_REG1_M_HMS_MASK
 
#define FXOS8700_WHO_AM_I_PROD_VALUE
 
#define FXOS8700_CTRL_REG1_DR_MASK
 
#define FXOS8700_M_CTRL_REG1_M_HMS_HYBRID_MODE
 
#define FXOS8700_CTRL_REG1_DR_SINGLE_12P5_HZ
 
#define __END_WRITE_DATA__
 
#define FXOS8700_M_CTRL_REG2_M_AUTOINC_HYBRID_MODE
 
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream. 
 
#define SPI_S_BAUDRATE
Transfer baudrate - 500k. 
 
#define SPI_S_DEVICE_INDEX
 
#define RAW_ACCELMAG_DATA_SIZE
 
int32_t FXOS8700_SPI_Initialize(fxos8700_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSlaveSelect, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
#define BOARD_BootClockRUN
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
int32_t FXOS8700_SPI_ReadData(fxos8700_spi_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
#define FXOS8700_M_CTRL_REG1_M_ACAL_EN
 
#define FXOS8700_M_CTRL_REG1_M_ACAL_MASK
 
This defines the sensor specific information for SPI. 
 
uint8_t data[FXLS8962_DATA_SIZE]
 
#define __END_READ_DATA__
 
const registerwritelist_t fxos8700_Config_Hybrid[]
 
int32_t FXOS8700_SPI_Configure(fxos8700_spi_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
void FXOS8700_SPI_SetIdleTask(fxos8700_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the SPI Idle Task. 
 
fxos8700_accelmagdata_t rawData
 
#define FXOS8700_M_CTRL_REG2_M_RST_CNT_DISABLE
 
#define FXOS8700_M_CTRL_REG2_M_RST_CNT_MASK
 
The fxos8700_drv.h file describes the fxos8700 driver interface and structures. 
 
This structure defines the Read command List. 
 
#define SPI_S_SIGNAL_EVENT
 
int main(void)
Main function. 
 
void BOARD_InitDebugConsole(void)
 
const registerreadlist_t FXOS8700_STATUS_READ[]
 
#define FXOS8700_DR_STATUS_ZYXDR_MASK
 
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features. 
 
const registerreadlist_t FXOS8700_ACCELMAG_READ[]