![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The mma865x_poll.c file implements the ISSDK MMA865x sensor driver example demonstration with Normal mode. More...
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_debug_console.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "mma865x_drv.h"
Go to the source code of this file.
Macros | |
| #define | MMA865x_ACCEL_DATA_SIZE (6) /* 2 byte X,Y,Z Axis Data each. */ |
Functions | |
| int | main (void) |
| Main function. More... | |
Variables | |
| const registerwritelist_t | cMma865xConfigNormal [] |
| const registerreadlist_t | cMma865xDataReady [] = {{.readFrom = MMA865x_STATUS, .numBytes = 1}, __END_READ_DATA__} |
| const registerreadlist_t | cMma865xOutputValues [] |
The mma865x_poll.c file implements the ISSDK MMA865x sensor driver example demonstration with Normal mode.
Definition in file mma865x_poll.c.
| #define MMA865x_ACCEL_DATA_SIZE (6) /* 2 byte X,Y,Z Axis Data each. */ |
Definition at line 35 of file mma865x_poll.c.
Referenced by main().
| int main | ( | void | ) |
Main function.
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize the MMA865x sensor driver.
Set the task to be executed while waiting for I2C transactions to complete.
Configure the MMA865x sensor driver with Normal mode.
Wait for data ready from the MMA865x.
Read the raw sensor data from the MMA865x.
Convert the raw sensor data to signed 16-bit container for display to the debug port.
Definition at line 63 of file mma865x_poll.c.
References mma865x_acceldata_t::accel, ASK_USER_TO_RESUME, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), data, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, I2Cdrv, int32_t(), MMA8652_I2C_ADDR, MMA8652_WHOAMI_VALUE, MMA865x_ACCEL_DATA_SIZE, MMA865x_I2C_Configure(), MMA865x_I2C_Initialize(), MMA865x_I2C_ReadData(), MMA865x_I2C_SetIdleTask(), MMA865x_STATUS_ZYXDR_MASK, rawData, SENSOR_ERROR_NONE, SMC, SMC_SetPowerModeVlpr(), and status.

| const registerwritelist_t cMma865xConfigNormal[] |
Prepare the register write list to configure MMA865x in Normal mode.
Definition at line 41 of file mma865x_poll.c.
| const registerreadlist_t cMma865xDataReady[] = {{.readFrom = MMA865x_STATUS, .numBytes = 1}, __END_READ_DATA__} |
Prepare the register read list to read the Data Ready Status from MMA865x.
Definition at line 51 of file mma865x_poll.c.
| const registerreadlist_t cMma865xOutputValues[] |
Prepare the register read list to read the raw Accel data from MMA865x.
Definition at line 54 of file mma865x_poll.c.