![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The fxls896xaf_spi.c file implements the ISSDK FXLS896xAF SPI sensor driver example demonstration for SPI Mode with polling. More...
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_debug_console.h"#include "issdk_hal.h"#include "gpio_driver.h"#include "fxls896x_drv.h"#include "systick_utils.h"#include "Driver_SPI.h"
Go to the source code of this file.
Macros | |
| #define | FXLS896x_DATA_SIZE (6) |
Functions | |
| int | main (void) |
| This is the The main function implementation. More... | |
Variables | |
| const registerwritelist_t | cFxls896xConfigNormal [] |
| Register settings for Normal (non buffered) mode. More... | |
| const registerreadlist_t | cFxls896xDRDYEvent [] = {{.readFrom = FXLS896x_INT_STATUS, .numBytes = 1}, __END_READ_DATA__} |
| Address of DATA Ready Status Register. More... | |
| const registerreadlist_t | cFxls896xOutputNormal [] |
| Address of Raw Accel Data in Normal Mode. More... | |
The fxls896xaf_spi.c file implements the ISSDK FXLS896xAF SPI sensor driver example demonstration for SPI Mode with polling.
Definition in file fxls896xaf_spi.c.
| #define FXLS896x_DATA_SIZE (6) |
Definition at line 38 of file fxls896xaf_spi.c.
Referenced by main().
| int main | ( | void | ) |
This is the The main function implementation.
This function invokes board initializes routines, then then brings up the sensor and finally enters an endless loop to continuously read available samples.
| [in] | void | This is no input parameter. |
Initialize the MCU hardware.
Initialize the SPI driver.
Set the SPI Power mode.
Set the SPI Slave speed.
Initialize the fxls896x sensor driver.
Set the task to be executed while waiting for SPI transactions to complete.
Configure the FXLS896x sensor driver.
Wait for data ready from the FXLS896x.
Read the raw sensor data from the FXLS896x.
Convert the raw sensor data for display to the debug port.
Definition at line 70 of file fxls896xaf_spi.c.
References fxls896x_acceldata_t::accel, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), BOARD_SystickEnable(), data, FXLS8962_WHOAMI_VALUE, FXLS8964_WHOAMI_VALUE, FXLS8967_WHOAMI_VALUE, FXLS8968_WHOAMI_VALUE, FXLS896x_CS, FXLS896x_DATA_SIZE, FXLS896x_INT_STATUS_SRC_DRDY_MASK, FXLS896x_SPI_Configure(), FXLS896x_SPI_Initialize(), FXLS896x_SPI_ReadData(), FXLS896x_SPI_SetIdleTask(), fxls896xDriver, FXLS8974_WHOAMI_VALUE, gFxls896xDataReady, int32_t(), rawData, SENSOR_ERROR_NONE, SMC, SMC_SetPowerModeVlpr(), SPI_S_BAUDRATE, SPI_S_DEVICE_INDEX, SPI_S_DRIVER, SPI_S_SIGNAL_EVENT, and status.

| const registerwritelist_t cFxls896xConfigNormal[] |
Register settings for Normal (non buffered) mode.
Definition at line 44 of file fxls896xaf_spi.c.
| const registerreadlist_t cFxls896xDRDYEvent[] = {{.readFrom = FXLS896x_INT_STATUS, .numBytes = 1}, __END_READ_DATA__} |
Address of DATA Ready Status Register.
Definition at line 52 of file fxls896xaf_spi.c.
| const registerreadlist_t cFxls896xOutputNormal[] |
Address of Raw Accel Data in Normal Mode.
Definition at line 55 of file fxls896xaf_spi.c.