![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The pedometer_stepcount_mma8652.c file implements the ISSDK prdometer example using MMA8652 sensor as the acceleration source. More...
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_debug_console.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "pedometer.h"#include "mma865x_drv.h"
Go to the source code of this file.
Macros | |
| #define | MMA865x_ACCEL_DATA_SIZE (6) /* 2 byte X,Y,Z Axis Data each. */ |
Functions | |
| int | main (void) |
| Main function. More... | |
Variables | |
| const registerwritelist_t | cMma865xConfigNormal [] |
| const registerreadlist_t | cMma865xDataReady [] = {{.readFrom = MMA865x_STATUS, .numBytes = 1}, __END_READ_DATA__} |
| const registerreadlist_t | cMma865xOutputValues [] |
The pedometer_stepcount_mma8652.c file implements the ISSDK prdometer example using MMA8652 sensor as the acceleration source.
The pedometer_stepcount_mma8652.c file implements the ISSDK MMA8652 sensor driver example demonstration for Motion Activated Pedometer.
Definition in file pedometer_stepcount_mma8652.c.
| #define MMA865x_ACCEL_DATA_SIZE (6) /* 2 byte X,Y,Z Axis Data each. */ |
Definition at line 32 of file pedometer_stepcount_mma8652.c.
Referenced by main().
| int main | ( | void | ) |
Main function.
Initialize the MCU hardware
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize the MMA865x sensor driver.
Set the task to be executed while waiting for I2C transactions to complete.
Configure the MMA865x sensor driver with Non FIFO mode.
Initialize the pedometer
Configure the pedometer
Read the data ready status from MMA865x
Read the raw sensor data from the MMA865x.
Convert the raw sensor data for display to the debug port.
Execute the pedometer Algorithm
Definition at line 84 of file pedometer_stepcount_mma8652.c.
References mma865x_acceldata_t::accel, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), data, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, I2Cdrv, int32_t(), MMA8652_I2C_ADDR, MMA8652_WHOAMI_VALUE, MMA865x_ACCEL_DATA_SIZE, MMA865x_I2C_Configure(), MMA865x_I2C_Initialize(), MMA865x_I2C_ReadData(), MMA865x_I2C_SetIdleTask(), MMA865x_STATUS_ZYXDR_MASK, pedometer_configure(), pedometer_init(), pedometer_run(), rawData, SENSOR_ERROR_NONE, SMC, SMC_SetPowerModeVlpr(), pedometer_t::status, status, and pedometer_t::pedometer_status_tag::stepcount.

| const registerwritelist_t cMma865xConfigNormal[] |
Prepare the register write list to configure MMA865x in Normal mode.
Definition at line 38 of file pedometer_stepcount_mma8652.c.
| const registerreadlist_t cMma865xDataReady[] = {{.readFrom = MMA865x_STATUS, .numBytes = 1}, __END_READ_DATA__} |
Prepare the register read list to read the Data Ready Status from MMA865x.
Definition at line 48 of file pedometer_stepcount_mma8652.c.
| const registerreadlist_t cMma865xOutputValues[] |
Prepare the register read list to read the raw Accel data from MMA865x.
Definition at line 51 of file pedometer_stepcount_mma8652.c.