45 #include "clock_config.h" 46 #include "fsl_debug_console.h" 51 #include "Driver_I2C.h" 54 #include "issdk_hal.h" 61 #define DIFF_P_DATA_SIZE (3) 93 float pressureInPascals;
95 uint8_t whoAmI, conversionFactor;
106 PRINTF(
"\r\n ISSDK DIFF-P Sensor Example !\r\n");
110 if (ARM_DRIVER_OK != status)
112 PRINTF(
"\r\n I2C Initialization Failed.\r\n");
117 status = I2Cdrv->PowerControl(ARM_POWER_FULL);
118 if (ARM_DRIVER_OK != status)
120 PRINTF(
"\r\n I2C Power Mode setting Failed.\r\n");
125 status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
126 if (ARM_DRIVER_OK != status)
128 PRINTF(
"\r\n I2C Control Mode setting Failed.\r\n");
167 PRINTF(
"\r\n Sensor Initialization Failed.\r\n");
170 PRINTF(
"\r\n Initiliazed Sensor with WHO_AM_I = [0x%X].\r\n", whoAmI);
179 PRINTF(
"\r\nDIFF_P now active and entering data read loop...\r\n");
182 PRINTF(
"\r\n Successfully Applied Sensor Poll Configuration.\r\n");
188 if (ARM_DRIVER_OK != status)
190 PRINTF(
"\r\n Read Failed. \r\n");
203 if (ARM_DRIVER_OK != status)
205 PRINTF(
"\r\n Read Failed. \r\n");
211 cDiffPClearStatusBits);
212 if (ARM_DRIVER_OK != status)
214 PRINTF(
"\r\n Write Failed. \r\n");
219 rawData.
pressure = ((int16_t)(data[1]) << 8) | data[0];
220 pressureInPascals = (1.0 * rawData.
pressure) / conversionFactor;
225 PRINTF(
"\r\n Pressure = %0.3f Pa", pressureInPascals);
226 PRINTF(
"\r\n Temperature = %d degC\r\n", tempInDegrees);
This defines the sensor specific information for I2C.
void DIFF_P_I2C_SetIdleTask(diff_p_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
const registerwritelist_t cDiffPConfigNormal[]
Register settings for Normal Mode.
#define __END_WRITE_DATA__
#define DIFF_P_CTRL_REG2_ODR_MASK
int32_t DIFF_P_I2C_Configure(diff_p_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
#define BOARD_BootClockRUN
#define DIFF_P_INT_STATUS_0_PDR_DRDY
#define NPS3002VV_PRESSURE_DIV_FACTOR
#define DIFF_P_CTRL_REG1_OSR_MASK
uint8_t data[FXLS8962_DATA_SIZE]
int32_t DIFF_P_I2C_ReadData(diff_p_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
void BOARD_InitDebugConsole(void)
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
int main(void)
Main function.
#define DIFF_P_NPS3001DV_WHOAMI_VALUE
#define DIFF_P_CTRL_REG2_ODR_ODR6P25
#define __END_READ_DATA__
registerDeviceInfo_t deviceInfo
int32_t DIFF_P_I2C_Initialize(diff_p_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
The diff_p_drv.h file describes the DIFF_P driver interface and structures.
#define DIFF_P_INT_STATUS_0_PDR_MASK
#define DIFF_P_CTRL_REG1_OSR_OSR512
#define NPS3001DV_PRESSURE_DIV_FACTOR
const registerreadlist_t cDiffPOutputNormal[]
Address and size of Raw Pressure+Temperature Data in Normal Mode.
#define ASK_USER_TO_RESUME(x)
#define NPS3005DV_PRESSURE_DIV_FACTOR
void BOARD_SystickEnable(void)
Function to enable systicks framework.
#define I2C_S_DEVICE_INDEX
#define DIFF_P_INT_STATUS_0_TDR_MASK
#define DIFF_P_NPS3000VV_WHOAMI_VALUE
This structure defines the diff_p data buffer in Pressure Mode.
const registerreadlist_t cDiffPStatus[]
Address of Status Register.
ARM_DRIVER_I2C * pCommDrv
#define NPS3000VV_PRESSURE_DIV_FACTOR
fxls8962_acceldataUser_t rawData
#define DIFF_P_NPS3002VV_WHOAMI_VALUE
This structure defines the Write command List.
This structure defines the Read command List.
const registerwritelist_t cDiffPClearStatusBits[]
Register settings for Clearing Pressure and Temperature Data Ready Bits.
#define DIFF_P_NPS3005DV_WHOAMI_VALUE
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
#define DIFF_P_INT_STATUS_0_TDR_DRDY
#define I2C_S_SIGNAL_EVENT
int32_t Sensor_I2C_Write(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerwritelist_t *pRegWriteList)
Write register data to a sensor.