45 #include "clock_config.h" 46 #include "fsl_debug_console.h" 51 #include "Driver_I2C.h" 54 #include "issdk_hal.h" 62 #define P_TGT0_MSB 0x03 63 #define P_TGT0_LSB 0x20 112 uint16_t thresholdValue;
113 uint8_t whoAmI, conversionFactor, dataReady;
124 PRINTF(
"\r\n ISSDK DIFF-P Sensor Example !\r\n");
134 if (ARM_DRIVER_OK != status)
136 PRINTF(
"\r\n I2C Initialization Failed.\r\n");
141 status = I2Cdrv->PowerControl(ARM_POWER_FULL);
142 if (ARM_DRIVER_OK != status)
144 PRINTF(
"\r\n I2C Power Mode setting Failed.\r\n");
149 status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
150 if (ARM_DRIVER_OK != status)
152 PRINTF(
"\r\n I2C Control Mode setting Failed.\r\n");
191 PRINTF(
"\r\n Sensor Initialization Failed.\r\n");
195 PRINTF(
"\r\n Initiliazed Sensor with WHO_AM_I = [0x%X] Threshold = [%dPa].\r\n", whoAmI, thresholdValue);
204 PRINTF(
"\r\nDIFF_P now active and entering data read loop...\r\n");
207 PRINTF(
"\r\n Successfully Applied Sensor Interrupt Configuration.\r\n");
224 if (ARM_DRIVER_OK != status)
226 PRINTF(
"\r\n Read Failed. \r\n");
238 cDiffPClearStatusBits);
239 if (ARM_DRIVER_OK != status)
241 PRINTF(
"\r\n Write Failed. \r\n");
245 PRINTF(
"\r\n Threshold Event... \r\n", conversionFactor);
This defines the sensor specific information for I2C.
void DIFF_P_I2C_SetIdleTask(diff_p_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
#define __END_WRITE_DATA__
#define DIFF_P_CTRL_REG2_ODR_MASK
#define DIFF_P_INT_MASK1_P_TGT0_INT_EN
const registerwritelist_t cDiffPConfigNormal[]
Register settings for Normal (non buffered) mode.
int32_t DIFF_P_I2C_Configure(diff_p_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
#define BOARD_BootClockRUN
#define NPS3002VV_PRESSURE_DIV_FACTOR
int main(void)
Main function.
#define DIFF_P_CTRL_REG1_OSR_MASK
volatile bool diff_pInterrupt
void(* toggle_pin)(pinID_t aPinId)
int32_t DIFF_P_I2C_ReadData(diff_p_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
void BOARD_InitDebugConsole(void)
#define DIFF_P_INT_STATUS_1_P_TGT0_MASK
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
#define DIFF_P_NPS3001DV_WHOAMI_VALUE
const registerwritelist_t cDiffPClearStatusBits[]
Register settings for Clearing Pressure and Temperature Data Ready Bits.
#define DIFF_P_CTRL_REG2_ODR_ODR6P25
#define __END_READ_DATA__
registerDeviceInfo_t deviceInfo
int32_t DIFF_P_I2C_Initialize(diff_p_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
The diff_p_drv.h file describes the DIFF_P driver interface and structures.
#define DIFF_P_CTRL_REG1_OSR_OSR512
#define NPS3001DV_PRESSURE_DIV_FACTOR
#define DIFF_P_INT_STATUS_1_P_TGT0_REACHED
gpioHandleKSDK_t GREEN_LED
void diff_p_isr(void *pUserData)
This is the Sensor Data Ready ISR implementation.
#define NPS3005DV_PRESSURE_DIV_FACTOR
void BOARD_SystickEnable(void)
Function to enable systicks framework.
#define I2C_S_DEVICE_INDEX
#define DIFF_P_NPS3000VV_WHOAMI_VALUE
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
#define DIFF_P_CTRL_REG3_IPOL1_ACTIVE_HIGH
Access structure of the GPIO Driver.
ARM_DRIVER_I2C * pCommDrv
#define NPS3000VV_PRESSURE_DIV_FACTOR
#define DIFF_P_INT_MASK1_P_TGT0_MASK
#define DIFF_P_NPS3002VV_WHOAMI_VALUE
This structure defines the Write command List.
This structure defines the Read command List.
#define DIFF_P_NPS3005DV_WHOAMI_VALUE
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
#define DIFF_P_CTRL_REG3_IPOL1_MASK
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
#define I2C_S_SIGNAL_EVENT
int32_t Sensor_I2C_Write(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerwritelist_t *pRegWriteList)
Write register data to a sensor.
const registerreadlist_t cDiffPStatus[]
Address of Status Register.