46 #include "clock_config.h"    47 #include "fsl_debug_console.h"    52 #include "Driver_I2C.h"    57 #include "issdk_hal.h"    58 #include "gpio_driver.h"    64 #define FXPQ3115_DATA_SIZE (5)     68 #define FXPQ3115_SAMPLING_EXPONENT (1)    127     int16_t tempInDegrees;
   128     uint32_t pressureInPascals;
   142     PRINTF(
"\r\n ISSDK FXPQ3115 sensor driver example demonstration with interrupt mode.\r\n");
   152     if (ARM_DRIVER_OK != status)
   154         PRINTF(
"\r\n I2C Initialization Failed\r\n");
   159     status = I2Cdrv->PowerControl(ARM_POWER_FULL);
   160     if (ARM_DRIVER_OK != status)
   162         PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
   167     status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   168     if (ARM_DRIVER_OK != status)
   170         PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
   179         PRINTF(
"\r\n Sensor Initialization Failed\r\n");
   182     PRINTF(
"\r\n Successfully Initiliazed Sensor\r\n");
   193         PRINTF(
"\r\n FXPQ3115 Sensor Configuration Failed, Err = %d\r\n", status);
   196     PRINTF(
"\r\n Successfully Applied FXPQ3115 Sensor Configuration\r\n");
   214         if (ARM_DRIVER_OK != status)
   216             PRINTF(
"\r\n Read Failed. \r\n");
   221         rawData.
pressure = (uint32_t)((data[0]) << 16) | ((data[1]) << 8) | ((data[2]));
   224         rawData.
temperature = (int16_t)((data[3]) << 8) | (data[4]);
   228         PRINTF(
"\r\nPressure    = %d Pa\r\n", pressureInPascals);
   229         PRINTF(
"\r\nTemperature = %d degC\r\n", tempInDegrees);
 #define FXPQ3115_TEMPERATURE_CONV_FACTOR
 
int main(void)
This is the The main function implementation. 
 
#define FXPQ3115_CTRL_REG1_OS_MASK
 
#define FXPQ3115_CTRL_REG5_INT_CFG_DRDY_MASK
 
#define __END_WRITE_DATA__
 
const registerreadlist_t B3115OutputNormal[]
Address and size of Raw Pressure+Temperature Data in Normal Mode. 
 
volatile uint8_t gB3115DataReady
 
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
 
#define BOARD_BootClockRUN
 
uint8_t data[FXLS8962_DATA_SIZE]
 
This structure defines the fxpq3115 data buffer in Pressure Mode. 
 
void(* toggle_pin)(pinID_t aPinId)
 
int32_t FXPQ3115_I2C_Initialize(fxpq3115_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
#define FXPQ3115_I2C_ADDR
 
void BOARD_InitDebugConsole(void)
 
#define FXPQ3115_PT_DATA_CFG_TDEFE_MASK
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
#define FXPQ3115_CTRL_REG3_IPOL1_MASK
 
#define FXPQ3115_PT_DATA_CFG_PDEFE_ENABLED
 
#define FXPQ3115_WHOAMI_VALUE
 
#define __END_READ_DATA__
 
#define FXPQ3115_CTRL_REG2_ST_MASK
 
GENERIC_DRIVER_GPIO * pGpioDriver
 
#define FXPQ3115_PRESSURE_CONV_FACTOR
 
#define FXPQ3115_CTRL_REG1_OS_OSR_128
 
#define FXPQ3115_CTRL_REG5_INT_CFG_DRDY_INT1
 
#define FXPQ3115_PT_DATA_CFG_DREM_MASK
 
gpioHandleKSDK_t GREEN_LED
 
#define FXPQ3115_CTRL_REG3_IPOL1_HIGH
 
This defines the sensor specific information. 
 
void fxpq3115_int_data_ready_callback(void *pUserData)
This is the Sensor Data Ready ISR implementation. 
 
#define ASK_USER_TO_RESUME(x)
 
void FXPQ3115_I2C_SetIdleTask(fxpq3115_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
#define FXPQ3115_DATA_SIZE
 
#define FXPQ3115_PT_DATA_CFG_DREM_ENABLED
 
#define I2C_S_DEVICE_INDEX
 
const registerwritelist_t B3115ConfigNormal[]
Register settings for Interrupt (non buffered) mode. 
 
#define FXPQ3115_CTRL_REG4_INT_EN_DRDY_MASK
 
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
 
#define FXPQ3115_SAMPLING_EXPONENT
 
#define FXPQ3115_PT_DATA_CFG_PDEFE_MASK
 
Access structure of the GPIO Driver. 
 
int32_t FXPQ3115_I2C_Configure(fxpq3115_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
fxls8962_acceldataUser_t rawData
 
This structure defines the Write command List. 
 
int32_t FXPQ3115_I2C_ReadData(fxpq3115_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
This structure defines the Read command List. 
 
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
 
#define FXPQ3115_CTRL_REG4_INT_EN_DRDY_INTENABLED
 
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features. 
 
#define FXPQ3115_PT_DATA_CFG_TDEFE_ENABLED
 
#define I2C_S_SIGNAL_EVENT
 
The fxpq3115_drv.h file describes the fxpq3115 driver interface and structures.