![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The mma865x_fifo.c file implements the ISSDK MMA865x sensor driver example demonstration with FIFO mode. More...
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_debug_console.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "mma865x_drv.h"
Go to the source code of this file.
Macros | |
| #define | FIFO_WATERMARK (16) /* Must be between 1 - 32 */ |
| #define | MMA865x_ACCEL_DATA_SIZE (6) /* 2 byte X,Y,Z Axis Data each. */ |
Functions | |
| int | main (void) |
| Main function. More... | |
Variables | |
| const registerwritelist_t | cMma865xConfigFifo [] |
| const registerreadlist_t | cMma865xFifoStatus [] = {{.readFrom = MMA865x_F_STATUS, .numBytes = 1}, __END_READ_DATA__} |
| const registerreadlist_t | cMma865xOutputValues [] |
The mma865x_fifo.c file implements the ISSDK MMA865x sensor driver example demonstration with FIFO mode.
Definition in file mma865x_fifo.c.
| #define FIFO_WATERMARK (16) /* Must be between 1 - 32 */ |
Definition at line 36 of file mma865x_fifo.c.
Referenced by main().
| #define MMA865x_ACCEL_DATA_SIZE (6) /* 2 byte X,Y,Z Axis Data each. */ |
Definition at line 37 of file mma865x_fifo.c.
Referenced by main().
| int main | ( | void | ) |
Main function.
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize the MMA865x sensor driver.
Set the task to be executed while waiting for I2C transactions to complete.
Configure the MMA865x sensor driver with FIFO mode.
Wait for data ready from the MMA865x.
Read the raw sensor data from the MMA865x.
Convert the raw sensor data to signed 16-bit container for display to the debug port.
Definition at line 68 of file mma865x_fifo.c.
References mma865x_acceldata_t::accel, ASK_USER_TO_RESUME, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), data, FIFO_WATERMARK, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, I2Cdrv, int32_t(), MMA8652_I2C_ADDR, MMA8652_WHOAMI_VALUE, MMA865x_ACCEL_DATA_SIZE, MMA865x_F_STATUS_F_WMKF_MASK, MMA865x_I2C_Configure(), MMA865x_I2C_Initialize(), MMA865x_I2C_ReadData(), MMA865x_I2C_SetIdleTask(), rawData, SENSOR_ERROR_NONE, SMC, SMC_SetPowerModeVlpr(), and status.

| const registerwritelist_t cMma865xConfigFifo[] |
Prepare the register write list to configure MMA865x in FIFO mode.
Definition at line 43 of file mma865x_fifo.c.
| const registerreadlist_t cMma865xFifoStatus[] = {{.readFrom = MMA865x_F_STATUS, .numBytes = 1}, __END_READ_DATA__} |
Prepare the register read list to read the FIFO Status from MMA865x.
Definition at line 56 of file mma865x_fifo.c.
| const registerreadlist_t cMma865xOutputValues[] |
Prepare the register read list to read the raw Accel data from MMA865x.
Definition at line 59 of file mma865x_fifo.c.