19 #include "clock_config.h" 21 #include "fsl_debug_console.h" 26 #include "Driver_I2C.h" 29 #include "issdk_hal.h" 36 #define FIFO_WATERMARK (16) 37 #define MMA865x_ACCEL_DATA_SIZE (6) 82 PRINTF(
"\r\n ISSDK MMA865x sensor driver example for FIFO Mode. \r\n");
86 if (ARM_DRIVER_OK != status)
88 PRINTF(
"\r\n I2C Initialization Failed\r\n");
93 status = I2Cdrv->PowerControl(ARM_POWER_FULL);
94 if (ARM_DRIVER_OK != status)
96 PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
101 status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
102 if (ARM_DRIVER_OK != status)
104 PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
113 PRINTF(
"\r\n Sensor Initialization Failed\r\n");
116 PRINTF(
"\r\n Successfully Initiliazed Sensor\r\n");
125 PRINTF(
"\r\n MMA865x Sensor Configuration Failed, Err = %d \r\n", status);
128 PRINTF(
"\r\n MMA865x now active and entering data read loop... \r\n");
141 if (ARM_DRIVER_OK != status)
143 PRINTF(
"\r\n Read Failed. \r\n");
152 rawData.
accel[0] /= 16;
155 rawData.
accel[1] /= 16;
158 rawData.
accel[2] /= 16;
162 PRINTF(
"\r\n Accel X = %d Y = %d Z = %d \r\n", rawData.
accel[0], rawData.
accel[1], rawData.
accel[2]);
#define MMA865x_CTRL_REG1_DR_MASK
This structure defines the Write command List.
This defines the sensor specific information.
const registerwritelist_t cMma865xConfigFifo[]
#define ASK_USER_TO_RESUME(x)
#define MMA865x_XYZ_DATA_CFG_FS_MASK
#define MMA865x_F_STATUS_F_WMKF_MASK
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
#define __END_WRITE_DATA__
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
int32_t MMA865x_I2C_ReadData(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
#define I2C_S_SIGNAL_EVENT
#define MMA865x_CTRL_REG2_MODS_MASK
#define BOARD_BootClockRUN
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
#define MMA865x_F_SETUP_F_WMRK_MASK
uint8_t data[FXLS8962_DATA_SIZE]
int32_t MMA865x_I2C_Configure(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
#define __END_READ_DATA__
The mma865x_drv.h file describes the MMA865x driver interface and structures.
const registerreadlist_t cMma865xOutputValues[]
#define MMA865x_F_SETUP_F_MODE_STOP_MODE
fxos8700_accelmagdata_t rawData
const registerreadlist_t cMma865xFifoStatus[]
#define MMA865x_CTRL_REG2_MODS_HR
#define MMA865x_ACCEL_DATA_SIZE
#define MMA865x_XYZ_DATA_CFG_FS_2G
This structure defines the Read command List.
This structure defines the mma865x raw data buffer.
#define I2C_S_DEVICE_INDEX
void MMA865x_I2C_SetIdleTask(mma865x_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
void BOARD_InitDebugConsole(void)
#define MMA8652_WHOAMI_VALUE
int32_t MMA865x_I2C_Initialize(mma865x_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
#define MMA865x_F_SETUP_F_MODE_MASK
int main(void)
Main function.
#define MMA865x_CTRL_REG1_DR_100HZ