![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The mma9553_pedometer_interrupt.c file implements the ISSDK MMA9553L sensor driver example demonstration as a Pedometer in I2C Mode with Interrupts. More...
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_debug_console.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "mma9553_drv.h"#include "gpio_driver.h"#include "systick_utils.h"
Go to the source code of this file.
Macros | |
| #define | MMA9553_ACCEL_DATA_SIZE (6) /* 2 byte X,Y,Z Axis Data each. */ |
| #define | MMA9553_INT_O A0 /* The INT_O pin of MMA9553 on the FRDM-STBC-SA955x Board. */ |
Functions | |
| void | mma9553_int_data_ready_callback (void *pUserData) |
| int | main (void) |
| Main function. More... | |
Variables | |
| const registercommandlist_t | cMma9553Config30Hz [] |
| const registerreadlist_t | cMma9553ReadRawOutput [] |
| const registercommandlist_t | cMma9553ReadPedometerCommand [] |
| const registercommandlist_t | cMma9553EnableInterruptCommand [] |
| const registerreadlist_t | cMma9553ReadPedometerOutput [] |
| volatile bool | gMma9553DataReady |
The mma9553_pedometer_interrupt.c file implements the ISSDK MMA9553L sensor driver example demonstration as a Pedometer in I2C Mode with Interrupts.
Definition in file mma9553_pedometer_interrupt.c.
| #define MMA9553_ACCEL_DATA_SIZE (6) /* 2 byte X,Y,Z Axis Data each. */ |
Definition at line 33 of file mma9553_pedometer_interrupt.c.
Definition at line 34 of file mma9553_pedometer_interrupt.c.
Referenced by main().
| int main | ( | void | ) |
Main function.
Initialize the MCU hardware
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize the MMA9553 sensor driver.
Set the task to be executed while waiting for I2C transactions to complete.
Configure the MMA9553 sensor driver with 30Hz Mode settings.
MMA9553_I2C_Configure sets the part to Legacy Mode. To enable MMA9553_INT_O interrupt for MMA9553 we need to override this by setting Legacy+AFE Sampling Interrupt.
Clear the data ready flag, it will be set again by the ISR.
Read the Pedometer data from the MMA9553.
Read the raw sensor data from the MMA9553.
Definition at line 80 of file mma9553_pedometer_interrupt.c.
References mma9553_acceldata_t::accel, ASK_USER_TO_RESUME, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), BOARD_SystickEnable(), Driver_GPIO_KSDK, gMma9553DataReady, GPIO_DIRECTION_IN, GPIO_DIRECTION_OUT, GREEN_LED, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, I2Cdrv, int32_t(), MMA9553_I2C_ADDR, MMA9553_I2C_CommandResponse(), MMA9553_I2C_Configure(), MMA9553_I2C_Initialize(), MMA9553_I2C_SetIdleTask(), mma9553_int_data_ready_callback(), MMA9553_INT_O, pGpioDriver, GENERIC_DRIVER_GPIO::pin_init, rawData, SENSOR_ERROR_NONE, SMC, SMC_SetPowerModeVlpr(), SMC_SetPowerModeWait(), status, and GENERIC_DRIVER_GPIO::toggle_pin.

| void mma9553_int_data_ready_callback | ( | void * | pUserData | ) |
Definition at line 72 of file mma9553_pedometer_interrupt.c.
References gMma9553DataReady.
Referenced by main().

| const registercommandlist_t cMma9553Config30Hz[] |
Prepare the register write list to configure MMA9553L in 30Hz Mode.
Definition at line 40 of file mma9553_pedometer_interrupt.c.
| const registercommandlist_t cMma9553EnableInterruptCommand[] |
Prepare the command list to enable interrupts for AFE sampling completion with Legacy Mode for MMA9553.
Definition at line 56 of file mma9553_pedometer_interrupt.c.
| const registercommandlist_t cMma9553ReadPedometerCommand[] |
Prepare the command list to read the Pedometer data from MMA9553.
Definition at line 52 of file mma9553_pedometer_interrupt.c.
| const registerreadlist_t cMma9553ReadPedometerOutput[] |
Prepare the read list to read the Pedometer data from MMA9553.
Definition at line 60 of file mma9553_pedometer_interrupt.c.
| const registerreadlist_t cMma9553ReadRawOutput[] |
Prepare the register read list to read the raw Accel data from MMA9553.
Definition at line 48 of file mma9553_pedometer_interrupt.c.
| volatile bool gMma9553DataReady |
Definition at line 66 of file mma9553_pedometer_interrupt.c.
Referenced by main(), and mma9553_int_data_ready_callback().