![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The fxpq3115_normal.c file implements the ISSDK FXPQ3115BV sensor driver example demonstration with polling mode. More...
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_debug_console.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "fxpq3115_drv.h"
Go to the source code of this file.
Macros | |
| #define | FXPQ3115_DATA_SIZE (5) /* 3 byte Pressure/Altitude and 2 byte Temperature. */ |
| #define | FXPQ3115_SAMPLING_EXPONENT (1) /* 2 seconds */ |
Functions | |
| int | main (void) |
| Main function. More... | |
Variables | |
| const registerwritelist_t | B3115ConfigPoll [] |
| Register settings for Normal (non buffered) mode. More... | |
| const registerreadlist_t | B3115Status [] = {{.readFrom = FXPQ3115_STATUS, .numBytes = 1}, __END_READ_DATA__} |
| Address of Status Register. More... | |
| const registerreadlist_t | B3115OutputNormal [] |
| Address and size of Raw Pressure+Temperature Data in Normal Mode. More... | |
The fxpq3115_normal.c file implements the ISSDK FXPQ3115BV sensor driver example demonstration with polling mode.
Definition in file fxpq3115_normal.c.
Definition at line 35 of file fxpq3115_normal.c.
Referenced by main().
| #define FXPQ3115_SAMPLING_EXPONENT (1) /* 2 seconds */ |
In FXPQ3115 the Auto Acquisition Time Step (ODR) can be set only in powers of 2 (i.e. 2^x, where x is the SAMPLING_EXPONENT). This gives a range of 1 second to 2^15 seconds (9 hours).
Definition at line 39 of file fxpq3115_normal.c.
| int main | ( | void | ) |
Main function.
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize FXPQ3115 sensor driver.
Set the task to be executed while waiting for I2C transactions to complete.
Configure the FXPQ3115 sensor.
Wait for data ready from the FXPQ3115.
Read new raw sensor data from the FXPQ3115.
Process the sample and convert the raw sensor data.
Definition at line 69 of file fxpq3115_normal.c.
References ASK_USER_TO_RESUME, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), data, FXPQ3115_DATA_SIZE, FXPQ3115_DR_STATUS_PTDR_MASK, FXPQ3115_I2C_ADDR, FXPQ3115_I2C_Configure(), FXPQ3115_I2C_Initialize(), FXPQ3115_I2C_ReadData(), FXPQ3115_I2C_SetIdleTask(), FXPQ3115_PRESSURE_CONV_FACTOR, FXPQ3115_TEMPERATURE_CONV_FACTOR, FXPQ3115_WHOAMI_VALUE, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, I2Cdrv, int32_t(), fxpq3115_pressuredata_t::pressure, rawData, SENSOR_ERROR_NONE, SMC, SMC_SetPowerModeVlpr(), status, and fxpq3115_pressuredata_t::temperature.

| const registerwritelist_t B3115ConfigPoll[] |
Register settings for Normal (non buffered) mode.
Definition at line 45 of file fxpq3115_normal.c.
| const registerreadlist_t B3115OutputNormal[] |
Address and size of Raw Pressure+Temperature Data in Normal Mode.
Definition at line 60 of file fxpq3115_normal.c.
| const registerreadlist_t B3115Status[] = {{.readFrom = FXPQ3115_STATUS, .numBytes = 1}, __END_READ_DATA__} |
Address of Status Register.
Definition at line 57 of file fxpq3115_normal.c.