19 #include "clock_config.h" 21 #include "fsl_debug_console.h" 26 #include "Driver_I2C.h" 29 #include "issdk_hal.h" 35 #define FXPQ3115_DATA_SIZE (5) 39 #define FXPQ3115_SAMPLING_EXPONENT (1) 71 int16_t tempInDegrees;
72 uint32_t pressureInPascals;
85 PRINTF(
"\r\n ISSDK FXPQ3115 sensor driver example demonstration with poll mode\r\n");
89 if (ARM_DRIVER_OK != status)
91 PRINTF(
"\r\n I2C Initialization Failed\r\n");
96 status = I2Cdrv->PowerControl(ARM_POWER_FULL);
97 if (ARM_DRIVER_OK != status)
99 PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
104 status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
105 if (ARM_DRIVER_OK != status)
107 PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
116 PRINTF(
"\r\n Sensor Initialization Failed\r\n");
119 PRINTF(
"\r\n Successfully Initiliazed Sensor\r\n");
128 PRINTF(
"\r\n FXPQ3115 sensor configuration failed.\r\n");
131 PRINTF(
"\r\n Successfully Applied FXPQ3115 Sensor Configuration\r\n");
144 if (ARM_DRIVER_OK != status)
146 PRINTF(
"\r\n Read Failed. \r\n");
151 rawData.
pressure = (uint32_t)((data[0]) << 16) | ((data[1]) << 8) | ((data[2]));
154 rawData.
temperature = (int16_t)((data[3]) << 8) | (data[4]);
157 PRINTF(
"\r\n Pressure = %d Pa\r\n", pressureInPascals);
158 PRINTF(
"\r\n Temperature = %d degC\r\n", tempInDegrees);
#define FXPQ3115_PRESSURE_CONV_FACTOR
const registerreadlist_t B3115OutputNormal[]
Address and size of Raw Pressure+Temperature Data in Normal Mode.
This structure defines the Write command List.
#define ASK_USER_TO_RESUME(x)
#define FXPQ3115_DR_STATUS_PTDR_MASK
#define FXPQ3115_SAMPLING_EXPONENT
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
#define FXPQ3115_PT_DATA_CFG_TDEFE_MASK
#define FXPQ3115_PT_DATA_CFG_TDEFE_ENABLED
#define FXPQ3115_CTRL_REG1_OS_MASK
#define __END_WRITE_DATA__
This structure defines the fxpq3115 data buffer in Pressure Mode.
int main(void)
Main function.
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
#define FXPQ3115_PT_DATA_CFG_PDEFE_MASK
#define I2C_S_SIGNAL_EVENT
int32_t FXPQ3115_I2C_Configure(fxpq3115_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
#define BOARD_BootClockRUN
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
void FXPQ3115_I2C_SetIdleTask(fxpq3115_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
int32_t FXPQ3115_I2C_Initialize(fxpq3115_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
const registerwritelist_t B3115ConfigPoll[]
Register settings for Normal (non buffered) mode.
#define FXPQ3115_PT_DATA_CFG_DREM_MASK
The fxpq3115_drv.h file describes the fxpq3115 driver interface and structures.
uint8_t data[FXLS8962_DATA_SIZE]
#define __END_READ_DATA__
const registerreadlist_t B3115Status[]
Address of Status Register.
#define FXPQ3115_DATA_SIZE
#define FXPQ3115_CTRL_REG1_OS_OSR_128
fxos8700_accelmagdata_t rawData
#define FXPQ3115_PT_DATA_CFG_PDEFE_ENABLED
#define FXPQ3115_WHOAMI_VALUE
This structure defines the Read command List.
#define FXPQ3115_I2C_ADDR
#define I2C_S_DEVICE_INDEX
This defines the sensor specific information.
void BOARD_InitDebugConsole(void)
int32_t FXPQ3115_I2C_ReadData(fxpq3115_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
#define FXPQ3115_PT_DATA_CFG_DREM_ENABLED
#define FXPQ3115_CTRL_REG2_ST_MASK
#define FXPQ3115_TEMPERATURE_CONV_FACTOR