![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The fxls8962_freefall.c file implements the ISSDK FXLS8962 sensor driver example demonstration for Freefall Detection. More...
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_debug_console.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "gpio_driver.h"#include "fxls8962_drv.h"#include "systick_utils.h"
Go to the source code of this file.
Macros | |
| #define | SDCD_WT_DBCNT 0x0A /* Debounce count value. */ |
| #define | SDCD_LTHS_LSB 0x33 /* Lower Threshold LSB value. */ |
| #define | SDCD_LTHS_MSB 0x0F /* Lower Threshold MSB value. */ |
| #define | SDCD_UTHS_LSB 0xCD /* Upper Threshold LSB value. */ |
| #define | SDCD_UTHS_MSB 0x00 /* Upper Threshold MSB value. */ |
Functions | |
| void | fxls8962_int_event_ready_callback (void *pUserData) |
| This is the Sensor Data Ready ISR implementation. More... | |
| int | main (void) |
| Main function. More... | |
Variables | |
| const registerwritelist_t | cFxls8962ConfigFreeFall [] |
| Register settings for free-fall detection. More... | |
| const registerreadlist_t | cFxls8962FreeFallEvent [] |
| Address of SDCD Status Register. More... | |
| volatile bool | gFxls8962EventReady = false |
The fxls8962_freefall.c file implements the ISSDK FXLS8962 sensor driver example demonstration for Freefall Detection.
Definition in file fxls8962_freefall.c.
| #define SDCD_LTHS_LSB 0x33 /* Lower Threshold LSB value. */ |
Definition at line 41 of file fxls8962_freefall.c.
| #define SDCD_LTHS_MSB 0x0F /* Lower Threshold MSB value. */ |
Definition at line 42 of file fxls8962_freefall.c.
| #define SDCD_UTHS_LSB 0xCD /* Upper Threshold LSB value. */ |
Definition at line 43 of file fxls8962_freefall.c.
| #define SDCD_UTHS_MSB 0x00 /* Upper Threshold MSB value. */ |
Definition at line 44 of file fxls8962_freefall.c.
| #define SDCD_WT_DBCNT 0x0A /* Debounce count value. */ |
Definition at line 40 of file fxls8962_freefall.c.
| void fxls8962_int_event_ready_callback | ( | void * | pUserData | ) |
This is the Sensor Data Ready ISR implementation.
Set flag to indicate Sensor has signalled data ready.
Definition at line 91 of file fxls8962_freefall.c.
References gFxls8962EventReady.
Referenced by main().

| int main | ( | void | ) |
Main function.
Initialize FXLS8962 pin used by FRDM board
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize the FXLS8962 sensor driver.
Set the task to be executed while waiting for I2C transactions to complete.
Configure the FXLS8962 sensor for Freefall detection Mode.
Clear the data ready flag, it will be set again by the ISR.
Read the Freefall event FLAGs from FXLS8962.
Display that a freefall event has been detected.
Definition at line 99 of file fxls8962_freefall.c.
References BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), BOARD_SystickEnable(), Driver_GPIO_KSDK, FXLS8962_I2C_ADDR, FXLS8962_I2C_Configure(), FXLS8962_I2C_Initialize(), FXLS8962_I2C_ReadData(), FXLS8962_I2C_SetIdleTask(), FXLS8962_INT1, fxls8962_int_event_ready_callback(), FXLS8962_SDCD_INT_SRC2_WT_EA_EVENT_NO, FXLS8962_SDCD_INT_SRC2_WT_EA_MASK, FXLS8962_WHOAMI_VALUE, fxls8962Driver, FXLS8964_WHOAMI_VALUE, FXLS8967_WHOAMI_VALUE, FXLS8974_WHOAMI_VALUE, gFxls8962EventReady, GPIO_DIRECTION_IN, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, I2Cdrv, int32_t(), pGpioDriver, GENERIC_DRIVER_GPIO::pin_init, SENSOR_ERROR_NONE, SMC, SMC_SetPowerModeVlpr(), SMC_SetPowerModeWait(), and status.

| const registerwritelist_t cFxls8962ConfigFreeFall[] |
Register settings for free-fall detection.
Definition at line 50 of file fxls8962_freefall.c.
| const registerreadlist_t cFxls8962FreeFallEvent[] |
Address of SDCD Status Register.
Definition at line 79 of file fxls8962_freefall.c.
| volatile bool gFxls8962EventReady = false |
Definition at line 85 of file fxls8962_freefall.c.
Referenced by fxls8962_int_event_ready_callback(), and main().