18 #include "clock_config.h" 20 #include "fsl_debug_console.h" 25 #include "issdk_hal.h" 26 #include "gpio_driver.h" 33 #include "Driver_SPI.h" 38 #define FXLS8974_DATA_SIZE (6) 74 uint8_t gfxls8974DataReady;
87 PRINTF(
"\r\n ISSDK FXLS8974 sensor driver example demonstration for SPI with Poll Mode.\r\n");
91 if (ARM_DRIVER_OK != status)
93 PRINTF(
"\r\n SPI Initialization Failed\r\n");
98 status = pSPIdriver->PowerControl(ARM_POWER_FULL);
99 if (ARM_DRIVER_OK != status)
101 PRINTF(
"\r\n SPI Power Mode setting Failed\r\n");
106 status = pSPIdriver->Control(ARM_SPI_MODE_MASTER | ARM_SPI_CPOL0_CPHA0,
SPI_S_BAUDRATE);
107 if (ARM_DRIVER_OK != status)
109 PRINTF(
"\r\n SPI Control Mode setting Failed\r\n");
118 PRINTF(
"\r\n FXLS8974 Sensor Initialization Failed\r\n");
123 PRINTF(
"\r\n Successfully Initialized Gemini with WHO_AM_I = 0x%X\r\n", whoami);
127 PRINTF(
"\r\n Successfully Initialized Timandra with WHO_AM_I = 0x%X\r\n", whoami);
131 PRINTF(
"\r\n Successfully Initialized Newstein with WHO_AM_I = 0x%X\r\n", whoami);
135 PRINTF(
"\r\n Bad WHO_AM_I = 0x%X\r\n", whoami);
145 PRINTF(
"\r\n FXLS8974 Sensor Configuration Failed, Err = %d\r\n", status);
148 PRINTF(
"\r\n Successfully Applied FXLS8974 Sensor Configuration\r\n");
161 if (ARM_DRIVER_OK != status)
163 PRINTF(
"\r\nRead Failed.\r\n");
168 rawData.
accel[0] = ((int16_t)data[1] << 8) | data[0];
169 rawData.
accel[1] = ((int16_t)data[3] << 8) | data[2];
170 rawData.
accel[2] = ((int16_t)data[5] << 8) | data[4];
173 PRINTF(
"\r\n X=%5d Y=%5d Z=%5d\r\n", rawData.
accel[0], rawData.
accel[1], rawData.
accel[2]);
const registerreadlist_t cfxls8974OutputNormal[]
Address of Raw Accel Data in Normal Mode.
This structure defines the Write command List.
#define FXLS8974_SENS_CONFIG1_FSR_MASK
#define FXLS8974_INT_STATUS_SRC_DRDY_MASK
void FXLS8974_SPI_SetIdleTask(fxls8974_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the SPI Idle Task.
const registerreadlist_t cfxls8974DRDYEvent[]
Address of DATA Ready Status Register.
int32_t FXLS8974_SPI_Initialize(fxls8974_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSlaveSelect, uint8_t *whoami)
The interface function to initialize the sensor.
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
int32_t FXLS8974_SPI_ReadData(fxls8974_spi_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
int main(void)
This is the The main function implementation.
#define __END_WRITE_DATA__
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
#define SPI_S_BAUDRATE
Transfer baudrate - 500k.
#define FXLS8967_WHOAMI_VALUE
#define SPI_S_DEVICE_INDEX
This defines the sensor specific information for SPI.
int32_t FXLS8974_SPI_Configure(fxls8974_spi_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
#define BOARD_BootClockRUN
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
This structure defines the fxls8974 raw data buffer.
uint8_t data[FXLS8962_DATA_SIZE]
#define __END_READ_DATA__
#define FXLS8974_SENS_CONFIG3_WAKE_ODR_MASK
fxls8974_i2c_sensorhandle_t fxls8974Driver
fxos8700_accelmagdata_t rawData
void BOARD_SystickEnable(void)
Function to enable systicks framework.
#define FXLS8974_SENS_CONFIG1_FSR_2G
This structure defines the Read command List.
#define FXLS8974_WHOAMI_VALUE
The fxls8974_drv.h file describes the FXLS8974CF driver interface and structures. ...
#define FXLS8968_WHOAMI_VALUE
#define SPI_S_SIGNAL_EVENT
const registerwritelist_t cfxls8974ConfigNormal[]
Register settings for Normal (non buffered) mode.
#define FXLS8974_DATA_SIZE
void BOARD_InitDebugConsole(void)
#define FXLS8962_WHOAMI_VALUE
#define FXLS8974_SENS_CONFIG3_WAKE_ODR_6_25HZ
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
#define FXLS8964_WHOAMI_VALUE