16 #include "clock_config.h" 18 #include "fsl_debug_console.h" 19 #include "fsl_irqsteer.h" 22 #include "Driver_I2C.h" 25 #include "issdk_hal.h" 31 #define RAW_ACCELMAG_DATA_SIZE (12) 78 ipc = BOARD_InitRpc();
85 PRINTF(
"\r\n -----------------------------------------------------------------\r\n");
86 PRINTF(
"\r\n ISSDK FXOS8700 sensor driver example demonstration with POLL mode\r\n");
87 PRINTF(
"\r\n -----------------------------------------------------------------\r\n");
90 if (sc_pm_set_resource_power_mode(ipc, SC_R_I2C_0, SC_PM_PW_MODE_ON) != SC_ERR_NONE)
92 PRINTF(
"Error: Failed to power on LPI2C\r\n");
96 freq = CLOCK_SetIpFreq(kCLOCK_DMA_Lpi2c0, SC_24MHZ);
99 PRINTF(
"Error: Failed to set LPI2C frequency\r\n");
103 #if (MIMX8QM_CM4_CORE0) 104 if (sc_pm_set_resource_power_mode(ipc, SC_R_IRQSTR_M4_0, SC_PM_PW_MODE_ON) != SC_ERR_NONE)
106 PRINTF(
"Error: Failed to power on IRQSTEER M4_0\r\n");
108 #elif (MIMX8QM_CM4_CORE1) 109 if (sc_pm_set_resource_power_mode(ipc, SC_R_IRQSTR_M4_1, SC_PM_PW_MODE_ON) != SC_ERR_NONE)
111 PRINTF(
"Error: Failed to power on IRQSTEER M4_1\r\n");
116 IRQSTEER_Init(IRQSTEER);
117 IRQSTEER_EnableInterrupt(IRQSTEER, DMA_I2C0_INT_IRQn);
121 if (ARM_DRIVER_OK != status)
123 PRINTF(
"\r\n I2C Initialization Failed\r\n");
128 status = I2Cdrv->PowerControl(ARM_POWER_FULL);
129 if (ARM_DRIVER_OK != status)
131 PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
136 status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
137 if (ARM_DRIVER_OK != status)
139 PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
148 PRINTF(
"\r\n Sensor Initialization Failed\r\n");
151 PRINTF(
"\r\n Successfully Initiliazed FXOS8700 Sensor\r\n");
158 PRINTF(
"\r\n FXOS8700 Sensor Configuration Failed, Err = %d\r\n", status);
161 PRINTF(
"\r\n Successfully Applied FXOS8700 Sensor Configuration\r\n");
163 PRINTF(
"\r\n Reading FXOS8700 Accel & Mag Values in Hybrid POLL mode\r\n");
176 if (ARM_DRIVER_OK != status)
178 PRINTF(
"\r\n Read Failed. \r\n");
183 rawData.
accel[0] = ((int16_t)data[0] << 8) | data[1];
184 rawData.
accel[0] /= 4;
185 rawData.
accel[1] = ((int16_t)data[2] << 8) | data[3];
186 rawData.
accel[1] /= 4;
187 rawData.
accel[2] = ((int16_t)data[4] << 8) | data[5];
188 rawData.
accel[2] /= 4;
189 rawData.
mag[0] = ((int16_t)data[6] << 8) | data[7];
190 rawData.
mag[1] = ((int16_t)data[8] << 8) | data[9];
191 rawData.
mag[2] = ((int16_t)data[10] << 8) | data[11];
194 PRINTF(
"\r\n Accel X = %d Y = %d Z = %d\r\n", rawData.
accel[0], rawData.
accel[1], rawData.
accel[2]);
195 PRINTF(
"\r\n Mag X = %d Y = %d Z = %d\r\n\r\n", rawData.
mag[0], rawData.
mag[1], rawData.
mag[2]);
int32_t FXOS8700_I2C_Initialize(fxos8700_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
This structure defines the fxos8700 raw data buffer.
This structure defines the Write command List.
#define FXOS8700_M_CTRL_REG2_M_AUTOINC_MASK
#define ASK_USER_TO_RESUME(x)
#define FXOS8700_M_CTRL_REG1_M_HMS_MASK
#define FXOS8700_WHO_AM_I_PROD_VALUE
#define FXOS8700_CTRL_REG1_DR_MASK
const registerreadlist_t FXOS8700_STATUS_READ[]
#define FXOS8700_M_CTRL_REG1_M_HMS_HYBRID_MODE
#define __END_WRITE_DATA__
#define FXOS8700_M_CTRL_REG2_M_AUTOINC_HYBRID_MODE
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
#define I2C_S_SIGNAL_EVENT
This defines the sensor specific information for I2C.
const registerreadlist_t FXOS8700_ACCEL_MAG_READ[]
int32_t FXOS8700_I2C_Configure(fxos8700_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
const registerwritelist_t fxos8700_Config_Hybrid[]
int32_t FXOS8700_I2C_ReadData(fxos8700_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
#define BOARD_BootClockRUN
#define FXOS8700_M_CTRL_REG1_M_ACAL_EN
#define FXOS8700_M_CTRL_REG1_M_ACAL_MASK
uint8_t data[FXLS8962_DATA_SIZE]
const registerreadlist_t FXOS8700_ACCELMAG_READ[]
#define __END_READ_DATA__
fxos8700_accelmagdata_t rawData
#define FXOS8700_M_CTRL_REG2_M_RST_CNT_DISABLE
#define FXOS8700_M_CTRL_REG2_M_RST_CNT_MASK
The fxos8700_drv.h file describes the fxos8700 driver interface and structures.
#define FXOS8700_CTRL_REG1_DR_HYBRID_25_HZ
This structure defines the Read command List.
#define I2C_S_DEVICE_INDEX
int main(void)
Main function.
void BOARD_InitDebugConsole(void)
#define FXOS8700_DR_STATUS_ZYXDR_MASK
#define FXOS8700_I2C_ADDR
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
#define RAW_ACCELMAG_DATA_SIZE