19 #include "clock_config.h" 21 #include "fsl_debug_console.h" 26 #include "Driver_I2C.h" 29 #include "issdk_hal.h" 35 #define MPL3115_DATA_SIZE (5) 39 #define MPL3115_SAMPLING_EXPONENT (1) 72 int16_t tempInDegrees;
86 PRINTF(
"\r\n ISSDK MPL3115 sensor driver example demonstration with poll mode\r\n");
90 if (ARM_DRIVER_OK != status)
92 PRINTF(
"\r\n I2C Initialization Failed\r\n");
97 status = I2Cdrv->PowerControl(ARM_POWER_FULL);
98 if (ARM_DRIVER_OK != status)
100 PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
105 status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
106 if (ARM_DRIVER_OK != status)
108 PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
117 PRINTF(
"\r\n Sensor Initialization Failed\r\n");
120 PRINTF(
"\r\n Successfully Initiliazed Sensor\r\n");
129 PRINTF(
"\r\nMPL3115 configuration failed...\r\n");
132 PRINTF(
"\r\n Successfully Applied MPL3115 Sensor Configuration\r\n");
145 if (ARM_DRIVER_OK != status)
147 PRINTF(
"\r\n Read Failed. \r\n");
152 rawData.
altitude = (
int32_t)((data[0]) << 24) | ((data[1]) << 16) | ((data[2]) << 8);
155 rawData.
temperature = (int16_t)((data[3]) << 8) | (data[4]);
158 PRINTF(
"\r\nAltitude = %d Meters\r\n", altitudeInMeters);
159 PRINTF(
"\r\nTemperature = %d degC\r\n", tempInDegrees);
This structure defines the Write command List.
#define ASK_USER_TO_RESUME(x)
void MPL3115_I2C_SetIdleTask(mpl3115_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
const registerreadlist_t cMpl3115Status[]
Address of Status Register.
This structure defines the mpl3115 data buffer in Altitude Mode.
int32_t MPL3115_I2C_ReadData(mpl3115_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
The mpl3115_drv.h file describes the MPL3115 driver interface and structures.
#define MPL3115_CTRL_REG2_ST_MASK
#define MPL3115_SAMPLING_EXPONENT
#define __END_WRITE_DATA__
#define MPL3115_PT_DATA_CFG_TDEFE_MASK
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
#define I2C_S_SIGNAL_EVENT
#define MPL3115_DR_STATUS_PTDR_MASK
#define BOARD_BootClockRUN
#define MPL3115_TEMPERATURE_CONV_FACTOR
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
const registerwritelist_t cMpl3115ConfigAltitude[]
Register settings for Altitude readings in Normal (non buffered) mode.
#define MPL3115_PT_DATA_CFG_DREM_ENABLED
uint8_t data[FXLS8962_DATA_SIZE]
#define MPL3115_PT_DATA_CFG_PDEFE_MASK
#define __END_READ_DATA__
const registerreadlist_t cMpl3115OutputNormal[]
Address and size of Raw Altitude+Temperature Data in Normal Mode.
This defines the sensor specific information.
#define MPL3115_CTRL_REG1_OS_OSR_128
#define MPL3115_CTRL_REG1_ALT_MASK
fxos8700_accelmagdata_t rawData
int32_t MPL3115_I2C_Initialize(mpl3115_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
#define MPL3115_PT_DATA_CFG_DREM_MASK
#define MPL3115_PT_DATA_CFG_PDEFE_ENABLED
int main(void)
Main function.
#define MPL3115_WHOAMI_VALUE
This structure defines the Read command List.
#define MPL3115_PT_DATA_CFG_TDEFE_ENABLED
#define I2C_S_DEVICE_INDEX
#define MPL3115_DATA_SIZE
void BOARD_InitDebugConsole(void)
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
int32_t MPL3115_I2C_Configure(mpl3115_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
#define MPL3115_CTRL_REG1_OS_MASK
#define MPL3115_CTRL_REG1_ALT_ALT
#define MPL3115_ALTITUDE_CONV_FACTOR