ISSDK  1.8
IoT Sensing Software Development Kit
mpl3115_fifo.c
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015-2016, Freescale Semiconductor, Inc.
3  * Copyright 2016-2017 NXP
4  * All rights reserved.
5  *
6  * SPDX-License-Identifier: BSD-3-Clause
7  */
8 
9 /**
10  * @file mpl3115_fifo.c
11  * @brief The mpl3115_fifo.c file implements the ISSDK MPL3115 sensor driver
12  * example demonstration with polling mode.
13  */
14 
15 //-----------------------------------------------------------------------
16 // SDK Includes
17 //-----------------------------------------------------------------------
18 #include "pin_mux.h"
19 #include "clock_config.h"
20 #include "board.h"
21 #include "fsl_debug_console.h"
22 
23 //-----------------------------------------------------------------------
24 // CMSIS Includes
25 //-----------------------------------------------------------------------
26 #include "Driver_I2C.h"
27 
28 /* ISSDK Includes */
29 #include "issdk_hal.h"
30 #include "mpl3115_drv.h"
31 
32 //-----------------------------------------------------------------------
33 // Macros
34 //-----------------------------------------------------------------------
35 #define FIFO_WMRK_SIZE (8) /* Buffer 8 Samples. */
36 #define MPL3115_DATA_SIZE (5) /* 3 byte Pressure/Altitude and 2 byte Temperature. */
37 /*! In MPL3115 the Auto Acquisition Time Step (ODR) can be set only in powers of 2 (i.e. 2^x, where x is the
38  * SAMPLING_EXPONENT).
39  * This gives a range of 1 second to 2^15 seconds (9 hours). */
40 #define MPL3115_SAMPLING_EXPONENT (0) /* 1 second. */
41 
42 //-----------------------------------------------------------------------
43 // Constants
44 //-----------------------------------------------------------------------
45 /*! @brief Register settings for FIFO (buffered) mode @ default 1 sample per second. */
47  /* Set FIFO Mode and set FIFO Watermark Level. */
50  /* Enable Data Ready and Event flags for Pressure, Temperature or either. */
54  /* Set Over Sampling Ratio to 128. */
58 
59 /*! @brief Address of Status Register. */
61 
62 /*! @brief Address and size of Pressure+Temperature Data in FIFO Mode. */
65 
66 //-----------------------------------------------------------------------
67 // Functions
68 //-----------------------------------------------------------------------
69 /*!
70  * @brief Main function
71  */
72 int main(void)
73 {
74  int16_t tempInDegrees;
75  uint32_t pressureInPascals;
77  uint8_t dataReady;
80 
81  ARM_DRIVER_I2C *I2Cdrv = &I2C_S_DRIVER; // Now using the shield.h value!!!
82  mpl3115_i2c_sensorhandle_t mpl3115Driver;
83 
87 
88  PRINTF("\r\n ISSDK MPL3115 sensor driver example demonstration with fifo mode\r\n");
89 
90  /*! Initialize the I2C driver. */
91  status = I2Cdrv->Initialize(I2C_S_SIGNAL_EVENT);
92  if (ARM_DRIVER_OK != status)
93  {
94  PRINTF("\r\n I2C Initialization Failed\r\n");
95  return -1;
96  }
97 
98  /*! Set the I2C Power mode. */
99  status = I2Cdrv->PowerControl(ARM_POWER_FULL);
100  if (ARM_DRIVER_OK != status)
101  {
102  PRINTF("\r\n I2C Power Mode setting Failed\r\n");
103  return -1;
104  }
105 
106  /*! Set the I2C bus speed. */
107  status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
108  if (ARM_DRIVER_OK != status)
109  {
110  PRINTF("\r\n I2C Control Mode setting Failed\r\n");
111  return -1;
112  }
113 
114  /*! Initialize MPL3115 sensor driver. */
117  if (SENSOR_ERROR_NONE != status)
118  {
119  PRINTF("\r\n Sensor Initialization Failed\r\n");
120  return -1;
121  }
122  PRINTF("\r\n Successfully Initiliazed Sensor\r\n");
123 
124  /*! Set the task to be executed while waiting for I2C transactions to complete. */
126 
127  /*! Configure the MPL3115 sensor. */
128  status = MPL3115_I2C_Configure(&mpl3115Driver, cMpl3115ConfigFIFO);
129  if (SENSOR_ERROR_NONE != status)
130  {
131  PRINTF("\r\nMPL3115 configuration failed...\r\n");
132  return -1;
133  }
134  PRINTF("\r\n Successfully Applied MPL3115 Sensor Configuration\r\n");
135 
136  for (;;) /* Forever loop */
137  {
138  /*! Wait for data ready from the MPL3115. */
139  status = MPL3115_I2C_ReadData(&mpl3115Driver, cMpl3115Status, &dataReady);
140  if (0 == (dataReady & MPL3115_F_STATUS_F_WMKF_FLAG_MASK))
141  { /* Loop, if new sample is not available. */
142  continue;
143  }
144 
145  /*! Read new raw sensor data from the MPL3115. */
146  status = MPL3115_I2C_ReadData(&mpl3115Driver, cMpl3115OutputFIFO, data);
147  if (ARM_DRIVER_OK != status)
148  {
149  PRINTF("\r\n Read Failed. \r\n");
150  return -1;
151  }
152 
153  /* Reset Counters */
154  pressureInPascals = 0;
155  tempInDegrees = 0;
156 
157  for (uint8_t i = 0; i < FIFO_WMRK_SIZE; i++)
158  { /*! Process all samples and convert the raw sensor data. */
159  rawData.pressure = (uint32_t)((data[i * MPL3115_DATA_SIZE + 0]) << 16) |
160  ((data[i * MPL3115_DATA_SIZE + 1]) << 8) | ((data[i * MPL3115_DATA_SIZE + 2]));
161  pressureInPascals += rawData.pressure / MPL3115_PRESSURE_CONV_FACTOR;
162 
163  rawData.temperature = (int16_t)((data[i * MPL3115_DATA_SIZE + 3]) << 8) | (data[i * MPL3115_DATA_SIZE + 4]);
164  tempInDegrees += rawData.temperature / MPL3115_TEMPERATURE_CONV_FACTOR;
165  }
166  PRINTF("\r\nAverage Pressure = %d Pa\r\n", pressureInPascals / FIFO_WMRK_SIZE);
167  PRINTF("\r\nAverage Temperature = %d degC\r\n", tempInDegrees / FIFO_WMRK_SIZE);
168  ASK_USER_TO_RESUME(16 / FIFO_WMRK_SIZE); /* Ask for user input after processing 16 samples. */
169  }
170 }
const registerreadlist_t cMpl3115OutputFIFO[]
Address and size of Pressure+Temperature Data in FIFO Mode.
Definition: mpl3115_fifo.c:63
This structure defines the Write command List.
Definition: sensor_drv.h:68
#define ASK_USER_TO_RESUME(x)
Definition: frdm_k64f.h:106
int32_t status
void MPL3115_I2C_SetIdleTask(mpl3115_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
Definition: mpl3115_drv.c:53
#define MPL3115_DATA_SIZE
Definition: mpl3115_fifo.c:36
#define MPL3115_PRESSURE_CONV_FACTOR
Definition: mpl3115_drv.h:28
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
Definition: lpc54114.c:169
const registerreadlist_t cMpl3115Status[]
Address of Status Register.
Definition: mpl3115_fifo.c:60
int32_t MPL3115_I2C_ReadData(mpl3115_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
Definition: mpl3115_drv.c:104
#define MPL3115_F_SETUP_F_MODE_MASK
Definition: mpl3115.h:410
The mpl3115_drv.h file describes the MPL3115 driver interface and structures.
#define MPL3115_CTRL_REG2_ST_MASK
Definition: mpl3115.h:916
#define SMC
Definition: lpc54114.h:118
#define __END_WRITE_DATA__
Definition: sensor_drv.h:45
#define MPL3115_F_SETUP_F_MODE_STOP_MODE
Definition: mpl3115.h:420
#define MPL3115_PT_DATA_CFG_TDEFE_MASK
Definition: mpl3115.h:550
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
#define MPL3115_F_SETUP_F_WMRK_MASK
Definition: mpl3115.h:407
#define I2C_S_SIGNAL_EVENT
Definition: issdk_hal.h:34
#define I2C_S_DRIVER
Definition: issdk_hal.h:33
#define BOARD_BootClockRUN
Definition: clock_config.h:19
#define MPL3115_TEMPERATURE_CONV_FACTOR
Definition: mpl3115_drv.h:30
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
Definition: sensor_drv.h:97
This structure defines the mpl3115 data buffer in Pressure Mode.
Definition: mpl3115_drv.h:45
#define MPL3115_PT_DATA_CFG_DREM_ENABLED
Definition: mpl3115.h:570
uint8_t data[FXLS8962_DATA_SIZE]
#define MPL3115_PT_DATA_CFG_PDEFE_MASK
Definition: mpl3115.h:553
#define __END_READ_DATA__
Definition: sensor_drv.h:51
This defines the sensor specific information.
Definition: mpl3115_drv.h:36
#define MPL3115_CTRL_REG1_OS_OSR_128
Definition: mpl3115.h:884
ARM_DRIVER_I2C * I2Cdrv
fxos8700_accelmagdata_t rawData
int32_t MPL3115_I2C_Initialize(mpl3115_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
Definition: mpl3115_drv.c:22
#define MPL3115_F_STATUS_F_WMKF_FLAG_MASK
Definition: mpl3115.h:359
uint16_t readFrom
Definition: sensor_drv.h:80
#define MPL3115_SAMPLING_EXPONENT
Definition: mpl3115_fifo.c:40
#define MPL3115_PT_DATA_CFG_DREM_MASK
Definition: mpl3115.h:556
#define MPL3115_PT_DATA_CFG_PDEFE_ENABLED
Definition: mpl3115.h:567
#define MPL3115_WHOAMI_VALUE
Definition: mpl3115.h:65
int main(void)
Main function.
Definition: mpl3115_fifo.c:72
const registerwritelist_t cMpl3115ConfigFIFO[]
Register settings for FIFO (buffered) mode @ default 1 sample per second.
Definition: mpl3115_fifo.c:46
This structure defines the Read command List.
Definition: sensor_drv.h:78
#define MPL3115_PT_DATA_CFG_TDEFE_ENABLED
Definition: mpl3115.h:564
#define I2C_S_DEVICE_INDEX
Definition: issdk_hal.h:35
#define FIFO_WMRK_SIZE
Definition: mpl3115_fifo.c:35
#define MPL3115_I2C_ADDR
void BOARD_InitDebugConsole(void)
Definition: board.c:15
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
Definition: pin_mux.c:47
int32_t MPL3115_I2C_Configure(mpl3115_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
Definition: mpl3115_drv.c:61
#define MPL3115_CTRL_REG1_OS_MASK
Definition: mpl3115.h:855