ISSDK  1.8
IoT Sensing Software Development Kit
mpl3115_normal.c
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015-2016, Freescale Semiconductor, Inc.
3  * Copyright 2016-2017 NXP
4  * All rights reserved.
5  *
6  * SPDX-License-Identifier: BSD-3-Clause
7  */
8 
9 /**
10  * @file mpl3115_normal.c
11  * @brief The mpl3115_normal.c file implements the ISSDK MPL3115 sensor driver
12  * example demonstration with polling mode.
13  */
14 
15 //-----------------------------------------------------------------------
16 // SDK Includes
17 //-----------------------------------------------------------------------
18 #include "pin_mux.h"
19 #include "clock_config.h"
20 #include "board.h"
21 #include "fsl_debug_console.h"
22 
23 //-----------------------------------------------------------------------
24 // CMSIS Includes
25 //-----------------------------------------------------------------------
26 #include "Driver_I2C.h"
27 
28 /* ISSDK Includes */
29 #include "issdk_hal.h"
30 #include "mpl3115_drv.h"
31 
32 //-----------------------------------------------------------------------
33 // Macros
34 //-----------------------------------------------------------------------
35 #define MPL3115_DATA_SIZE (5) /* 3 byte Pressure/Altitude and 2 byte Temperature. */
36 /*! In MPL3115 the Auto Acquisition Time Step (ODR) can be set only in powers of 2 (i.e. 2^x, where x is the
37  * SAMPLING_EXPONENT).
38  * This gives a range of 1 second to 2^15 seconds (9 hours). */
39 #define MPL3115_SAMPLING_EXPONENT (1) /* 2 seconds */
40 
41 //-----------------------------------------------------------------------
42 // Constants
43 //-----------------------------------------------------------------------
44 /*! @brief Register settings for Normal (non buffered) mode. */
46  /* Enable Data Ready and Event flags for Pressure, Temperature or either. */
50  /* Set Over Sampling Ratio to 128. */
52  /* Set Auto acquisition time step. */
55 
56 /*! @brief Address of Status Register. */
58 
59 /*! @brief Address and size of Raw Pressure+Temperature Data in Normal Mode. */
62 
63 //-----------------------------------------------------------------------
64 // Functions
65 //-----------------------------------------------------------------------
66 /*!
67  * @brief Main function
68  */
69 int main(void)
70 {
71  int16_t tempInDegrees;
72  uint32_t pressureInPascals;
74  uint8_t dataReady;
75  uint8_t data[MPL3115_DATA_SIZE];
77 
78  ARM_DRIVER_I2C *I2Cdrv = &I2C_S_DRIVER; // Now using the shield.h value!!!
79  mpl3115_i2c_sensorhandle_t mpl3115Driver;
80 
84 
85  PRINTF("\r\n ISSDK MPL3115 sensor driver example demonstration with poll mode\r\n");
86 
87  /*! Initialize the I2C driver. */
88  status = I2Cdrv->Initialize(I2C_S_SIGNAL_EVENT);
89  if (ARM_DRIVER_OK != status)
90  {
91  PRINTF("\r\n I2C Initialization Failed\r\n");
92  return -1;
93  }
94 
95  /*! Set the I2C Power mode. */
96  status = I2Cdrv->PowerControl(ARM_POWER_FULL);
97  if (ARM_DRIVER_OK != status)
98  {
99  PRINTF("\r\n I2C Power Mode setting Failed\r\n");
100  return -1;
101  }
102 
103  /*! Set the I2C bus speed. */
104  status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
105  if (ARM_DRIVER_OK != status)
106  {
107  PRINTF("\r\n I2C Control Mode setting Failed\r\n");
108  return -1;
109  }
110 
111  /*! Initialize MPL3115 sensor driver. */
114  if (SENSOR_ERROR_NONE != status)
115  {
116  PRINTF("\r\n Sensor Initialization Failed\r\n");
117  return -1;
118  }
119  PRINTF("\r\n Successfully Initiliazed Sensor\r\n");
120 
121  /*! Set the task to be executed while waiting for I2C transactions to complete. */
123 
124  /*! Configure the MPL3115 sensor. */
125  status = MPL3115_I2C_Configure(&mpl3115Driver, cMpl3115ConfigNormal);
126  if (SENSOR_ERROR_NONE != status)
127  {
128  PRINTF("\r\nMPL3115 configuration failed...\r\n");
129  return -1;
130  }
131  PRINTF("\r\n Successfully Applied MPL3115 Sensor Configuration\r\n");
132 
133  for (;;) /* Forever loop */
134  {
135  /*! Wait for data ready from the MPL3115. */
136  status = MPL3115_I2C_ReadData(&mpl3115Driver, cMpl3115Status, &dataReady);
137  if (0 == (dataReady & MPL3115_DR_STATUS_PTDR_MASK))
138  { /* Loop, if new sample is not available. */
139  continue;
140  }
141 
142  /*! Read new raw sensor data from the MPL3115. */
143  status = MPL3115_I2C_ReadData(&mpl3115Driver, cMpl3115OutputNormal, data);
144  if (ARM_DRIVER_OK != status)
145  {
146  PRINTF("\r\n Read Failed. \r\n");
147  return -1;
148  }
149 
150  /*! Process the sample and convert the raw sensor data. */
151  rawData.pressure = (uint32_t)((data[0]) << 16) | ((data[1]) << 8) | ((data[2]));
152  pressureInPascals = rawData.pressure / MPL3115_PRESSURE_CONV_FACTOR;
153 
154  rawData.temperature = (int16_t)((data[3]) << 8) | (data[4]);
155  tempInDegrees = rawData.temperature / MPL3115_TEMPERATURE_CONV_FACTOR;
156 
157  PRINTF("\r\nPressure = %d Pa\r\n", pressureInPascals);
158  PRINTF("\r\nTemperature = %d degC\r\n", tempInDegrees);
159  ASK_USER_TO_RESUME(8); /* Ask for user input after processing 8 samples. */
160  }
161 }
#define MPL3115_SAMPLING_EXPONENT
This structure defines the Write command List.
Definition: sensor_drv.h:68
#define ASK_USER_TO_RESUME(x)
Definition: frdm_k64f.h:106
int32_t status
int main(void)
Main function.
void MPL3115_I2C_SetIdleTask(mpl3115_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
Definition: mpl3115_drv.c:53
#define MPL3115_PRESSURE_CONV_FACTOR
Definition: mpl3115_drv.h:28
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
Definition: lpc54114.c:169
int32_t MPL3115_I2C_ReadData(mpl3115_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
Definition: mpl3115_drv.c:104
The mpl3115_drv.h file describes the MPL3115 driver interface and structures.
#define MPL3115_CTRL_REG2_ST_MASK
Definition: mpl3115.h:916
#define SMC
Definition: lpc54114.h:118
#define __END_WRITE_DATA__
Definition: sensor_drv.h:45
#define MPL3115_PT_DATA_CFG_TDEFE_MASK
Definition: mpl3115.h:550
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
#define I2C_S_SIGNAL_EVENT
Definition: issdk_hal.h:34
#define I2C_S_DRIVER
Definition: issdk_hal.h:33
#define MPL3115_DR_STATUS_PTDR_MASK
Definition: mpl3115.h:195
const registerwritelist_t cMpl3115ConfigNormal[]
Register settings for Normal (non buffered) mode.
#define BOARD_BootClockRUN
Definition: clock_config.h:19
#define MPL3115_TEMPERATURE_CONV_FACTOR
Definition: mpl3115_drv.h:30
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
Definition: sensor_drv.h:97
This structure defines the mpl3115 data buffer in Pressure Mode.
Definition: mpl3115_drv.h:45
#define MPL3115_PT_DATA_CFG_DREM_ENABLED
Definition: mpl3115.h:570
uint8_t data[FXLS8962_DATA_SIZE]
#define MPL3115_DATA_SIZE
#define MPL3115_PT_DATA_CFG_PDEFE_MASK
Definition: mpl3115.h:553
#define __END_READ_DATA__
Definition: sensor_drv.h:51
This defines the sensor specific information.
Definition: mpl3115_drv.h:36
#define MPL3115_CTRL_REG1_OS_OSR_128
Definition: mpl3115.h:884
ARM_DRIVER_I2C * I2Cdrv
fxos8700_accelmagdata_t rawData
int32_t MPL3115_I2C_Initialize(mpl3115_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
Definition: mpl3115_drv.c:22
uint16_t readFrom
Definition: sensor_drv.h:80
#define MPL3115_PT_DATA_CFG_DREM_MASK
Definition: mpl3115.h:556
#define MPL3115_PT_DATA_CFG_PDEFE_ENABLED
Definition: mpl3115.h:567
#define MPL3115_WHOAMI_VALUE
Definition: mpl3115.h:65
This structure defines the Read command List.
Definition: sensor_drv.h:78
const registerreadlist_t cMpl3115Status[]
Address of Status Register.
#define MPL3115_PT_DATA_CFG_TDEFE_ENABLED
Definition: mpl3115.h:564
#define I2C_S_DEVICE_INDEX
Definition: issdk_hal.h:35
#define MPL3115_I2C_ADDR
void BOARD_InitDebugConsole(void)
Definition: board.c:15
const registerreadlist_t cMpl3115OutputNormal[]
Address and size of Raw Pressure+Temperature Data in Normal Mode.
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
Definition: pin_mux.c:47
int32_t MPL3115_I2C_Configure(mpl3115_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
Definition: mpl3115_drv.c:61
#define MPL3115_CTRL_REG1_OS_MASK
Definition: mpl3115.h:855