46 #include "clock_config.h" 51 #include "Driver_I2C.h" 52 #include "Driver_USART.h" 57 #include "issdk_hal.h" 58 #include "gpio_driver.h" 62 #include "auto_detection_service.h" 67 #define RAW_ACCEL_MAG_DATA_SIZE 12 68 #define FXOS8700_STREAM_DATA_SIZE 17 71 #define APPLICATION_NAME "FXOS8700 6-axis (Accel, Mag) Demo" 73 #define APPLICATION_VERSION "2.5" 167 uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse,
size_t *hostMsgSize,
size_t respBufferSize)
169 bool success =
false;
184 if (respBufferSize >= boardNameLen + shieldNameLen + appNameLen + 3)
193 hostResponse[*hostMsgSize] = appNameLen;
196 memcpy(hostResponse + *hostMsgSize,
embAppName, appNameLen);
197 *hostMsgSize += appNameLen;
199 hostResponse[*hostMsgSize] = boardNameLen;
202 memcpy(hostResponse + *hostMsgSize,
boardString, boardNameLen);
203 *hostMsgSize += boardNameLen;
205 hostResponse[*hostMsgSize] = shieldNameLen;
208 memcpy(hostResponse + *hostMsgSize,
shieldString, shieldNameLen);
209 *hostMsgSize += shieldNameLen;
219 switch (hostCommand[0])
278 if (ARM_DRIVER_OK != status)
284 status = I2Cdrv->PowerControl(ARM_POWER_FULL);
285 if (ARM_DRIVER_OK != status)
291 status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
292 if (ARM_DRIVER_OK != status)
299 if (ARM_DRIVER_OK != status)
305 status = pUartDriver->PowerControl(ARM_POWER_FULL);
306 if (ARM_DRIVER_OK != status)
313 if (ARM_DRIVER_OK != status)
365 if (ARM_DRIVER_OK != status)
377 if (ARM_DRIVER_OK != status)
386 rawData.
accel[0] = ((int16_t)data[0] << 8) | data[1];
387 rawData.
accel[0] /= 4;
388 rawData.
accel[1] = ((int16_t)data[2] << 8) | data[3];
389 rawData.
accel[1] /= 4;
390 rawData.
accel[2] = ((int16_t)data[4] << 8) | data[5];
391 rawData.
accel[2] /= 4;
392 rawData.
mag[0] = ((int16_t)data[6] << 8) | data[7];
393 rawData.
mag[1] = ((int16_t)data[8] << 8) | data[9];
394 rawData.
mag[2] = ((int16_t)data[10] << 8) | data[11];
400 if((regdata & 0x04) == 0x04)
405 else if((regdata & 0x02) == 0x02)
#define FXOS8700_M_CTRL_REG1_M_HMS_MASK
uint32_t BOARD_SystickElapsedTime_us(int32_t *pStart)
Function to compute the Elapsed Time.
#define FXOS8700_PL_CFG_DBCNTM_MASK
#define FXOS8700_M_CTRL_REG1_M_ACAL_EN
GENERIC_DRIVER_GPIO * pGpioDriver
#define FXOS8700_PL_CFG_DBCNTM_CLEAR_MODE
#define __END_WRITE_DATA__
The fxos8700_drv.h file describes the fxos8700 driver interface and structures.
const registerreadlist_t cFXOS8700_ffmt_src[]
#define HOST_PRO_CMD_W_CFG_TAG
void FXOS8700_I2C_SetIdleTask(fxos8700_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
#define FXOS8700_CTRL_REG2_MODS_HIGH_RES
#define APPLICATION_NAME
Unique Name for this application which should match the target GUI pkg name.
#define HOST_S_SIGNAL_EVENT
void Host_IO_Receive(host_cmd_proc_fn_t process_host_command, uint8_t encoding)
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
#define BOARD_BootClockRUN
bool process_host_command(uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse, size_t *hostMsgSize, size_t respBufferSize)
#define RAW_ACCEL_MAG_DATA_SIZE
#define FXOS8700_PL_CFG_PL_EN_ENABLE
#define FXOS8700_A_FFMT_CFG_ZEFE_RAISE_EVENT
uint8_t data[FXLS8962_DATA_SIZE]
#define FXOS8700_A_VECM_THS_MSB_A_VBECM_THS_MASK
This structure defines the fxos8700 raw data buffer.
void(* toggle_pin)(pinID_t aPinId)
#define FXOS8700_XYZ_DATA_CFG_FS_2G_0P244
ARM_DRIVER_I2C * pCommDrv
const registerreadlist_t cFXOS8700_pl_status[]
#define FXOS8700_A_FFMT_CFG_OAE_FREEFALL
#define ADS_MAX_STRING_LENGTH
const registerreadlist_t cFXOS8700_int_src[]
const registerreadlist_t FXOS8700_STATUS_READ[]
#define HOST_PRO_INT_DEV_TAG
uint8_t streamingPacket[STREAMING_HEADER_LEN+FXLS8962_STREAM_DATA_SIZE]
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
This defines the sensor specific information for I2C.
int main(void)
Main function.
#define HOST_PRO_INT_CMD_TAG
Bit aligned values for Host Protocol Interface IDs (Bits 5-6).
volatile bool bFxos8700Ready
char embAppName[ADS_MAX_STRING_LENGTH]
#define __END_READ_DATA__
#define FXOS8700_A_VECM_THS_MSB_A_VBECM_DBCNTM_MASK
#define FXOS8700_CTRL_REG2_MODS_MASK
#define FXOS8700_WHO_AM_I_PROD_VALUE
#define FXOS8700_A_FFMT_CFG_ZEFE_MASK
gpioHandleKSDK_t GREEN_LED
char shieldString[ADS_MAX_STRING_LENGTH]
#define FXOS8700_M_CTRL_REG2_M_AUTOINC_MASK
const registerwritelist_t fxos8700_Config_InterruptHybrid[]
#define FXOS8700_M_CTRL_REG1_M_ACAL_MASK
const registerreadlist_t FXOS8700_ACCEL_READ[]
#define FXOS8700_CTRL_REG1_DR_HYBRID_100_HZ
#define FXOS8700_A_FFMT_CFG_XEFE_MASK
#define APPLICATION_VERSION
Version to distinguish between instances the same application based on target Shield and updates...
void Host_IO_Add_ISO_Header(uint8_t streamID, uint8_t *pStreamingPacket, size_t sizePayload)
void Host_IO_Send(uint8_t *pMsg, size_t size, uint8_t encoding)
void(* clr_pin)(pinID_t aPinId)
int32_t FXOS8700_I2C_Initialize(fxos8700_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
void BOARD_SystickEnable(void)
Function to enable systicks framework.
int32_t FXOS8700_I2C_ReadData(fxos8700_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
registerDeviceInfo_t deviceInfo
#define FXOS8700_M_CTRL_REG2_M_AUTOINC_HYBRID_MODE
#define I2C_S_DEVICE_INDEX
#define FXOS8700_A_FFMT_CFG_YEFE_RAISE_EVENT
#define FXOS8700_PL_BF_ZCOMP_ZLOCK_MASK
#define FXOS8700_M_CTRL_REG1_M_OS_MASK
#define FXOS8700_A_FFMT_THS_THS_MASK
#define FXOS8700_A_FFMT_CFG_YEFE_MASK
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
int32_t FXOS8700_I2C_Configure(fxos8700_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
#define BOARD_DEBUG_UART_BAUDRATE
volatile bool bStreamingEnabled
#define FXOS8700_CTRL_REG1_DR_MASK
#define FXOS8700_XYZ_DATA_CFG_FS_MASK
Access structure of the GPIO Driver.
void BOARD_SystickStart(int32_t *pStart)
Function to Record the Start systick.
void BOARD_RunADS(const char *appName, char *boardString, char *shieldString, size_t bufferLength)
The function to register Application Name and initialte ADS.
fxls8962_acceldataUser_t rawData
#define FXOS8700_DR_STATUS_ZYXDR_MASK
uint8_t Host_IO_Init(ARM_DRIVER_USART *pDrv, void *pBus, void *pDevInfo, void *spiSlaveParams, uint16_t slaveAddress)
#define FXOS8700_STREAM_DATA_SIZE
#define FXOS8700_A_FFMT_CFG_OAE_MASK
This structure defines the Write command List.
This structure defines the Read command List.
#define FXOS8700_M_CTRL_REG1_M_OS_OSR0
The host_io_uart.h file contains the Host Protocol interface definitions and configuration.
#define STREAMING_HEADER_LEN
#define FXOS8700_PL_CFG_PL_EN_MASK
#define FXOS8700_PL_BF_ZCOMP_BKFR_MASK
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
#define FXOS8700_A_FFMT_CFG_XEFE_RAISE_EVENT
#define FXOS8700_I2C_ADDR
#define FXOS8700_M_CTRL_REG1_M_HMS_HYBRID_MODE
#define I2C_S_SIGNAL_EVENT
char boardString[ADS_MAX_STRING_LENGTH]