46 #include "clock_config.h" 51 #include "Driver_I2C.h" 52 #include "Driver_USART.h" 57 #include "issdk_hal.h" 59 #include "gpio_driver.h" 62 #include "auto_detection_service.h" 67 #define MMA865x_ACCEL_DATA_SIZE 6 68 #define MMA865x_STREAM_DATA_SIZE 11 71 #define APPLICATION_NAME "MMA8652 Accelerometer Demo" 73 #define APPLICATION_VERSION "2.5" 157 uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse,
size_t *hostMsgSize,
size_t respBufferSize)
159 bool success =
false;
174 if (respBufferSize >= boardNameLen + shieldNameLen + appNameLen + 3)
183 hostResponse[*hostMsgSize] = appNameLen;
186 memcpy(hostResponse + *hostMsgSize,
embAppName, appNameLen);
187 *hostMsgSize += appNameLen;
189 hostResponse[*hostMsgSize] = boardNameLen;
192 memcpy(hostResponse + *hostMsgSize,
boardString, boardNameLen);
193 *hostMsgSize += boardNameLen;
195 hostResponse[*hostMsgSize] = shieldNameLen;
198 memcpy(hostResponse + *hostMsgSize,
shieldString, shieldNameLen);
199 *hostMsgSize += shieldNameLen;
209 switch (hostCommand[0])
271 if (ARM_DRIVER_OK != status)
277 status = pI2Cdriver->PowerControl(ARM_POWER_FULL);
278 if (ARM_DRIVER_OK != status)
284 status = pI2Cdriver->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
285 if (ARM_DRIVER_OK != status)
292 if (ARM_DRIVER_OK != status)
298 status = pUartDriver->PowerControl(ARM_POWER_FULL);
299 if (ARM_DRIVER_OK != status)
306 if (ARM_DRIVER_OK != status)
362 if (ARM_DRIVER_OK != status)
371 rawData.
accel[0] = ((int16_t)data[0] << 8) | data[1];
372 rawData.
accel[0] /= 16;
373 rawData.
accel[1] = ((int16_t)data[2] << 8) | data[3];
374 rawData.
accel[1] /= 16;
375 rawData.
accel[2] = ((int16_t)data[4] << 8) | data[5];
376 rawData.
accel[2] /= 16;
383 rawData.
intsrc = intsrcdata;
uint32_t BOARD_SystickElapsedTime_us(int32_t *pStart)
Function to compute the Elapsed Time.
#define MMA865x_CTRL_REG3_IPOL_MASK
#define MMA865x_XYZ_DATA_CFG_FS_MASK
#define __END_WRITE_DATA__
int32_t MMA865x_I2C_Initialize(mma865x_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
#define HOST_PRO_CMD_W_CFG_TAG
#define MMA865x_TRANSIENT_THS_DBCNTM_INC_CLR
#define HOST_S_SIGNAL_EVENT
#define MMA865x_PULSE_CFG_ZSPEFE_EN
volatile bool bMma865xDataReady
void Host_IO_Receive(host_cmd_proc_fn_t process_host_command, uint8_t encoding)
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
#define BOARD_BootClockRUN
#define MMA865x_CTRL_REG3_IPOL_ACTIVE_HIGH
uint8_t data[FXLS8962_DATA_SIZE]
int32_t MMA865x_I2C_ReadData(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
#define MMA865x_TRANSIENT_CFG_ZTEFE_EN
void(* toggle_pin)(pinID_t aPinId)
GENERIC_DRIVER_GPIO * pGpioDriver
volatile bool bMma865xReady
const registerreadlist_t cMma865xOutputValues[]
#define MMA865x_PL_CFG_PL_EN_EN
#define MMA865x_ACCEL_DATA_SIZE
#define ADS_MAX_STRING_LENGTH
This defines the sensor specific information.
registerDeviceInfo_t deviceInfo
#define HOST_PRO_INT_DEV_TAG
uint8_t streamingPacket[STREAMING_HEADER_LEN+FXLS8962_STREAM_DATA_SIZE]
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
#define HOST_PRO_INT_CMD_TAG
Bit aligned values for Host Protocol Interface IDs (Bits 5-6).
const registerreadlist_t cMma8652qStatus[]
#define MMA865x_CTRL_REG1_DR_MASK
#define __END_READ_DATA__
#define MMA865x_CTRL_REG4_INT_EN_LNDPRT_EN
volatile bool bStreamingEnabled
#define MMA865x_CTRL_REG1_DR_100HZ
void MMA865x_I2C_SetIdleTask(mma865x_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
#define MMA8652_WHOAMI_VALUE
#define MMA865x_CTRL_REG4_INT_EN_FF_MT_EN
gpioHandleKSDK_t GREEN_LED
#define MMA865x_FF_MT_CFG_OAE_FREEFALL
#define MMA865x_CTRL_REG4_INT_EN_DRDY_EN
int32_t MMA865x_I2C_Configure(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
#define MMA865x_FF_MT_CFG_XEFE_EN
#define MMA865x_XYZ_DATA_CFG_FS_2G
void Host_IO_Add_ISO_Header(uint8_t streamID, uint8_t *pStreamingPacket, size_t sizePayload)
void Host_IO_Send(uint8_t *pMsg, size_t size, uint8_t encoding)
char boardString[ADS_MAX_STRING_LENGTH]
void(* clr_pin)(pinID_t aPinId)
#define MMA865x_CTRL_REG2_MODS_MASK
#define MMA865x_FF_MT_CFG_ZEFE_EN
void mma865x_int_data_ready_callback(void *pUserData)
void BOARD_SystickEnable(void)
Function to enable systicks framework.
#define MMA865x_CTRL_REG4_INT_EN_PULSE_EN
#define MMA865x_STREAM_DATA_SIZE
char shieldString[ADS_MAX_STRING_LENGTH]
#define MMA865x_PL_CFG_DBCNTM_CLEAR
#define I2C_S_DEVICE_INDEX
#define MMA865x_PULSE_CFG_YSPEFE_EN
#define MMA865x_PULSE_CFG_XSPEFE_EN
#define APPLICATION_VERSION
Version to distinguish between instances the same application based on target Shield and updates...
#define MMA865x_CTRL_REG5_INT_CFG_DRDY_INT1
const registerreadlist_t cMma8652qPLStatus[]
The mma865x_drv.h file describes the MMA865x driver interface and structures.
int main(void)
Main function.
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
#define MMA865x_TRANSIENT_CFG_XTEFE_EN
#define MMA865x_FF_MT_THS_DBCNTM_INC_CLR
#define BOARD_DEBUG_UART_BAUDRATE
bool process_host_command(uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse, size_t *hostMsgSize, size_t respBufferSize)
Access structure of the GPIO Driver.
void BOARD_SystickStart(int32_t *pStart)
Function to Record the Start systick.
void BOARD_RunADS(const char *appName, char *boardString, char *shieldString, size_t bufferLength)
The function to register Application Name and initialte ADS.
fxls8962_acceldataUser_t rawData
uint8_t Host_IO_Init(ARM_DRIVER_USART *pDrv, void *pBus, void *pDevInfo, void *spiSlaveParams, uint16_t slaveAddress)
#define MMA865x_CTRL_REG2_MODS_HR
This structure defines the Write command List.
This structure defines the Read command List.
#define MMA865x_FF_MT_CFG_YEFE_EN
The host_io_uart.h file contains the Host Protocol interface definitions and configuration.
#define MMA865x_CTRL_REG4_INT_EN_TRANS_EN
#define STREAMING_HEADER_LEN
char embAppName[ADS_MAX_STRING_LENGTH]
const registerwritelist_t cMma865xConfigInterrupt[]
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
#define MMA865x_TRANSIENT_CFG_YTEFE_EN
#define I2C_S_SIGNAL_EVENT
#define APPLICATION_NAME
Unique Name for this application which should match the target GUI pkg name.
ARM_DRIVER_I2C * pCommDrv