46 #include "clock_config.h"    51 #include "Driver_I2C.h"    52 #include "Driver_USART.h"    57 #include "issdk_hal.h"    58 #include "gpio_driver.h"    62 #include "auto_detection_service.h"    67 #define MPL3115_T_ON_MAX 1000           68 #define MPL3115_DATA_SIZE 5             69 #define MPL3115_STREAM_DATA_SIZE 10     70 #define LED_TOGGLE_RATE 100             73 #define APPLICATION_NAME "Digital Pressure Altimeter Demo (MPL3115)"    75 #define APPLICATION_VERSION "2.5"   118     uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse, 
size_t *hostMsgSize, 
size_t respBufferSize)
   120     bool success = 
false;
   135         if (respBufferSize >= boardNameLen + shieldNameLen + appNameLen + 3)
   144         hostResponse[*hostMsgSize] = appNameLen;
   147         memcpy(hostResponse + *hostMsgSize, 
embAppName, appNameLen);
   148         *hostMsgSize += appNameLen;
   150         hostResponse[*hostMsgSize] = boardNameLen;
   153         memcpy(hostResponse + *hostMsgSize, 
boardString, boardNameLen);
   154         *hostMsgSize += boardNameLen;
   156         hostResponse[*hostMsgSize] = shieldNameLen;
   159         memcpy(hostResponse + *hostMsgSize, 
shieldString, shieldNameLen);
   160         *hostMsgSize += shieldNameLen;
   170         switch (hostCommand[0]) 
   203     uint8_t dataReady, toggle_led = 0;
   230     if (ARM_DRIVER_OK != status)
   236     status = pI2cDriver->PowerControl(ARM_POWER_FULL);
   237     if (ARM_DRIVER_OK != status)
   243     status = pI2cDriver->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   244     if (ARM_DRIVER_OK != status)
   251     if (ARM_DRIVER_OK != status)
   257     status = pUartDriver->PowerControl(ARM_POWER_FULL);
   258     if (ARM_DRIVER_OK != status)
   265     if (ARM_DRIVER_OK != status)
   281         if (ARM_DRIVER_OK == status)
   316         if (ARM_DRIVER_OK != status)
   324             if (ARM_DRIVER_OK != status)
   335         if (ARM_DRIVER_OK != status)
   344         rawData.
pressure = (uint32_t)((data[0]) << 16) | ((data[1]) << 8) | ((data[2]));
   345         rawData.
temperature = (int16_t)((data[3]) << 8) | (data[4]);
 registerDeviceInfo_t deviceInfo
 
uint32_t BOARD_SystickElapsedTime_us(int32_t *pStart)
Function to compute the Elapsed Time. 
 
#define MPL3115_CTRL_REG1_SBYB_MASK
 
ARM_DRIVER_I2C * pCommDrv
 
#define __END_WRITE_DATA__
 
#define HOST_PRO_CMD_W_CFG_TAG
 
char boardString[ADS_MAX_STRING_LENGTH]
 
#define MPL3115_DATA_SIZE
 
int32_t MPL3115_I2C_Initialize(mpl3115_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
#define HOST_S_SIGNAL_EVENT
 
void Host_IO_Receive(host_cmd_proc_fn_t process_host_command, uint8_t encoding)
 
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
 
#define BOARD_BootClockRUN
 
uint8_t data[FXLS8962_DATA_SIZE]
 
int32_t MPL3115_I2C_ReadData(mpl3115_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
#define MPL3115_CTRL_REG1_ALT_MASK
 
#define MPL3115_CTRL_REG1_OST_SET
 
void(* toggle_pin)(pinID_t aPinId)
 
#define MPL3115_PT_DATA_CFG_PDEFE_ENABLED
 
#define ADS_MAX_STRING_LENGTH
 
#define APPLICATION_VERSION
Version to distinguish between instances the same application based on target Shield and updates...
 
#define MPL3115_CTRL_REG1_OST_MASK
 
#define HOST_PRO_INT_DEV_TAG
 
uint8_t streamingPacket[STREAMING_HEADER_LEN+FXLS8962_STREAM_DATA_SIZE]
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
#define HOST_PRO_INT_CMD_TAG
Bit aligned values for Host Protocol Interface IDs (Bits 5-6). 
 
#define __END_READ_DATA__
 
void MPL3115_I2C_SetIdleTask(mpl3115_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
volatile bool bMpl3115Ready
 
#define MPL3115_PT_DATA_CFG_DREM_ENABLED
 
#define MPL3115_CTRL_REG1_OS_OSR_2
 
#define MPL3115_CTRL_REG1_OS_MASK
 
char embAppName[ADS_MAX_STRING_LENGTH]
 
#define MPL3115_PT_DATA_CFG_PDEFE_MASK
 
#define MPL3115_PT_DATA_CFG_TDEFE_ENABLED
 
#define MPL3115_WHOAMI_VALUE
 
#define MPL3115_STREAM_DATA_SIZE
 
const registerreadlist_t cMpl3115GetOST[]
Address of Register containing OST Bit. 
 
gpioHandleKSDK_t GREEN_LED
 
This defines the sensor specific information. 
 
GENERIC_DRIVER_GPIO * pGpioDriver
 
const registerwritelist_t cMpl3115SetOST[]
Register settings for Triggring One-Shot Sampling. 
 
const registerreadlist_t cMpl3115OutputNormal[]
Address and size of Raw Pressure+Temperature Data in Normal Mode. 
 
int main(void)
Main function. 
 
char shieldString[ADS_MAX_STRING_LENGTH]
 
void Host_IO_Add_ISO_Header(uint8_t streamID, uint8_t *pStreamingPacket, size_t sizePayload)
 
void Host_IO_Send(uint8_t *pMsg, size_t size, uint8_t encoding)
 
void(* clr_pin)(pinID_t aPinId)
 
void BOARD_SystickEnable(void)
Function to enable systicks framework. 
 
#define I2C_S_DEVICE_INDEX
 
bool process_host_command(uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse, size_t *hostMsgSize, size_t respBufferSize)
 
#define MPL3115_CTRL_REG1_ALT_BAR
 
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
 
volatile bool bStreamingEnabled
 
#define BOARD_DEBUG_UART_BAUDRATE
 
The mpl3115_drv.h file describes the MPL3115 driver interface and structures. 
 
const registerwritelist_t cMpl3115ConfigPoll[]
Register settings for Interrupt (non buffered) Enablement with ONe-Shot Mode. 
 
Access structure of the GPIO Driver. 
 
#define APPLICATION_NAME
Unique Name for this application which should match the target GUI pkg name. 
 
void BOARD_SystickStart(int32_t *pStart)
Function to Record the Start systick. 
 
void BOARD_RunADS(const char *appName, char *boardString, char *shieldString, size_t bufferLength)
The function to register Application Name and initialte ADS. 
 
fxls8962_acceldataUser_t rawData
 
#define MPL3115_CTRL_REG1_SBYB_STANDBY
 
uint8_t Host_IO_Init(ARM_DRIVER_USART *pDrv, void *pBus, void *pDevInfo, void *spiSlaveParams, uint16_t slaveAddress)
 
This structure defines the Write command List. 
 
This structure defines the Read command List. 
 
The host_io_uart.h file contains the Host Protocol interface definitions and configuration. 
 
#define STREAMING_HEADER_LEN
 
#define MPL3115_PT_DATA_CFG_DREM_MASK
 
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
 
#define MPL3115_PT_DATA_CFG_TDEFE_MASK
 
This structure defines the mpl3115 data buffer in Pressure Mode. 
 
#define MPL3115_CTRL_REG1_OST_RESET
 
#define I2C_S_SIGNAL_EVENT
 
int32_t Sensor_I2C_Write(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerwritelist_t *pRegWriteList)
Write register data to a sensor.