45 #include "clock_config.h"    46 #include "fsl_debug_console.h"    51 #include "Driver_I2C.h"    56 #include "issdk_hal.h"    58 #include "gpio_driver.h"    64 #define SDCD_LTHS_LSB 0xA0        65 #define SDCD_LTHS_MSB 0x0F        66 #define SDCD_UTHS_LSB 0x40        67 #define SDCD_UTHS_MSB 0x00        68 #define ASLP_COUNT_LSB 0xFA       69 #define ASLP_COUNT_MSB 0x00       70 #define FXLS8962_DATA_SIZE 6     124 const char *
pActivity[5] = {
"Unknown ", 
"Rest    ", 
"Walking ", 
"Jogging ", 
"Running "};
   135     .bits = {.config = 1},
   144             .filtertime = 2, .male = 1,
   157     .portPinConfig = {.pullSelect = kPORT_PullUp, .mux = kPORT_MuxAsGpio},
   158     .interruptMode = kPORT_InterruptFallingEdge,
   190     uint16_t lastReportedSteps;
   205     PRINTF(
"\r\n ISSDK FXLS8962 sensor driver example for Motion Activated Pedometer.\r\n");
   215     if (ARM_DRIVER_OK != status)
   217         PRINTF(
"\r\n I2C Initialization Failed\r\n");
   222     status = I2Cdrv->PowerControl(ARM_POWER_FULL);
   223     if (ARM_DRIVER_OK != status)
   225         PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
   230     status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   231     if (ARM_DRIVER_OK != status)
   233         PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
   242         PRINTF(
"\r\n Sensor Initialization Failed\r\n");
   251                               fxls8962Driver.
slaveAddress, cFxls8962ConfigInitialize);
   254         PRINTF(
"\r\n Write FXLS8962 Initialization Failed.\r\n");
   260     PRINTF(
"\r\n Pedometer successfully Initialized and Ready for measurements.");
   271             PRINTF(
"\r\n Write FXLS8962 Motion Configuration Failed!\r\n");
   277         PRINTF(
"\r\n\r\n Waiting for Motion | MCU switching to Sleep Mode ...\r\n");
   294             if (ARM_DRIVER_OK != status)
   296                 PRINTF(
"\r\n Read INT Status Failed!\r\n");
   305                     PRINTF(
" Motion detected...\r\n");
   311                         PRINTF(
"\r\n Write FXLS8962 DRDY Configuration Failed.\r\n");
   314                     motionDetect = 
false;
   322                 if (ARM_DRIVER_OK != status)
   324                     PRINTF(
"\r\n ERROR : Read Data Failed!\r\n");
   329                 rawData.
accel[0] = ((int16_t)data[1] << 8) | data[0];
   330                 rawData.
accel[0] *= 16; 
   331                 rawData.
accel[1] = ((int16_t)data[3] << 8) | data[2];
   332                 rawData.
accel[1] *= 16; 
   333                 rawData.
accel[2] = ((int16_t)data[5] << 8) | data[4];
   334                 rawData.
accel[2] *= 16; 
   346                         PRINTF(
"\r\n | Steps | Distance |  Speed  | Calories | Activity |\r\n");
   348                     PRINTF(
"\033[K | %5d |    %4dm |  %2dkmph |      %3d | %s |\r",
 const registerwritelist_t cFxls8962ConfigInitialize[]
FXLS8962 Motion based Pedometer Register Write List. 
 
void fxls8962_int_callback(void *pUserData)
This is the Sensor Event Ready ISR implementation. 
 
void pedometer_init(pedometer_t *pPedometer)
The interface function initialize the pedometer. 
 
This defines the configuration structure of the pedometer. 
 
#define FXLS8962_SENS_CONFIG4_WK_SDCD_OT_MASK
 
The pedometer.h file contains the interface and structure definitions for pedometer application...
 
This structure defines the fxls8962 raw data buffer. 
 
#define FXLS8962_SDCD_CONFIG1_Z_OT_EN_EN
 
#define __END_WRITE_DATA__
 
const registerreadlist_t cFxls8962INTStatus[]
Address of INT Status Register. 
 
int32_t FXLS8962_I2C_Initialize(fxls8962_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
#define FXLS8962_SENS_CONFIG3_WAKE_ODR_50HZ
 
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
 
const char * pActivity[5]
Pedometer Mode Name Strings. 
 
#define BOARD_BootClockRUN
 
const registerwritelist_t cFxls8962ConfigDataReady[]
FXLS8962 DRDY and ASLP Detect Mode Register Write List. 
 
#define FXLS8962_SDCD_CONFIG1_Y_OT_EN_EN
 
This defines the sensor specific information for I2C. 
 
const registerreadlist_t cFxls8962Output[]
Address of Data Output Registers. 
 
uint8_t data[FXLS8962_DATA_SIZE]
 
int32_t FXLS8962_I2C_Configure(fxls8962_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
#define FXLS8962_SDCD_CONFIG2_SDCD_EN_EN
 
void(* toggle_pin)(pinID_t aPinId)
 
This defines the acceleration input data for the pedometer. 
 
volatile bool gFxls8962EventReady
 
The GPIO Configuration KSDK. 
 
void FXLS8962_I2C_SetIdleTask(fxls8962_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
#define FXLS8962_SENS_CONFIG3_SLEEP_ODR_MASK
 
void BOARD_InitDebugConsole(void)
 
#define FXLS8962_SDCD_CONFIG1_X_OT_EN_EN
 
#define FXLS8962_SENS_CONFIG4_INT_POL_ACT_LOW
 
registerDeviceInfo_t deviceInfo
 
#define FXLS8962_SDCD_CONFIG2_WT_DBCTM_CLEARED
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
fxls8962_i2c_sensorhandle_t fxls8962Driver
 
#define __END_READ_DATA__
 
This defines the pedometer instance. 
 
GENERIC_DRIVER_GPIO * pGpioDriver
 
#define FXLS8962_SDCD_CONFIG2_OT_DBCTM_CLEARED
 
#define FXLS8962_INT_EN_SDCD_OT_EN_EN
 
#define FXLS8962_I2C_ADDR
 
pedometer_config_t cPedoConfig
 
#define FXLS8962_SENS_CONFIG4_INT_POL_MASK
 
gpioHandleKSDK_t GREEN_LED
 
#define FXLS8962_SENS_CONFIG3_WAKE_ODR_MASK
 
debounce_count_t sleepcount_threshold
 
union pedometer_t::pedometer_status_tag::@292 status
 
gpio_pin_config_t pinConfig
 
const registerwritelist_t cFxls8962ConfigMotionDetect[]
FXLS8962 Motion Detect Mode Register Write List. 
 
void(* set_pin)(pinID_t aPinId)
 
void(* clr_pin)(pinID_t aPinId)
 
void pedometer_configure(pedometer_t *pPedometer, const pedometer_config_t *pConfig)
The interface function to configure the pedometer. 
 
#define FXLS8962_SDCD_CONFIG2_REF_UPDM_SDCD_REF
 
The fxls8962_drv.h file describes the FXLS8962AF driver interface and structures. ...
 
int32_t pedometer_run(pedometer_t *pPedometer, ped_accel_t *pData)
The interface function excutes the pedometer algorithm. 
 
#define I2C_S_DEVICE_INDEX
 
#define FXLS8962_INT_STATUS_SRC_ASLP_MASK
 
gpioConfigKSDK_t gpioConfigINT1
 
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
 
#define FXLS8962_WHOAMI_VALUE
 
#define FXLS8962_DATA_SIZE
 
ARM_DRIVER_I2C * pCommDrv
 
struct pedometer_t::pedometer_status_tag status
 
Access structure of the GPIO Driver. 
 
int main(void)
This is the The main function implementation. 
 
#define FXLS8962_INT_STATUS_SRC_SDCD_OT_MASK
 
fxls8962_acceldataUser_t rawData
 
This structure defines the Write command List. 
 
This structure defines the Read command List. 
 
struct pedometer_t::pedometer_status_tag::@292::@293 bits
 
int32_t FXLS8962_I2C_ReadData(fxls8962_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
 
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features. 
 
#define FXLS8962_INT_EN_DRDY_EN_EN
 
#define FXLS8962_INT_EN_ASLP_EN_EN
 
#define FXLS8962_SENS_CONFIG3_SLEEP_ODR_0_781HZ
 
#define I2C_S_SIGNAL_EVENT
 
int32_t Sensor_I2C_Write(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerwritelist_t *pRegWriteList)
Write register data to a sensor. 
 
#define FXLS8962_SENS_CONFIG4_WK_SDCD_OT_EN