![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The mma845x_interrupt.c file implements the ISSDK MMA845x sensor driver example demonstration with Interrupt mode. More...
#include "pin_mux.h"#include "clock_config.h"#include "board.h"#include "fsl_debug_console.h"#include "Driver_I2C.h"#include "issdk_hal.h"#include "gpio_driver.h"#include "mma845x_drv.h"
Go to the source code of this file.
Functions | |
| void | mma845x_isr (void *pUserData) |
| This is the Sensor Data Ready ISR implementation. More... | |
| int | main (void) |
| This is the The main function implementation. More... | |
Variables | |
| const registerwritelist_t | mma845x_Config_Isr [] |
| const registerreadlist_t | MMA845x_Data_Ready [] = {{.readFrom = MMA845x_STATUS, .numBytes = 1}, __END_READ_DATA__} |
| const registerreadlist_t | mma845x_Output_Values [] |
| volatile bool | mma845xInterrupt = false |
The mma845x_interrupt.c file implements the ISSDK MMA845x sensor driver example demonstration with Interrupt mode.
Definition in file mma845x_interrupt.c.
| int main | ( | void | ) |
This is the The main function implementation.
This function invokes board initializes routines, then then brings up the sensor and finally enters an endless loop to continuously read available samples.
| [in] | void | This is no input parameter. |
Initialize the MCU hardware.
Initialize INT1 pin used by FRDM board
Initialize RGB LED pin used by FRDM board
Initialize the I2C driver.
Set the I2C Power mode.
Set the I2C bus speed.
Initialize the MMA845x sensor driver.
Set the task to be executed while waiting for I2C transactions to complete.
Configure the MMA845x sensor driver with No FIFO mode.
Clear the data ready flag, it will be set again by the ISR.
Read the raw sensor data from the MMA845x.
Convert the raw sensor data to signed 16-bit container for display to the debug port.
Definition at line 91 of file mma845x_interrupt.c.
References mma845x_acceldata_t::accel, ASK_USER_TO_RESUME, BOARD_BootClockRUN, BOARD_InitDebugConsole(), BOARD_InitPins(), data, Driver_GPIO_KSDK, GPIO_DIRECTION_IN, GPIO_DIRECTION_OUT, GREEN_LED, I2C_S_DEVICE_INDEX, I2C_S_DRIVER, I2C_S_SIGNAL_EVENT, I2Cdrv, int32_t(), MMA8451_WHO_AM_I_WHOAMI_VALUE, MMA845x_ACCEL_DATA_SIZE, MMA845x_I2C_ADDR, MMA845x_I2C_Configure(), MMA845x_I2C_Initialize(), MMA845x_I2C_ReadData(), MMA845x_I2C_SetIdleTask(), MMA845x_INT1, mma845x_isr(), mma845xInterrupt, GENERIC_DRIVER_GPIO::pin_init, rawData, SENSOR_ERROR_NONE, SMC, SMC_SetPowerModeVlpr(), SMC_SetPowerModeWait(), status, and GENERIC_DRIVER_GPIO::toggle_pin.

| void mma845x_isr | ( | void * | pUserData | ) |
This is the Sensor Data Ready ISR implementation.
This function sets the flag which indicates if a new sample(s) is available for reading.
| [in] | pUserData | This is a void pointer to the instance of the user specific data structure for the ISR. |
Set flag to indicate Sensor has signalled data ready.
Definition at line 77 of file mma845x_interrupt.c.
References mma845xInterrupt.
Referenced by main().

| const registerwritelist_t mma845x_Config_Isr[] |
Prepare the register write list to configure MMA845x in non-FIFO and ISR mode.
Definition at line 39 of file mma845x_interrupt.c.
| const registerreadlist_t MMA845x_Data_Ready[] = {{.readFrom = MMA845x_STATUS, .numBytes = 1}, __END_READ_DATA__} |
Prepare the register read list to read the Data Ready Status from MMA845x.
Definition at line 55 of file mma845x_interrupt.c.
| const registerreadlist_t mma845x_Output_Values[] |
Prepare the register read list to read the raw Accel data from MMA845x.
Definition at line 58 of file mma845x_interrupt.c.
| volatile bool mma845xInterrupt = false |
Definition at line 64 of file mma845x_interrupt.c.
Referenced by main(), and mma845x_isr().