ISSDK  1.8
IoT Sensing Software Development Kit
mma845x_interrupt.c
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015 - 2016, Freescale Semiconductor, Inc.
3  * Copyright 2016-2017 NXP
4  * All rights reserved.
5  *
6  * SPDX-License-Identifier: BSD-3-Clause
7  */
8 
9 /**
10  * @file mma845x_interrupt.c
11 * @brief The mma845x_interrupt.c file implements the ISSDK MMA845x sensor driver
12 * example demonstration with Interrupt mode.
13 */
14 
15 //-----------------------------------------------------------------------
16 // SDK Includes
17 //-----------------------------------------------------------------------
18 #include "pin_mux.h"
19 #include "clock_config.h"
20 #include "board.h"
21 #include "fsl_debug_console.h"
22 
23 //-----------------------------------------------------------------------
24 // CMSIS Includes
25 //-----------------------------------------------------------------------
26 #include "Driver_I2C.h"
27 
28 //-----------------------------------------------------------------------
29 // ISSDK Includes
30 //-----------------------------------------------------------------------
31 #include "issdk_hal.h"
32 #include "gpio_driver.h"
33 #include "mma845x_drv.h"
34 
35 //-----------------------------------------------------------------------
36 // Constants
37 //-----------------------------------------------------------------------
38 /*! Prepare the register write list to configure MMA845x in non-FIFO and ISR mode. */
40  /*! Configure the MMA845x CTRL_REG1 to set mode to STANDBY and odr to 12.5Hz. */
42  /*! Configure the MMA845x to disable FIFO */
44  /*! Configure the MMA845x CTRL_REG2 to set the Oversampling mode to High Resolution. */
46  /*! Configure the MMA845x CTRL_REG3 to set the Interrupt polarity to ACTIVE high. */
48  /*! Configure the MMA845x CTRL_REG4 to enable the data ready interrupt. */
50  /*! Configure the MMA845x CTRL_REG5 to route Interrupt to INT1 pin. */
53 
54 /*! Prepare the register read list to read the Data Ready Status from MMA845x. */
56 
57 /*! Prepare the register read list to read the raw Accel data from MMA845x. */
60 
61 //-----------------------------------------------------------------------
62 // Global Variables
63 //-----------------------------------------------------------------------
64 volatile bool mma845xInterrupt = false;
65 
66 //-----------------------------------------------------------------------
67 // Functions
68 //-----------------------------------------------------------------------
69 /*! -----------------------------------------------------------------------
70  * @brief This is the Sensor Data Ready ISR implementation.
71  * @details This function sets the flag which indicates if a new sample(s) is available for reading.
72  * @param[in] pUserData This is a void pointer to the instance of the user specific data structure for the ISR.
73  * @return void There is no return value.
74  * @constraints None
75  * @reeentrant Yes
76  * -----------------------------------------------------------------------*/
77 void mma845x_isr(void *pUserData)
78 { /*! @brief Set flag to indicate Sensor has signalled data ready. */
79  mma845xInterrupt = true;
80 }
81 
82 /*! -----------------------------------------------------------------------
83  * @brief This is the The main function implementation.
84  * @details This function invokes board initializes routines, then then brings up the sensor and
85  * finally enters an endless loop to continuously read available samples.
86  * @param[in] void This is no input parameter.
87  * @return void There is no return value.
88  * @constraints None
89  * @reeentrant No
90  * -----------------------------------------------------------------------*/
91 int main(void)
92 {
96 
97  ARM_DRIVER_I2C *I2Cdrv = &I2C_S_DRIVER; // Now using the shield.h value!!!
98  mma845x_i2c_sensorhandle_t MMA845xdrv;
100 
101  /*! Initialize the MCU hardware. */
102  BOARD_InitPins();
105 
106  PRINTF("\r\n ISSDK MMA845x sensor driver example for interrupt mode.\r\n");
107 
108  /*! Initialize INT1 pin used by FRDM board */
109  gpioDriver->pin_init(&MMA845x_INT1, GPIO_DIRECTION_IN, NULL, &mma845x_isr, NULL);
110  /*! Initialize RGB LED pin used by FRDM board */
111  gpioDriver->pin_init(&GREEN_LED, GPIO_DIRECTION_OUT, NULL, NULL, NULL);
112 
113  /*! Initialize the I2C driver. */
114  status = I2Cdrv->Initialize(I2C_S_SIGNAL_EVENT);
115  if (ARM_DRIVER_OK != status)
116  {
117  PRINTF("\r\n I2C Initialization Failed\r\n");
118  return -1;
119  }
120 
121  /*! Set the I2C Power mode. */
122  status = I2Cdrv->PowerControl(ARM_POWER_FULL);
123  if (ARM_DRIVER_OK != status)
124  {
125  PRINTF("\r\n I2C Power Mode setting Failed\r\n");
126  return -1;
127  }
128 
129  /*! Set the I2C bus speed. */
130  status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
131  if (ARM_DRIVER_OK != status)
132  {
133  PRINTF("\r\n I2C Control Mode setting Failed\r\n");
134  return -1;
135  }
136 
137  /*! Initialize the MMA845x sensor driver. */
140  if (SENSOR_ERROR_NONE != status)
141  {
142  PRINTF("\r\n Sensor Initialization Failed\r\n");
143  return -1;
144  }
145  PRINTF("\r\n Successfully Initiliazed Sensor\r\n");
146 
147  /*! Set the task to be executed while waiting for I2C transactions to complete. */
149 
150  /*! Configure the MMA845x sensor driver with No FIFO mode. */
151  status = MMA845x_I2C_Configure(&MMA845xdrv, mma845x_Config_Isr);
152  if (SENSOR_ERROR_NONE != status)
153  {
154  PRINTF("\r\n MMA845x Sensor Configuration Failed, Err = %d\r\n", status);
155  return -1;
156  }
157  PRINTF("\r\n Successfully Applied MMA845x Sensor Configuration\r\n");
158 
159  for (;;) /* Forever loop */
160  { /* In ISR Mode we do not need to check Data Ready Register.
161  * The receipt of interrupt will indicate data is ready. */
162  if (false == mma845xInterrupt)
163  { /* Loop, if new sample is not available. */
165  continue;
166  }
167  else
168  { /*! Clear the data ready flag, it will be set again by the ISR. */
169  mma845xInterrupt = false;
170  gpioDriver->toggle_pin(&GREEN_LED);
171  }
172 
173  /*! Read the raw sensor data from the MMA845x. */
174  status = MMA845x_I2C_ReadData(&MMA845xdrv, mma845x_Output_Values, data);
175  if (ARM_DRIVER_OK != status)
176  {
177  PRINTF("\r\n Read Failed. \r\n");
178  return -1;
179  }
180 
181  /*! Convert the raw sensor data to signed 16-bit container for display to the debug port. */
182  rawData.accel[0] = ((int16_t)data[0] << 8) | data[1];
183  rawData.accel[0] /= 4;
184  rawData.accel[1] = ((int16_t)data[2] << 8) | data[3];
185  rawData.accel[1] /= 4;
186  rawData.accel[2] = ((int16_t)data[4] << 8) | data[5];
187  rawData.accel[2] /= 4;
188 
189  /* NOTE: PRINTF is relatively expensive in terms of CPU time, specially when used with-in execution loop. */
190  PRINTF("\r\n Accel X = %d Y = %d Z = %d\r\n", rawData.accel[0], rawData.accel[1], rawData.accel[2]);
191  ASK_USER_TO_RESUME(100); /* Ask for user input after processing 100 samples. */
192  }
193 }
#define MMA845x_CTRL_REG1_DR_12DOT5HZ
Definition: mma845x.h:1610
#define MMA8451_WHO_AM_I_WHOAMI_VALUE
Definition: mma845x.h:482
#define MMA845x_CTRL_REG5_INT_CFG_DRDY_INT1
Definition: mma845x.h:1895
int16_t accel[3]
Definition: mma845x_drv.h:41
This structure defines the Write command List.
Definition: sensor_drv.h:68
#define ASK_USER_TO_RESUME(x)
Definition: frdm_k64f.h:106
int32_t status
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
Definition: lpc54114.c:169
int32_t MMA845x_I2C_Configure(mma845x_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
Definition: mma845x_drv.c:61
Access structure of the GPIO Driver.
Definition: Driver_GPIO.h:38
#define SMC
Definition: lpc54114.h:118
int32_t MMA845x_I2C_Initialize(mma845x_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
Definition: mma845x_drv.c:22
const registerreadlist_t MMA845x_Data_Ready[]
volatile bool mma845xInterrupt
int main(void)
This is the The main function implementation.
#define __END_WRITE_DATA__
Definition: sensor_drv.h:45
void MMA845x_I2C_SetIdleTask(mma845x_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
Definition: mma845x_drv.c:53
This structure defines the mma845x raw data buffer.
Definition: mma845x_drv.h:38
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
#define I2C_S_SIGNAL_EVENT
Definition: issdk_hal.h:34
#define I2C_S_DRIVER
Definition: issdk_hal.h:33
#define BOARD_BootClockRUN
Definition: clock_config.h:19
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
Definition: sensor_drv.h:97
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
Definition: gpio_driver.c:177
uint8_t data[FXLS8962_DATA_SIZE]
#define MMA845x_CTRL_REG2_MODS_HIGHRES
Definition: mma845x.h:1669
#define __END_READ_DATA__
Definition: sensor_drv.h:51
void mma845x_isr(void *pUserData)
This is the Sensor Data Ready ISR implementation.
const registerreadlist_t mma845x_Output_Values[]
ARM_DRIVER_I2C * I2Cdrv
fxos8700_accelmagdata_t rawData
const registerwritelist_t mma845x_Config_Isr[]
uint16_t readFrom
Definition: sensor_drv.h:80
void(* toggle_pin)(pinID_t aPinId)
Definition: Driver_GPIO.h:48
#define MMA845x_F_SETUP_F_MODE_FIFODISABLED
Definition: mma845x.h:285
#define MMA845x_ACCEL_DATA_SIZE
The size of the MMA845x accel data.
Definition: mma845x_drv.h:47
#define MMA845x_CTRL_REG3_IPOL_HIGH
Definition: mma845x.h:1744
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
Definition: lpc54114.c:155
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
Definition: Driver_GPIO.h:41
This structure defines the Read command List.
Definition: sensor_drv.h:78
gpioHandleKSDK_t GREEN_LED
Definition: frdm_k64f.c:188
#define I2C_S_DEVICE_INDEX
Definition: issdk_hal.h:35
#define MMA845x_CTRL_REG1_MODE_STANDBY
Definition: mma845x.h:1599
This defines the sensor specific information.
Definition: mma845x_drv.h:29
The mma845x_drv.h file describes the MMA845x driver interface and structures.
void BOARD_InitDebugConsole(void)
Definition: board.c:15
#define MMA845x_INT1
Definition: frdm_kl25z.h:103
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
Definition: pin_mux.c:47
#define MMA845x_CTRL_REG4_INT_EN_DRDY_ENABLED
Definition: mma845x.h:1820
int32_t MMA845x_I2C_ReadData(mma845x_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
Definition: mma845x_drv.c:104
#define MMA845x_I2C_ADDR
Definition: frdm_kl25z.h:102