17 #include "clock_config.h" 19 #include "fsl_lptmr.h" 20 #include "fsl_debug_console.h" 23 #include "Driver_I2C.h" 26 #include "issdk_hal.h" 33 #define SAMPLING_RATE_ms (100) 34 #define MMA9553_ACCEL_DATA_SIZE (6) 35 #define mma9553_en_callback LPTMR0_IRQHandler 71 LPTMR_ClearStatusFlags(LPTMR0, kLPTMR_TimerCompareFlag);
81 lptmr_config_t lptmrConfig;
95 LPTMR_GetDefaultConfig(&lptmrConfig);
96 LPTMR_Init(LPTMR0, &lptmrConfig);
97 LPTMR_EnableInterrupts(LPTMR0, kLPTMR_TimerInterruptEnable);
98 LPTMR_SetTimerPeriod(LPTMR0, MSEC_TO_COUNT(
SAMPLING_RATE_ms, CLOCK_GetFreq(kCLOCK_LpoClk)));
99 EnableIRQ(LPTMR0_IRQn);
101 PRINTF(
"\r\n ISSDK MMA9553 sensor driver example for Pedometer Mode. \r\n");
105 if (ARM_DRIVER_OK != status)
107 PRINTF(
"\r\n I2C Initialization Failed\r\n");
112 status = I2Cdrv->PowerControl(ARM_POWER_FULL);
113 if (ARM_DRIVER_OK != status)
115 PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
120 status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
121 if (ARM_DRIVER_OK != status)
123 PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
131 PRINTF(
"\r\n Sensor Initialization Failed\r\n");
134 PRINTF(
"\r\n Successfully Initialized Sensor. \r\n");
145 PRINTF(
"\r\n MMA9553 Sensor Configuration Failed, Err = %d \r\n", status);
149 LPTMR_StartTimer(LPTMR0);
150 PRINTF(
"\r\n Successfully Applied MMA9553 Sensor Configuration\r\n");
165 (uint8_t *)&pedometerData);
166 if (ARM_DRIVER_OK != status)
168 PRINTF(
"\r\n Read Failed. \r\n");
173 pedometerData.statusRegister = (pedometerData.statusRegister >> 8) | (pedometerData.statusRegister << 8);
174 pedometerData.stepCount = (pedometerData.stepCount >> 8) | (pedometerData.stepCount << 8);
175 pedometerData.distance = (pedometerData.distance >> 8) | (pedometerData.distance << 8);
176 pedometerData.speed = (pedometerData.speed >> 8) | (pedometerData.speed << 8);
177 pedometerData.calories = (pedometerData.calories >> 8) | (pedometerData.calories << 8);
178 pedometerData.sleepCount = (pedometerData.sleepCount >> 8) | (pedometerData.sleepCount << 8);
180 PRINTF(
"\r\n Steps = %d Distance = %dm Speed = %dm/h Calories = %d \r\n", pedometerData.stepCount,
181 pedometerData.distance, pedometerData.speed, pedometerData.calories);
185 if (ARM_DRIVER_OK != status)
187 PRINTF(
"\r\n Read Failed. \r\n");
191 PRINTF(
"\r\n Accel X = %d Y = %d Z = %d \r\n", rawData.
accel[0], rawData.
accel[1], rawData.
accel[2]);
This defines the sensor specific information for I2C.
#define ASK_USER_TO_RESUME(x)
void MMA9553_I2C_SetIdleTask(mma9553_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
const uint8_t SetSampleRate_30Hz[5]
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
const uint8_t ReadPedometerData[4]
Command to Read Pedometer Data.
This structure defines the Size of response for pedometer data read command.
This structure defines the Block command List.
int32_t MMA9553_I2C_Configure(mma9553_i2c_sensorhandle_t *pSensorHandle, const registercommandlist_t *pCommandList)
The interface function to configure he sensor.
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
The mma9553_drv.h file describes the MMA9553L driver interface and structures.
This structure defines the mma9553 pedometer data buffer.
#define I2C_S_SIGNAL_EVENT
const uint8_t SetFSRange_2g[5]
Full-Scale Range Selections.
#define MMA9553_XYZ_DATA_OFFSET
XYZ Data Register Offset.
#define BOARD_BootClockRUN
const uint8_t SetAFEPriority_for30Hz[5]
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
int32_t MMA9553_I2C_CommandResponse(mma9553_i2c_sensorhandle_t *pSensorHandle, const registercommandlist_t *pCommandList, const registerreadlist_t *pResponseList, uint8_t *pBuffer)
The interface function to read the sensor data.
#define mma9553_en_callback
const registerreadlist_t cMma9553ReadRawOutput[]
#define __END_READ_DATA__
#define __END_WRITE_CMD__
fxos8700_accelmagdata_t rawData
int32_t MMA9553_I2C_Initialize(mma9553_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress)
The interface function to initialize the sensor.
const uint8_t SetMBoxPriority_for30Hz[5]
void BOARD_SystickEnable(void)
Function to enable systicks framework.
This structure defines the Read command List.
#define I2C_S_DEVICE_INDEX
int main(void)
Main function.
void BOARD_InitDebugConsole(void)
#define MMA9553_ACCEL_DATA_SIZE
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
volatile bool gMma9553DataReady
const registercommandlist_t cMma9553Config30Hz[]
const registerreadlist_t cMma9553ReadPedometerOutput[]
const registercommandlist_t cMma9553ReadPedometerCommand[]