ISSDK  1.8
IoT Sensing Software Development Kit
mpl3115_fifo.c
Go to the documentation of this file.
1 /*
2  * Copyright 2018 NXP
3  * All rights reserved.
4  *
5  * SPDX-License-Identifier: BSD-3-Clause
6  */
7 
8 /**
9  * @file mpl3115_fifo.c
10  * @brief The mpl3115_fifo.c file implements the ISSDK MPL3115 sensor driver
11  * example demonstration with FIFO mode.
12  */
13 
14 //-----------------------------------------------------------------------
15 // SDK Includes
16 //-----------------------------------------------------------------------
17 #include "pin_mux.h"
18 #include "clock_config.h"
19 #include "board.h"
20 #include "fsl_debug_console.h"
21 #include "fsl_irqsteer.h"
22 
23 /* CMSIS Includes */
24 #include "Driver_I2C.h"
25 
26 /* ISSDK Includes */
27 #include "issdk_hal.h"
28 #include "mpl3115_drv.h"
29 
30 //-----------------------------------------------------------------------
31 // Macros
32 //-----------------------------------------------------------------------
33 #define FIFO_WMRK_SIZE (8) /* Buffer 8 Samples. */
34 #define MPL3115_DATA_SIZE (5) /* 3 byte Pressure/Altitude and 2 byte Temperature. */
35 /*! In MPL3115 the Auto Acquisition Time Step (ODR) can be set only in powers of 2 (i.e. 2^x, where x is the
36  * SAMPLING_EXPONENT).
37  * This gives a range of 1 second to 2^15 seconds (9 hours). */
38 #define MPL3115_SAMPLING_EXPONENT (0) /* 1 second. */
39 
40 //-----------------------------------------------------------------------
41 // Constants
42 //-----------------------------------------------------------------------
43 /*! @brief Register settings for FIFO (buffered) mode @ default 1 sample per second. */
45  /* Set FIFO Mode and set FIFO Watermark Level. */
48  /* Enable Data Ready and Event flags for Pressure, Temperature or either. */
52  /* Set Over Sampling Ratio to 128. */
56 
57 /*! @brief Address of Status Register. */
59 
60 /*! @brief Address and size of Pressure+Temperature Data in FIFO Mode. */
63 
64 //-----------------------------------------------------------------------
65 // Functions
66 //-----------------------------------------------------------------------
67 /*!
68  * @brief Main function
69  */
70 int main(void)
71 {
72  int16_t tempInDegrees;
73  uint32_t pressureInPascals;
75  uint8_t dataReady;
78  sc_ipc_t ipc;
79  uint32_t freq;
80 
81  ARM_DRIVER_I2C *I2Cdrv = &I2C_S_DRIVER; // Now using the shield.h value!!!
82  mpl3115_i2c_sensorhandle_t mpl3115Driver;
83 
84  ipc = BOARD_InitRpc();
85  BOARD_InitMemory();
88 
90 
91  PRINTF("\r\n ----------------------------------------------------------------\r\n");
92  PRINTF("\r\n ISSDK MPL3115 sensor driver example demonstration with FIFO mode\r\n");
93  PRINTF("\r\n ----------------------------------------------------------------\r\n");
94 
95  /* Power on LPI2C. */
96  if (sc_pm_set_resource_power_mode(ipc, SC_R_I2C_0, SC_PM_PW_MODE_ON) != SC_ERR_NONE)
97  {
98  PRINTF("Error: Failed to power on LPI2C\r\n");
99  }
100 
101  /* Set LPI2C clock */
102  freq = CLOCK_SetIpFreq(kCLOCK_DMA_Lpi2c0, SC_24MHZ);
103  if (freq == 0)
104  {
105  PRINTF("Error: Failed to set LPI2C frequency\r\n");
106  }
107 
108  /* Power on IRQSTEER. */
109 #if (MIMX8QM_CM4_CORE0)
110  if (sc_pm_set_resource_power_mode(ipc, SC_R_IRQSTR_M4_0, SC_PM_PW_MODE_ON) != SC_ERR_NONE)
111  {
112  PRINTF("Error: Failed to power on IRQSTEER M4_0\r\n");
113  }
114 #elif (MIMX8QM_CM4_CORE1)
115  if (sc_pm_set_resource_power_mode(ipc, SC_R_IRQSTR_M4_1, SC_PM_PW_MODE_ON) != SC_ERR_NONE)
116  {
117  PRINTF("Error: Failed to power on IRQSTEER M4_1\r\n");
118  }
119 #endif
120  /* Enable interrupt in irqsteer */
121  IRQSTEER_Init(IRQSTEER);
122  IRQSTEER_EnableInterrupt(IRQSTEER, DMA_I2C0_INT_IRQn);
123 
124  /*! Initialize the I2C driver. */
125  status = I2Cdrv->Initialize(I2C_S_SIGNAL_EVENT);
126  if (ARM_DRIVER_OK != status)
127  {
128  PRINTF("\r\n I2C Initialization Failed\r\n");
129  return -1;
130  }
131 
132  /*! Set the I2C Power mode. */
133  status = I2Cdrv->PowerControl(ARM_POWER_FULL);
134  if (ARM_DRIVER_OK != status)
135  {
136  PRINTF("\r\n I2C Power Mode setting Failed\r\n");
137  return -1;
138  }
139 
140  /*! Set the I2C bus speed. */
141  status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
142  if (ARM_DRIVER_OK != status)
143  {
144  PRINTF("\r\n I2C Control Mode setting Failed\r\n");
145  return -1;
146  }
147 
148  /*! Initialize MPL3115 sensor driver. */
151  if (SENSOR_ERROR_NONE != status)
152  {
153  PRINTF("\r\n Sensor Initialization Failed\r\n");
154  return -1;
155  }
156  PRINTF("\r\n Successfully Initiliazed MPL3115 Sensor\r\n");
157  PRINTF("\r\n Device Address is 0x%x and WHOAMI Value is 0x%x\r\n", MPL3115_I2C_ADDR, MPL3115_WHOAMI_VALUE);
158 
159  /*! Configure the MPL3115 sensor. */
160  status = MPL3115_I2C_Configure(&mpl3115Driver, cMpl3115ConfigFIFO);
161  if (SENSOR_ERROR_NONE != status)
162  {
163  PRINTF("\r\nMPL3115 configuration failed...\r\n");
164  return -1;
165  }
166  PRINTF("\r\n Successfully Applied MPL3115 Sensor Configuration\r\n");
167 
168  PRINTF("\r\n Reading MPL3115 Pressure & Temperature Values, FIFO width=%d\r\n", FIFO_WMRK_SIZE);
169 
170  for (;;) /* Forever loop */
171  {
172  /*! Wait for data ready from the MPL3115. */
173  status = MPL3115_I2C_ReadData(&mpl3115Driver, cMpl3115Status, &dataReady);
174  if (0 == (dataReady & MPL3115_F_STATUS_F_WMKF_FLAG_MASK))
175  { /* Loop, if new sample is not available. */
176  continue;
177  }
178 
179  /*! Read new raw sensor data from the MPL3115. */
180  status = MPL3115_I2C_ReadData(&mpl3115Driver, cMpl3115OutputFIFO, data);
181  if (ARM_DRIVER_OK != status)
182  {
183  PRINTF("\r\n Read Failed. \r\n");
184  return -1;
185  }
186 
187  /* Reset Counters */
188  pressureInPascals = 0;
189  tempInDegrees = 0;
190 
191  for (uint8_t i = 0; i < FIFO_WMRK_SIZE; i++)
192  { /*! Process all samples and convert the raw sensor data. */
193  rawData.pressure = (uint32_t)((data[i * MPL3115_DATA_SIZE + 0]) << 16) |
194  ((data[i * MPL3115_DATA_SIZE + 1]) << 8) | ((data[i * MPL3115_DATA_SIZE + 2]));
195  pressureInPascals += rawData.pressure / MPL3115_PRESSURE_CONV_FACTOR;
196 
197  rawData.temperature = (int16_t)((data[i * MPL3115_DATA_SIZE + 3]) << 8) | (data[i * MPL3115_DATA_SIZE + 4]);
198  tempInDegrees += rawData.temperature / MPL3115_TEMPERATURE_CONV_FACTOR;
199  }
200  PRINTF("\r\n Avg Pressure = %d Pa", pressureInPascals / FIFO_WMRK_SIZE);
201  PRINTF("\t Avg Temperature = %d degC\r\n", tempInDegrees / FIFO_WMRK_SIZE);
202  ASK_USER_TO_RESUME(16 / FIFO_WMRK_SIZE); /* Ask for user input after processing 16 samples. */
203  }
204 }
const registerreadlist_t cMpl3115OutputFIFO[]
Address and size of Pressure+Temperature Data in FIFO Mode.
Definition: mpl3115_fifo.c:63
This structure defines the Write command List.
Definition: sensor_drv.h:68
#define ASK_USER_TO_RESUME(x)
Definition: frdm_k64f.h:106
int32_t status
#define MPL3115_PRESSURE_CONV_FACTOR
Definition: mpl3115_drv.h:28
#define FIFO_WMRK_SIZE
Definition: mpl3115_fifo.c:33
const registerreadlist_t cMpl3115Status[]
Address of Status Register.
Definition: mpl3115_fifo.c:60
int32_t MPL3115_I2C_ReadData(mpl3115_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
Definition: mpl3115_drv.c:104
#define MPL3115_F_SETUP_F_MODE_MASK
Definition: mpl3115.h:410
The mpl3115_drv.h file describes the MPL3115 driver interface and structures.
#define MPL3115_CTRL_REG2_ST_MASK
Definition: mpl3115.h:916
#define __END_WRITE_DATA__
Definition: sensor_drv.h:45
#define MPL3115_F_SETUP_F_MODE_STOP_MODE
Definition: mpl3115.h:420
#define MPL3115_PT_DATA_CFG_TDEFE_MASK
Definition: mpl3115.h:550
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
#define MPL3115_F_SETUP_F_WMRK_MASK
Definition: mpl3115.h:407
#define I2C_S_SIGNAL_EVENT
Definition: issdk_hal.h:34
#define I2C_S_DRIVER
Definition: issdk_hal.h:33
#define BOARD_BootClockRUN
Definition: clock_config.h:19
#define MPL3115_TEMPERATURE_CONV_FACTOR
Definition: mpl3115_drv.h:30
This structure defines the mpl3115 data buffer in Pressure Mode.
Definition: mpl3115_drv.h:45
#define MPL3115_PT_DATA_CFG_DREM_ENABLED
Definition: mpl3115.h:570
uint8_t data[FXLS8962_DATA_SIZE]
#define MPL3115_PT_DATA_CFG_PDEFE_MASK
Definition: mpl3115.h:553
#define __END_READ_DATA__
Definition: sensor_drv.h:51
This defines the sensor specific information.
Definition: mpl3115_drv.h:36
#define MPL3115_CTRL_REG1_OS_OSR_128
Definition: mpl3115.h:884
ARM_DRIVER_I2C * I2Cdrv
fxos8700_accelmagdata_t rawData
int32_t MPL3115_I2C_Initialize(mpl3115_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
Definition: mpl3115_drv.c:22
#define MPL3115_F_STATUS_F_WMKF_FLAG_MASK
Definition: mpl3115.h:359
uint16_t readFrom
Definition: sensor_drv.h:80
#define MPL3115_PT_DATA_CFG_DREM_MASK
Definition: mpl3115.h:556
#define MPL3115_PT_DATA_CFG_PDEFE_ENABLED
Definition: mpl3115.h:567
#define MPL3115_WHOAMI_VALUE
Definition: mpl3115.h:65
int main(void)
Main function.
Definition: mpl3115_fifo.c:72
const registerwritelist_t cMpl3115ConfigFIFO[]
Register settings for FIFO (buffered) mode @ default 1 sample per second.
Definition: mpl3115_fifo.c:46
This structure defines the Read command List.
Definition: sensor_drv.h:78
#define MPL3115_PT_DATA_CFG_TDEFE_ENABLED
Definition: mpl3115.h:564
#define I2C_S_DEVICE_INDEX
Definition: issdk_hal.h:35
#define MPL3115_I2C_ADDR
void BOARD_InitDebugConsole(void)
Definition: board.c:15
#define MPL3115_SAMPLING_EXPONENT
Definition: mpl3115_fifo.c:38
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
Definition: pin_mux.c:47
int32_t MPL3115_I2C_Configure(mpl3115_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
Definition: mpl3115_drv.c:61
#define MPL3115_CTRL_REG1_OS_MASK
Definition: mpl3115.h:855
#define MPL3115_DATA_SIZE
Definition: mpl3115_fifo.c:34