dsc_crc

Overview

The CRC Example project is a demonstration program that uses the KSDK software to generate checksums for an ASCII string. Several CRC protocols are implemented using the CRC driver API.

Running the demo

Example output on terminal:

CRC Peripheral Driver Example.

Test same string base on different CRC protocol. test string: 123456789 1.CRC-16 CCIT FALSE: 0x29b1 2.CRC-16 KERMIT: 0x2189 3.CRC-16 MAXIM: 0x44c2 4.CRC-32: 0xcbf43926 5.CRC-32 POSIX: 0x765e7680

Test different string based on CRC-32 POSIX protocol. 1.test string: abcdefgh CRC-32 POSIX: 0x5024ec61 2.test string: abcd1234 CRC-32 POSIX: 0x3fbda0ab

Supported Boards