eeprom

Overview

The EEPROM Example project is a demonstration program that uses the KSDK software to program eeprom memory and verify the program.

Prepare the Demo

Connect a serial cable from the debug UART port of the board to the PC. Start Tera Term (http://ttssh2.osdn.jp) and make a connection to the virtual serial port.

  1. Start Tera Term

  2. New connection -> Serial

  3. Set apropriate COMx port (x is port number) in Port context menu. Number is provided by operation system and could be different from computer to computer. Select COM number related to virtual serial port. Confirm selected port by OK button.

  4. Set following connection parameters in menu Setup->Serial port… Baud rate: 115200 Data: 8 Parity: none Stop: 1 Flow control: one

  5. Confirm selected parameters by OK button.

Running the demo

Example output on terminal:

EEPROM example begins… Page 0 program finished! Page 1 program finished! Page 2 program finished! Page 3 program finished! Page 4 program finished! Page 5 program finished! Page 6 program finished! Page 7 program finished! Page 8 program finished! Page 9 program finished! … Page 126 program finished! All data is correct! EEPROM example succeed!

Supported Boards