evtg

Overview

The EVTG demo application demonstrates the use of IO and EVTG peripherals. The example Use the two IO as the input of the EVTG function: EVTG_OUT = (IO0 & IO1). When IO0 and IO1 are both high level, the EVTG_OUT is high level. When any of IO is low level, the EVTG_OUT is low level. The purpose of this demonstration is to show how to use the EVTG driver in the SDK software.

Supported Boards