mrt_example
Overview
The MRT project is a simple demonstration program of the SDK MRT driver. It sets up the MRT hardware block to trigger a periodic interrupt after every 250 milliseconds. When the PIT interrupt is triggered a message a printed on the UART terminal and an LED is toggled on the board.