itrc

Overview

The ITRC Example project is a demonstration program that uses the MCUX SDK software to set up Intrusion and Tamper Response Controller. Then tests the expected behaviour.

Running the demo

When the demo runs successfully, the terminal displays similar information like the following:


ITRC Peripheral Driver Example

Pass: No Event/Action triggered after Init

Enable ITRC IRQ Action response to SW Event 0

Trigger SW Event 0

ITRC IRQ Reached!
ITRC STATUS:
SW Event0 occured!
Generated ITRC interrupt!

Clear ITRC IRQ and SW Event 0 STATUS

Disable ITRC IRQ Action response to SW Event 0

Trigger SW Event 0

Pass: No Action triggered

End of example

Supported Boards