fsl_romapi

Overview

The fsl_romapi example shows how to use flexspi rom api In this example, rom api will send data and operate the external Nor flash connected with FLEXSPI. Some simple flash command willbe executed, such as Write Enable, Erase sector, Program page.Example will first erase the sector and program a page into the flash, at last check if the data in flash is correct.

Supported Boards