46 #include "clock_config.h"    51 #include "Driver_I2C.h"    52 #include "Driver_USART.h"    57 #include "issdk_hal.h"    58 #include "gpio_driver.h"    62 #include "auto_detection_service.h"    67 #define MMA845x_STREAM_DATA_SIZE 11     70 #define APPLICATION_NAME "MMA845x Accelerometer Demo"    72 #define APPLICATION_VERSION "2.5"   163     uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse, 
size_t *hostMsgSize, 
size_t respBufferSize)
   165     bool success = 
false;
   180         if (respBufferSize >= boardNameLen + shieldNameLen + appNameLen + 3)
   189         hostResponse[*hostMsgSize] = appNameLen;
   192         memcpy(hostResponse + *hostMsgSize, 
embAppName, appNameLen);
   193         *hostMsgSize += appNameLen;
   195         hostResponse[*hostMsgSize] = boardNameLen;
   198         memcpy(hostResponse + *hostMsgSize, 
boardString, boardNameLen);
   199         *hostMsgSize += boardNameLen;
   201         hostResponse[*hostMsgSize] = shieldNameLen;
   204         memcpy(hostResponse + *hostMsgSize, 
shieldString, shieldNameLen);
   205         *hostMsgSize += shieldNameLen;
   215         switch (hostCommand[0]) 
   277     if (ARM_DRIVER_OK != status)
   283     status = pI2cDriver->PowerControl(ARM_POWER_FULL);
   284     if (ARM_DRIVER_OK != status)
   290     status = pI2cDriver->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   291     if (ARM_DRIVER_OK != status)
   298     if (ARM_DRIVER_OK != status)
   304     status = pUartDriver->PowerControl(ARM_POWER_FULL);
   305     if (ARM_DRIVER_OK != status)
   312     if (ARM_DRIVER_OK != status)
   368         if (ARM_DRIVER_OK != status)
   377         rawData.
accel[0] = ((int16_t)data[0] << 8) | data[1];
   378         rawData.
accel[0] /= 4;
   379         rawData.
accel[1] = ((int16_t)data[2] << 8) | data[3];
   380         rawData.
accel[1] /= 4;
   381         rawData.
accel[2] = ((int16_t)data[4] << 8) | data[5];
   382         rawData.
accel[2] /= 4;
   388         rawData.
intsrc = intsrcdata;
 
uint32_t BOARD_SystickElapsedTime_us(int32_t *pStart)
Function to compute the Elapsed Time. 
 
const registerwritelist_t mma845x_Config_Isr[]
 
volatile bool bMma845xReady
 
#define MMA845x_FF_MT_CFG_ZEFE_ENABLED
 
#define MMA845x_CTRL_REG5_INT_CFG_DRDY_INT1
 
#define __END_WRITE_DATA__
 
ARM_DRIVER_I2C * pCommDrv
 
int main(void)
Main function. 
 
#define MMA845x_CTRL_REG1_DR_100HZ
 
#define HOST_PRO_CMD_W_CFG_TAG
 
const registerreadlist_t cMma845xqStatus[]
 
#define HOST_S_SIGNAL_EVENT
 
This defines the sensor specific information. 
 
bool process_host_command(uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse, size_t *hostMsgSize, size_t respBufferSize)
 
void Host_IO_Receive(host_cmd_proc_fn_t process_host_command, uint8_t encoding)
 
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
 
char embAppName[ADS_MAX_STRING_LENGTH]
 
#define BOARD_BootClockRUN
 
#define MMA845x_CTRL_REG3_IPOL_HIGH
 
#define MMA845x_PULSE_CFG_YSPEFE_ENABLED
 
#define MMA845x_TRANSIENT_CFG_ZTEFE_ENABLED
 
uint8_t data[FXLS8962_DATA_SIZE]
 
void(* toggle_pin)(pinID_t aPinId)
 
#define MMA845x_CTRL_REG4_INT_EN_LNDPRT_ENABLED
 
#define MMA845x_FF_MT_CFG_YEFE_ENABLED
 
#define MMA845x_PL_CFG_DBCNTM_CLR
 
#define MMA845x_PL_CFG_PL_EN_ENABLED
 
#define ADS_MAX_STRING_LENGTH
 
#define MMA845x_TRANSIENT_THS_DBCNTM_CLR
 
#define MMA845x_CTRL_REG4_INT_EN_PULSE_ENABLED
 
#define HOST_PRO_INT_DEV_TAG
 
uint8_t streamingPacket[STREAMING_HEADER_LEN+FXLS8962_STREAM_DATA_SIZE]
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
#define MMA845x_PULSE_CFG_XSPEFE_ENABLED
 
#define HOST_PRO_INT_CMD_TAG
Bit aligned values for Host Protocol Interface IDs (Bits 5-6). 
 
int32_t MMA845x_I2C_Initialize(mma845x_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
#define __END_READ_DATA__
 
#define MMA845x_PULSE_CFG_ZSPEFE_ENABLED
 
#define MMA845x_CTRL_REG2_MODS_HIGHRES
 
#define MMA845x_FF_MT_THS_DBCNTM_CLR
 
gpioHandleKSDK_t GREEN_LED
 
#define MMA845x_FF_MT_CFG_XEFE_ENABLED
 
#define MMA845x_CTRL_REG4_INT_EN_DRDY_ENABLED
 
#define MMA845x_FF_MT_CFG_OAE_FREEFALL
 
volatile bool bStreamingEnabled
 
void Host_IO_Add_ISO_Header(uint8_t streamID, uint8_t *pStreamingPacket, size_t sizePayload)
 
const registerreadlist_t cMma845xqPLStatus[]
 
void Host_IO_Send(uint8_t *pMsg, size_t size, uint8_t encoding)
 
char shieldString[ADS_MAX_STRING_LENGTH]
 
GENERIC_DRIVER_GPIO * pGpioDriver
 
void(* clr_pin)(pinID_t aPinId)
 
void BOARD_SystickEnable(void)
Function to enable systicks framework. 
 
#define MMA845x_CTRL_REG4_INT_EN_TRANS_ENABLED
 
#define MMA845x_STREAM_DATA_SIZE
 
#define I2C_S_DEVICE_INDEX
 
int32_t MMA845x_I2C_ReadData(mma845x_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
#define MMA845x_XYZ_DATA_CFG_FS_MASK
 
volatile bool bMma845xDataReady
 
#define MMA845x_TRANSIENT_CFG_YTEFE_ENABLED
 
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
 
#define APPLICATION_NAME
Unique Name for this application which should match the target GUI pkg name. 
 
#define BOARD_DEBUG_UART_BAUDRATE
 
registerDeviceInfo_t deviceInfo
 
int32_t MMA845x_I2C_Configure(mma845x_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
Access structure of the GPIO Driver. 
 
void BOARD_SystickStart(int32_t *pStart)
Function to Record the Start systick. 
 
#define MMA845x_CTRL_REG4_INT_EN_FF_MT_ENABLED
 
void BOARD_RunADS(const char *appName, char *boardString, char *shieldString, size_t bufferLength)
The function to register Application Name and initialte ADS. 
 
fxls8962_acceldataUser_t rawData
 
void mma845x_int_data_ready_callback(void *pUserData)
 
#define APPLICATION_VERSION
Version to distinguish between instances the same application based on target Shield and updates...
 
uint8_t Host_IO_Init(ARM_DRIVER_USART *pDrv, void *pBus, void *pDevInfo, void *spiSlaveParams, uint16_t slaveAddress)
 
#define MMA845x_XYZ_DATA_CFG_FS_FS_RANGE_2G
 
This structure defines the Write command List. 
 
This structure defines the Read command List. 
 
The host_io_uart.h file contains the Host Protocol interface definitions and configuration. 
 
#define STREAMING_HEADER_LEN
 
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
 
void MMA845x_I2C_SetIdleTask(mma845x_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
#define MMA845x_ACCEL_DATA_SIZE
The size of the MMA845x accel data. 
 
#define MMA845x_TRANSIENT_CFG_XTEFE_ENABLED
 
char boardString[ADS_MAX_STRING_LENGTH]
 
#define MMA845x_CTRL_REG1_DR_MASK
 
#define I2C_S_SIGNAL_EVENT
 
const registerreadlist_t mma845x_Output_Values[]
 
#define MMA8451_WHO_AM_I_WHOAMI_VALUE
 
The mma845x_drv.h file describes the MMA845x driver interface and structures.