46 #include "clock_config.h"    51 #include "Driver_I2C.h"    52 #include "Driver_USART.h"    57 #include "issdk_hal.h"    58 #include "gpio_driver.h"    65 #include "auto_detection_service.h"    70 #define MPL3115_PADDING_SIZE (1)    71 #define MPL3115_PRESSURE_DATA_SIZE (3)    72 #define MPL3115_TEMPERATURE_DATA_SIZE (2)    74 #define STREAMING_PKT_TIMESTAMP_LEN (4)    75 #define MMA865x_DATA_SIZE (6)    76 #define MAG3110_DATA_SIZE (6)    77 #define FXAS21002_DATA_SIZE (FXAS21002_GYRO_DATA_SIZE)    78 #define MPL3115_DATA_SIZE (MPL3115_PRESSURE_DATA_SIZE + MPL3115_TEMPERATURE_DATA_SIZE)    80 #define STREAMING_PAYLOAD_LEN                                                                                        \    81     (STREAMING_PKT_TIMESTAMP_LEN + MMA865x_DATA_SIZE + MAG3110_DATA_SIZE + FXAS21002_DATA_SIZE + MPL3115_DATA_SIZE + \    85 #define APPLICATION_NAME "11 Axis Sensor Demo"    87 #define APPLICATION_VERSION "2.5"    93 #define FF_MT_WT_DBCNT 0x32      94 #define FF_MT_THS_VALUE 0x03     96 #define SDCD_FF_EVT_ID (0x01)    97 #define P_THS_EVENT_ID (0x02)    98 #define EVENT_PAYLOAD_LEN (1)   214     uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse, 
size_t *hostMsgSize, 
size_t respBufferSize)
   216     bool success = 
false;
   231         if (respBufferSize >= boardNameLen + shieldNameLen + appNameLen + 3)
   240         hostResponse[*hostMsgSize] = appNameLen;
   243         memcpy(hostResponse + *hostMsgSize, 
embAppName, appNameLen);
   244         *hostMsgSize += appNameLen;
   246         hostResponse[*hostMsgSize] = boardNameLen;
   249         memcpy(hostResponse + *hostMsgSize, 
boardString, boardNameLen);
   250         *hostMsgSize += boardNameLen;
   252         hostResponse[*hostMsgSize] = shieldNameLen;
   255         memcpy(hostResponse + *hostMsgSize, 
shieldString, shieldNameLen);
   256         *hostMsgSize += shieldNameLen;
   266         switch (hostCommand[0]) 
   300             secondaryStreamID2, secondaryStreamID3, 
   346     if (ARM_DRIVER_OK != status)
   352     status = pI2cDriver->PowerControl(ARM_POWER_FULL);
   353     if (ARM_DRIVER_OK != status)
   359     status = pI2cDriver->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   360     if (ARM_DRIVER_OK != status)
   367     if (ARM_DRIVER_OK != status)
   373     status = pUartDriver->PowerControl(ARM_POWER_FULL);
   374     if (ARM_DRIVER_OK != status)
   381     if (ARM_DRIVER_OK != status)
   456     if (0 == secondaryStreamID1)
   464     if (0 == secondaryStreamID2)
   471     if (0 == secondaryStreamID3)
   534         if (ARM_DRIVER_OK != status)
   540         rawData_mma865x.
accel[0] = ((int16_t)data[0] << 8) | data[1];
   541         rawData_mma865x.
accel[0] /= 16;
   542         rawData_mma865x.
accel[1] = ((int16_t)data[2] << 8) | data[3];
   543         rawData_mma865x.
accel[1] /= 16;
   544         rawData_mma865x.
accel[2] = ((int16_t)data[4] << 8) | data[5];
   545         rawData_mma865x.
accel[2] /= 16;
   549                sizeof(rawData_mma865x.
accel));
   553         if (ARM_DRIVER_OK != status)
   559         rawData_mag3110.
mag[0] = ((int16_t)data[6] << 8) | data[7];
   560         rawData_mag3110.
mag[1] = ((int16_t)data[8] << 8) | data[9];
   561         rawData_mag3110.
mag[2] = ((int16_t)data[10] << 8) | data[11];
   567                &rawData_mag3110.
mag, 
sizeof(rawData_mag3110.
mag));
   572         if (ARM_DRIVER_OK != status)
   578         rawData_fxas21002.
gyro[0] = ((int16_t)data[12] << 8) | data[13];
   579         rawData_fxas21002.
gyro[1] = ((int16_t)data[14] << 8) | data[15];
   580         rawData_fxas21002.
gyro[2] = ((int16_t)data[16] << 8) | data[17];
   585                &rawData_fxas21002.
gyro, 
sizeof(rawData_fxas21002.
gyro));
   590         if (ARM_DRIVER_OK != status)
   596         rawData_mpl3115.
pressure = (uint32_t)((data[18]) << 16) | ((data[19]) << 8) | ((data[20]));
   598         rawData_mpl3115.
temperature = (int16_t)((data[21]) << 8) | (data[22]);
 
registerDeviceInfo_t deviceInfo
 
#define MAG3110_CTRL_REG1_OS_OSR_16
 
uint32_t BOARD_SystickElapsedTime_us(int32_t *pStart)
Function to compute the Elapsed Time. 
 
#define MMA865x_CTRL_REG3_IPOL_MASK
 
#define FXAS21002_CTRL_REG2_INT_EN_DRDY_MASK
 
#define FXAS21002_CTRL_REG2_INT_CFG_DRDY_INT1
 
#define MMA865x_XYZ_DATA_CFG_FS_MASK
 
int32_t MAG3110_I2C_Initialize(mag3110_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
#define FXAS21002_CTRL_REG2_IPOL_MASK
 
ARM_DRIVER_I2C * pCommDrv
 
#define __END_WRITE_DATA__
 
int32_t MMA865x_I2C_Initialize(mma865x_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
#define HOST_PRO_CMD_W_CFG_TAG
 
char embAppName[ADS_MAX_STRING_LENGTH]
 
volatile bool bMult2bReady
 
int32_t MPL3115_I2C_Initialize(mpl3115_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
This structure defines the mma865x raw data buffer. 
 
#define MAG3110_CTRL_REG2_MAG_RST_EN
 
void Host_IO_Receive(host_cmd_proc_fn_t process_host_command, uint8_t encoding)
 
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
 
#define MMA865x_DATA_SIZE
 
#define BOARD_BootClockRUN
 
#define FXAS21002_CTRL_REG1_DR_MASK
 
int32_t MAG3110_I2C_Configure(mag3110_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
#define MMA865x_CTRL_REG5_INT_CFG_FF_MT_MASK
 
volatile bool bMpl3115EventReady
 
#define MMA865x_FF_MT_SRC_EA_DETECTED
 
#define MMA865x_CTRL_REG3_IPOL_ACTIVE_HIGH
 
const registerreadlist_t cMma865xOutputValues[]
 
#define MPL3115_CTRL_REG3_IPOL1_MASK
 
The mag3110_drv.h file describes the MAG3110 driver interface and structures. 
 
const registerreadlist_t cMag3110OutputNormal[]
Address and size of Raw Magnetic Data in Normal Mode. 
 
volatile bool bStreamingEnabled
 
#define FXAS21002_DATA_SIZE
 
#define MMA865x_FF_MT_THS_THS_MASK
 
This defines the sensor specific information. 
 
uint8_t data[FXLS8962_DATA_SIZE]
 
int32_t MPL3115_I2C_ReadData(mpl3115_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
int32_t MMA865x_I2C_ReadData(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
#define MAG3110_CTRL_REG1_DR_ODR_1
 
#define MPL3115_CTRL_REG5_INT_CFG_PTH_MASK
 
#define MPL3115_CTRL_REG1_OST_SET
 
#define FXAS21002_CTRL_REG2_INT_EN_DRDY_ENABLE
 
void(* toggle_pin)(pinID_t aPinId)
 
const registerreadlist_t mpl3115_Output_Values[]
Address and size of Raw Pressure+Temperature Data in Normal Mode. 
 
#define APPLICATION_NAME
Unique Name for this application which should match the target GUI pkg name. 
 
#define MMA865x_FF_MT_CFG_ELE_EN
 
ARM_DRIVER_I2C * pCommDrv
 
#define HOST_B_SIGNAL_EVENT
 
#define ADS_MAX_STRING_LENGTH
 
#define MPL3115_CTRL_REG4_INT_EN_PTH_INTENABLED
 
#define MPL3115_CTRL_REG1_OST_MASK
 
This defines the sensor specific information. 
 
registerDeviceInfo_t deviceInfo
 
#define HOST_PRO_INT_DEV_TAG
 
uint8_t streamingPacket[STREAMING_HEADER_LEN+FXLS8962_STREAM_DATA_SIZE]
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
GENERIC_DRIVER_GPIO * pGpioDriver
 
#define MAG3110_CTRL_REG1_OS_MASK
 
The fxas21002_drv.h file describes the fxas21002 driver interface and structures. ...
 
#define HOST_PRO_INT_CMD_TAG
Bit aligned values for Host Protocol Interface IDs (Bits 5-6). 
 
#define MMA865x_CTRL_REG1_DR_MASK
 
#define MPL3115_CTRL_REG4_INT_EN_PTH_MASK
 
#define MAG3110_CTRL_REG2_RAW_RAW
 
#define __END_READ_DATA__
 
#define MMA865x_CTRL_REG1_DR_50HZ
 
void MPL3115_I2C_SetIdleTask(mpl3115_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
void mma865x_int_event_ready_callback(void *pUserData)
This is the Sensor WT Event Ready ISR implementation. 
 
#define MMA865x_FF_MT_CFG_YEFE_MASK
 
#define MPL3115_CTRL_REG5_INT_CFG_PTH_INT1
 
#define MPL3115_WHOAMI_VALUE
 
#define FXAS21002_CTRL_REG2_INT_CFG_DRDY_MASK
 
void MAG3110_I2C_SetIdleTask(mag3110_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
const registerwritelist_t cMma865xConfigFreeFall[]
Register settings for freefall detection and poll mode. 
 
void MMA865x_I2C_SetIdleTask(mma865x_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
#define MMA8652_WHOAMI_VALUE
 
#define MPL3115_DATA_SIZE
 
This structure defines the mag3110 data buffer. 
 
#define MMA865x_CTRL_REG4_INT_EN_FF_MT_EN
 
gpioHandleKSDK_t GREEN_LED
 
This defines the sensor specific information. 
 
This structure defines the fxas21002 raw data buffer. 
 
This defines the sensor specific information for I2C. 
 
void MAG3110_CalibrateHardIronOffset(int16_t *xValue, int16_t *yValue, int16_t *zValue)
Calibrates the magnetometer reading by determining the current hard iron offset. 
 
const registerreadlist_t fxas21002_Output_Values[]
 
const registerwritelist_t cMag3110ConfigNormal[]
Register settings for Normal (non buffered) mode. 
 
#define MMA865x_FF_MT_CFG_OAE_FREEFALL
 
#define MAG3110_CTRL_REG1_DR_MASK
 
#define MAG3110_CTRL_REG2_MAG_RST_MASK
 
#define MAG3110_DATA_SIZE
 
int32_t MMA865x_I2C_Configure(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
#define MMA865x_FF_MT_CFG_XEFE_EN
 
#define MAG3110_CTRL_REG2_RAW_MASK
 
#define MMA865x_XYZ_DATA_CFG_FS_2G
 
void Host_IO_Add_ISO_Header(uint8_t streamID, uint8_t *pStreamingPacket, size_t sizePayload)
 
#define MMA865x_CTRL_REG4_INT_EN_FF_MT_MASK
 
#define APPLICATION_VERSION
Version to distinguish between instances the same application based on target Shield and updates...
 
void Host_IO_Send(uint8_t *pMsg, size_t size, uint8_t encoding)
 
void(* clr_pin)(pinID_t aPinId)
 
#define MMA865x_CTRL_REG2_MODS_MASK
 
#define MMA865x_FF_MT_CFG_ZEFE_EN
 
#define MPL3115_PRESSURE_DATA_SIZE
 
char boardString[ADS_MAX_STRING_LENGTH]
 
#define STREAMING_PKT_TIMESTAMP_LEN
 
#define EVENT_PAYLOAD_LEN
 
int32_t FXAS21002_I2C_ReadData(fxas21002_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
void BOARD_SystickEnable(void)
Function to enable systicks framework. 
 
#define MMA865x_FF_MT_CFG_ZEFE_MASK
 
#define MMA865x_CTRL_REG5_INT_CFG_FF_MT_INT1
 
#define MAG3110_CTRL_REG2_AUTO_MSRT_EN_EN
 
char shieldString[ADS_MAX_STRING_LENGTH]
 
int main(void)
Main function. 
 
#define I2C_S_DEVICE_INDEX
 
#define MMA865x_FF_MT_CFG_XEFE_MASK
 
#define FXAS21002_WHO_AM_I_WHOAMI_PROD_VALUE
 
#define FXAS21002_I2C_ADDR
 
int32_t FXAS21002_I2C_Configure(fxas21002_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
The mma865x_drv.h file describes the MMA865x driver interface and structures. 
 
void fxas21002_int_data_ready_callback(void *pUserData)
 
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
 
#define MMA865x_FF_MT_THS_DBCNTM_INC_CLR
 
volatile bool bFxas21002DataReady
 
#define STREAMING_PAYLOAD_LEN
 
void FXAS21002_I2C_SetIdleTask(fxas21002_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
#define BOARD_DEBUG_UART_BAUDRATE
 
#define MMA865x_FF_MT_CFG_ELE_MASK
 
The mpl3115_drv.h file describes the MPL3115 driver interface and structures. 
 
const registerwritelist_t cMpl3115SetOST[]
Register settings for Triggring One-Shot Sampling. 
 
registerDeviceInfo_t deviceInfo
 
Access structure of the GPIO Driver. 
 
void BOARD_SystickStart(int32_t *pStart)
Function to Record the Start systick. 
 
volatile bool bMma865xEventReady
 
void BOARD_RunADS(const char *appName, char *boardString, char *shieldString, size_t bufferLength)
The function to register Application Name and initialte ADS. 
 
#define MMA865x_FF_MT_SRC_EA_MASK
 
uint8_t Host_IO_Init(ARM_DRIVER_USART *pDrv, void *pBus, void *pDevInfo, void *spiSlaveParams, uint16_t slaveAddress)
 
#define MMA865x_CTRL_REG2_MODS_HR
 
This structure defines the Write command List. 
 
const registerreadlist_t cMma865xFreeFallEvent[]
Address of Freefall Status Register. 
 
This structure defines the Read command List. 
 
#define MAG3110_WHOAMI_VALUE
 
#define MMA865x_FF_MT_CFG_YEFE_EN
 
The host_io_uart.h file contains the Host Protocol interface definitions and configuration. 
 
#define STREAMING_HEADER_LEN
 
#define MPL3115_PADDING_SIZE
 
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
 
int32_t MAG3110_I2C_ReadData(mag3110_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
const registerwritelist_t fxas21002_Config_Normal[]
 
#define FXAS21002_CTRL_REG2_IPOL_ACTIVE_HIGH
 
#define MAG3110_CTRL_REG2_AUTO_MSRT_EN_MASK
 
void mpl3115_int_event_ready_callback(void *pUserData)
 
This structure defines the mpl3115 data buffer in Pressure Mode. 
 
#define FXAS21002_CTRL_REG1_DR_25HZ
 
bool process_host_command(uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse, size_t *hostMsgSize, size_t respBufferSize)
 
#define I2C_S_SIGNAL_EVENT
 
int32_t FXAS21002_I2C_Initialize(fxas21002_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
#define MMA865x_FF_MT_THS_DBCNTM_MASK
 
ARM_DRIVER_I2C * pCommDrv
 
ARM_DRIVER_I2C * pCommDrv
 
int32_t Sensor_I2C_Write(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerwritelist_t *pRegWriteList)
Write register data to a sensor. 
 
#define MPL3115_CTRL_REG3_IPOL1_HIGH
 
#define MMA865x_FF_MT_CFG_OAE_MASK
 
registerDeviceInfo_t deviceInfo