46 #include "fsl_lptmr.h"    47 #include "clock_config.h"    52 #include "Driver_I2C.h"    53 #include "Driver_USART.h"    58 #include "issdk_hal.h"    59 #include "gpio_driver.h"    63 #include "auto_detection_service.h"    68 #define fxlc95000_odrCallback LPTMR0_IRQHandler     69 #define SAMPLING_RATE_ms 100                        70 #define FXLC95000_SAMPLE_SIZE 10                    73 #define APPLICATION_NAME "FXLC95000 Accelerometer Demo"    75 #define APPLICATION_VERSION "2.5"    90     {QuickReadInterruptDisable, 0, 
sizeof(QuickReadInterruptDisable)}, 
    91     {ConfigureMBoxCmd, 0, 
sizeof(ConfigureMBoxCmd)}, 
    97     {StopDataCmd, 0, 
sizeof(StopDataCmd)},                                   
   101     {StartDataCmd, 0, 
sizeof(StartDataCmd)},                                 
   106     {UnprotectFlash, 0, 
sizeof(UnprotectFlash)},           
   107     {EraseMainFlashArray, 0, 
sizeof(EraseMainFlashArray)}, 
   113     {ProtectFlash, 0, 
sizeof(ProtectFlash)}, 
   139     LPTMR_ClearStatusFlags(LPTMR0, kLPTMR_TimerCompareFlag);
   172     LPTMR_StartTimer(LPTMR0);
   181     uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse, 
size_t *hostMsgSize, 
size_t respBufferSize)
   183     static uint8_t toggle_led = 0;
   184     bool success = 
false;
   185     size_t rxMsgSize = *hostMsgSize; 
   201         if (respBufferSize >= boardNameLen + shieldNameLen + appNameLen + 3)
   210         hostResponse[*hostMsgSize] = appNameLen;
   213         memcpy(hostResponse + *hostMsgSize, 
embAppName, appNameLen);
   214         *hostMsgSize += appNameLen;
   216         hostResponse[*hostMsgSize] = boardNameLen;
   219         memcpy(hostResponse + *hostMsgSize, 
boardString, boardNameLen);
   220         *hostMsgSize += boardNameLen;
   222         hostResponse[*hostMsgSize] = shieldNameLen;
   225         memcpy(hostResponse + *hostMsgSize, 
shieldString, shieldNameLen);
   226         *hostMsgSize += shieldNameLen;
   244         switch (hostCommand[0]) 
   279         switch (hostCommand[0]) 
   305                     if (toggle_led++ % 32 == 0 ? 
true : 
false)
   317                                                                          cFxlc95000FlashPostprocess))
   340     lptmr_config_t lptmrConfig;
   359     LPTMR_GetDefaultConfig(&lptmrConfig);
   360     LPTMR_Init(LPTMR0, &lptmrConfig);
   361     LPTMR_EnableInterrupts(LPTMR0, kLPTMR_TimerInterruptEnable);
   362     LPTMR_SetTimerPeriod(LPTMR0, MSEC_TO_COUNT(
SAMPLING_RATE_ms, CLOCK_GetFreq(kCLOCK_LpoClk)));
   363     EnableIRQ(LPTMR0_IRQn);
   375     if (ARM_DRIVER_OK != status)
   381     status = I2Cdrv->PowerControl(ARM_POWER_FULL);
   382     if (ARM_DRIVER_OK != status)
   388     status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   389     if (ARM_DRIVER_OK != status)
   396     if (ARM_DRIVER_OK != status)
   402     status = pUartDriver->PowerControl(ARM_POWER_FULL);
   403     if (ARM_DRIVER_OK != status)
   410     if (ARM_DRIVER_OK != status)
   445         if (ARM_DRIVER_OK != status)
 #define FXLC95000_SET_RESOLUTION_CMD_HDR
The FXLC95000 Set Resolution Command Header Bytes. 
 
const uint8_t cFxlc95000_SetResolution_Cmd[]
 
const registercommandlist_t cFxlc95000ConfigMBox[]
 
#define FXLC95000_I2C_ADDR
 
#define HOST_PRO_CMD_W_CFG_TAG
 
int32_t FXLC95000_I2C_CheckRomMode(ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress)
The interface function to check if the sensor is in ROM CI Mode. 
 
const uint8_t cFxlc95000_SetRange_Cmd[]
 
#define HOST_S_SIGNAL_EVENT
 
#define FXLC95000_ACCEL_RANGE_2G
The FXLC95000 FS Range 2G. 
 
void Host_IO_Receive(host_cmd_proc_fn_t process_host_command, uint8_t encoding)
 
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
 
#define BOARD_BootClockRUN
 
char shieldString[ADS_MAX_STRING_LENGTH]
 
registerDeviceInfo_t deviceInfo
 
char embAppName[ADS_MAX_STRING_LENGTH]
 
void(* toggle_pin)(pinID_t aPinId)
 
int fxlc95000_enSensor(fxlc95000_i2c_sensorhandle_t *pSensorHandle)
 
#define ADS_MAX_STRING_LENGTH
 
#define HOST_PRO_INT_DEV_TAG
 
uint8_t streamingPacket[STREAMING_HEADER_LEN+FXLS8962_STREAM_DATA_SIZE]
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
#define HOST_PRO_INT_CMD_TAG
Bit aligned values for Host Protocol Interface IDs (Bits 5-6). 
 
const uint8_t cFxlc95000_SetODR_Cmd[]
 
#define __END_READ_DATA__
 
GENERIC_DRIVER_GPIO * pGpioDriver
 
volatile bool bFxlc95000Boot
 
#define APPLICATION_VERSION
Version to distinguish between instances the same application based on target Shield and updates...
 
const registercommandlist_t cFxlc95000ConfigSensor[]
 
#define FXLC95000_SET_RANGE_CMD_HDR
The FXLC95000 Set Range Command Header Bytes. 
 
const registercommandlist_t cFxlc95000FlashPostprocess[]
 
The fxlc95000_drv.h file describes the FXLC95000L driver interface and structures. 
 
gpioHandleKSDK_t GREEN_LED
 
volatile bool bFxlc95000Ready
 
volatile bool bStreamingEnabled
 
int32_t FXLC95000_I2C_FlashPayload(ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t *pFlashBytes, uint8_t numBytes)
The interface function to write ROM CI Data Payload. 
 
int32_t FXLC95000_I2C_FlashCommands(ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, const registercommandlist_t *pCommandList)
The interface function to write ROM CI Commands. 
 
#define fxlc95000_odrCallback
 
#define FXLC95000_SAMPLE_OFFSET
Time stamp and XYZ Data Register Offset. 
 
#define __END_WRITE_CMD__
 
void Host_IO_Add_ISO_Header(uint8_t streamID, uint8_t *pStreamingPacket, size_t sizePayload)
 
#define APPLICATION_NAME
Unique Name for this application which should match the target GUI pkg name. 
 
void Host_IO_Send(uint8_t *pMsg, size_t size, uint8_t encoding)
 
void(* set_pin)(pinID_t aPinId)
 
void(* clr_pin)(pinID_t aPinId)
 
void FXLC95000_I2C_SetIdleTask(fxlc95000_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
void BOARD_SystickEnable(void)
Function to enable systicks framework. 
 
int32_t FXLC95000_I2C_CommandResponse(fxlc95000_i2c_sensorhandle_t *pSensorHandle, const registercommandlist_t *pCommandList, const registerreadlist_t *pResponseList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
#define I2C_S_DEVICE_INDEX
 
#define FXLC95000_SET_ODR_CMD_HDR
The FXLC95000 Set Report Rate Command Header Bytes. 
 
fxlc95000_i2c_sensorhandle_t fxlc95000Driver
 
volatile bool bFxlc95000DataReady
 
#define FXLC95000_SAMPLE_SIZE
 
char boardString[ADS_MAX_STRING_LENGTH]
 
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
 
volatile bool bFxlc95000Flashing
 
#define BOARD_DEBUG_UART_BAUDRATE
 
Access structure of the GPIO Driver. 
 
int32_t FXLC95000_I2C_Initialize(fxlc95000_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint16_t buildId)
The interface function to initialize the sensor. 
 
bool process_host_command(uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse, size_t *hostMsgSize, size_t respBufferSize)
 
void BOARD_RunADS(const char *appName, char *boardString, char *shieldString, size_t bufferLength)
The function to register Application Name and initialte ADS. 
 
const registercommandlist_t cFxlc95000FlashPreprocess[]
 
#define FXLC95000_BUILD_ID
The FXLC95000 BCD encoded ISF1.1_95k_Build_ID. 
 
uint8_t Host_IO_Init(ARM_DRIVER_USART *pDrv, void *pBus, void *pDevInfo, void *spiSlaveParams, uint16_t slaveAddress)
 
int main(void)
Main function. 
 
This structure defines the Read command List. 
 
The host_io_uart.h file contains the Host Protocol interface definitions and configuration. 
 
#define STREAMING_HEADER_LEN
 
const registerreadlist_t cFxlc95000ReadSample[]
 
This defines the sensor specific information for I2C. 
 
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
 
This structure defines the Block command List. 
 
#define FXLC95000_SST_ODR_PAYLOAD(x)
The FXLC95000 Set Report Rate Payload Bytes. 
 
#define I2C_S_SIGNAL_EVENT
 
#define FXLC95000_ACCEL_RESOLUTION_14_BIT
The FXLC95000 Resoultion 14-Bit.