16 #include "clock_config.h" 18 #include "fsl_debug_console.h" 21 #include "Driver_I2C.h" 24 #include "issdk_hal.h" 31 #define FXLS8974_DATA_SIZE 6 74 PRINTF(
"\r\n ISSDK FXLS8974 sensor driver example demonstration with poll mode\r\n");
78 if (ARM_DRIVER_OK != status)
80 PRINTF(
"\r\n I2C Initialization Failed\r\n");
85 status = I2Cdrv->PowerControl(ARM_POWER_FULL);
86 if (ARM_DRIVER_OK != status)
88 PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
93 status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
94 if (ARM_DRIVER_OK != status)
96 PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
103 if (ARM_DRIVER_OK != status)
105 PRINTF(
"\r\n Sensor Initialization Failed\r\n");
110 PRINTF(
"\r\n Successfully Initialized Gemini with WHO_AM_I = 0x%X\r\n", whoami);
114 PRINTF(
"\r\n Successfully Initialized Timandra with WHO_AM_I = 0x%X\r\n", whoami);
118 PRINTF(
"\r\n Successfully Initialized Newstein with WHO_AM_I = 0x%X\r\n", whoami);
122 PRINTF(
"\r\n Bad WHO_AM_I = 0x%X\r\n", whoami);
131 if (ARM_DRIVER_OK != status)
133 PRINTF(
"\r\n FXLS8974 Sensor Configuration Failed, Err = %d\r\n", status);
136 PRINTF(
"\r\n Successfully Applied FXLS8974 Sensor Configuration\r\n");
149 if (ARM_DRIVER_OK != status)
151 PRINTF(
"\r\n Read Failed. \r\n");
156 rawData.
accel[0] = ((int16_t)data[1] << 8) | data[0];
157 rawData.
accel[1] = ((int16_t)data[3] << 8) | data[2];
158 rawData.
accel[2] = ((int16_t)data[5] << 8) | data[4];
161 PRINTF(
"\r\nX=%5d Y=%5d Z=%5d\r\n", rawData.
accel[0], rawData.
accel[1], rawData.
accel[2]);
This structure defines the Write command List.
#define FXLS8974_SENS_CONFIG1_FSR_MASK
#define FXLS8974_INT_STATUS_SRC_DRDY_MASK
int32_t FXLS8974_I2C_Configure(fxls8974_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
#define ASK_USER_TO_RESUME(x)
int32_t FXLS8974_I2C_Initialize(fxls8974_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t *whoami)
The interface function to initialize the sensor.
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
const registerwritelist_t cFxls8974ConfigNormal[]
Register settings for Normal (non buffered) mode.
This defines the sensor specific information for I2C.
const registerreadlist_t cFxls8974DRDYEvent[]
Address of DATA Ready Status Register.
#define __END_WRITE_DATA__
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
#define FXLS8967_WHOAMI_VALUE
#define I2C_S_SIGNAL_EVENT
#define FXLS8974_I2C_ADDR
#define BOARD_BootClockRUN
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
int32_t FXLS8974_I2C_ReadData(fxls8974_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
This structure defines the fxls8974 raw data buffer.
uint8_t data[FXLS8962_DATA_SIZE]
#define __END_READ_DATA__
#define FXLS8974_SENS_CONFIG3_WAKE_ODR_MASK
#define FXLS8974_DATA_SIZE
fxls8974_i2c_sensorhandle_t fxls8974Driver
fxos8700_accelmagdata_t rawData
void FXLS8974_I2C_SetIdleTask(fxls8974_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
void BOARD_SystickEnable(void)
Function to enable systicks framework.
int main(void)
Main function.
#define FXLS8974_SENS_CONFIG1_FSR_2G
This structure defines the Read command List.
#define FXLS8974_WHOAMI_VALUE
The fxls8974_drv.h file describes the FXLS8974CF driver interface and structures. ...
#define FXLS8968_WHOAMI_VALUE
#define I2C_S_DEVICE_INDEX
void BOARD_InitDebugConsole(void)
#define FXLS8962_WHOAMI_VALUE
#define FXLS8974_SENS_CONFIG3_WAKE_ODR_6_25HZ
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
#define FXLS8964_WHOAMI_VALUE
const registerreadlist_t cFxls8974OutputNormal[]
Address of Raw Accel Data in Normal Mode.