edma_single_transfer

Overview

The EDMA single transfer example is a simple demonstration program that uses the SDK software. It excuates one shot transfer from source buffer to destination buffer using the SDK EDMA drivers. The purpose of this example is to show how to use the EDMA transactional interface to perform a single transfer and to provide a simple example for debugging and further development.

Supported Boards