dsc_i2c_interrupt

Overview

The i2c_functional_interrupt example shows how to use I2C functional driver to build a interrupt based application:

In this example , one i2c instance used as I2C master and another i2c instance used as I2C slave .

  1. I2C master send data to I2C slave in interrupt . (I2C Slave using interrupt to receive the data)

  2. I2C master read data from I2C slave in interrupt . (I2C Slave using interrupt to send the data)

  3. The example assumes that the connection is OK between master and slave, so there’s NO error handling code.

Supported Boards