dsc_mscan_loopback

Overview

The mscan_loopback_functional example shows how to use the loopback test mode to debug your CAN Bus design:

To demonstrates this example, only one board is needed. The example will configure one MSCAN Message Tx buffer and Rx buffer with same ID. After that, the example will send a CAN Message from the Tx Buffer to the Rx Buffer throuth internal loopback interconnect and print out the Message payload to terminal.

Supported Boards