dspi_interrupt_b2b_transfer_slave
Overview
The dspi_interrupt_b2b_transfer example shows how to use DSPI driver in interrupt way:
In this example , we need two boards, one board used as DSPI master and another board used as DSPI slave. The file ‘dspi_interrupt_b2b_transfer_slave.c’ includes the DSPI slave code. This example uses the transactional API in DSPI driver.
DSPI master send/received data to/from DSPI slave in interrupt . (DSPI Slave using interrupt to receive/send the data)