dspi_polling_b2b_transfer_slave

Overview

The dspi_polling_b2b_transfer example shows how to use DSPI driver in polling way:

In this example , we need two boards, one board used as DSPI master and another board used as DSPI slave. The file ‘dspi_polling_b2b_transfer_slave.c’ includes the DSPI slave code.

  1. DSPI master send/received data to/from DSPI slave in polling . (DSPI Slave using interrupt to receive/send the data)

Supported Boards