i2c_interrupt
Overview
The i2c_functional_interrupt example shows how to use I2C functional driver to build a interrupt based application:
In this example , one i2c instance used as I2C master and another i2c instance used as I2C slave .
I2C master send data to I2C slave in interrupt . (I2C Slave using interrupt to receive the data)
I2C master read data from I2C slave in interrupt . (I2C Slave using interrupt to send the data)
The example assumes that the connection is OK between master and slave, so there’s NO error handling code.