igpio_input_eqdc_signal
Overview
The GPIO Example project is a program functioning as an encoder which outputs two quadrature signals and one interrupt signal.
The example is supported by the set, clear registers, and toggle write-only registers for each port output data register.
Running the demo
When the example runs successfully, the following message is displayed in the terminal: If you turn on the SW8 , and “SW8 is turned on, INDEX generated” is shown on the terminal window
GPIO Driver example.
Out put signals for EQDC module.
SW8 is turned on, INDEX generated.
......