isi_dwc_mipi_csi2_rgb565
Overview
This example shows how to use ISI to receive camera frame through MIPI CSI2.
In this example, the camera input frame and ISI output frame are both RGB565 format. The output frame is shown in the screen.
NOTE:
the example is for newly Synopsys DWC MIPI CSI2 driver and IMX95 platform.
This example must run continously to get the right result, breaking during debug will results to display tearing. Because the ISI driver maintains IP state through ISR, if the core is halted, then driver state does not match the IP state. When exiting debug, the core might be halted for a short while, so the tearing may happen when exiting debug.
If the camera and LCD panel resolutions are not the same, then only part of the camera frame will be shown.