lpspi_3wire_int_transfer_master
Overview
The lpspi_3wire_int_transfer example shows how to use LPSPI’s 3-wire mode in interrupt way:
In this example , we need two boards, one board used as LPSPI master and another board used as LPSPI slave. The file ‘lpspi_3wire_int_b2b_transfer_master.c’ includes the LPSPI master code. This example uses the transactional API in LPSPI driver.
LPSPI master send/received data to/from LPSPI slave in interrupt . (LPSPI Slave using interrupt to receive/send the data)
LPSPI master will use SOUT pin as input/output pin, and slave will use SIN pin as input/output pin.